KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADRV9002
Recommended for New Designs
The ADRV9002 is a highly integrated RF transceiver that has dual-channel transmitters, dual-channel receivers, integrated synthesizers, and digital signal...
Datasheet
ADRV9002 on Analog.com
Hi,
Currently i am trying to establish a ADC DAC loopback for ADRV9002 transceiver for ZCU102 eval board. For that i have taken the HDL and C files from the github and make changes in it as per the requirement . While doing so i am facing some error messages on launching the project. The issue is very frequent and i got stuck into it. I have attached the prints of the error, kindly look into it and suggest any changes or modification in the project if required. Also let me know if any further information you required so as to establish the loopback.
regards,
Anurag
Hello [ERROR]: Error number 3 (0x00000003), Recovery action -101.In file ../noos/drivers/rf-transceiver/navassa/devices/adrv9001/public/src/adi_adrv9001_arm.c, in function adi_adrv9001_arm_CmdStatus_Wait, in line 671, variable name device.Error message ArmCmdStatusWait() failed due to thrown ARM error. Is device in correct state for calling command?. [ERROR]: Error number 13315 (0x00003403), Recovery action -2.In file ../noos/drivers/rf-transceiver/navassa/devices/adrv9001/private/src/adrv9001_arm.c, in function adrv9001_ArmCmdErrorHandler, in line 2852, variable name mailboxErrCode.Error message Error occurred during an Init Calibration. Check that no signal is being applied to the Rx ports. Check that correct external LOs are applied, and synchronized, where appropriate. [ERROR]: Error number 13315 (0x00003403), Recovery action -2.In file ../noos/drivers/rf-transceiver/navassa/devices/adrv9001/public/src/adi_adrv9001_cals.c, in function adi_adrv9001_cals_InitCals_Run, in line 117, variable name NULL.Error message Error occurred during an Init Calibration. Check that no signal is being applied to the Rx ports. Check that correct external LOs are applied, and synchronized, where appropriate. adrv9002_setup, 981: failed with "Error occurred during an Init Calibration. Check that no signal is being applied to the Rx ports. Check that correct external LOs are applied, and synchronized, where appropriate" (13315)
Hello!
We have replied to this question on the original thread: Issues in getting RF output for NO-OS project - Q&A - Microcontroller no-OS Drivers - EngineerZone
Please continue the conversation there.
Will close this thread as it is a duplicate.
All the best,
Tudor