Post Go back to editing

EVAL-AD7606 no-OS: Parallel Interface Support Status and "getting samples error" on ZC702

Thread Summary

The user encountered a 'getting samples error' when using the parallel interface of the AD7606 on ZC702, despite successful initialization. The final answer confirms that the no-OS driver now supports parallel mode and provides HDL and no-OS fixes tested on ZedBoard. The user should update their local branches with the provided commits and verify the DDR buffer address for ZC702.
AI Generated Content
Category: Hardware
Product Number: EVAL-AD7606

Hi,

I tested the EVAL-AD7606CFMCZ and then ported the design to ZC702.

For the serial interface, the no-OS driver works correctly and I can read valid data.

For the parallel interface, the initialization completes successfully, but when trying to acquire samples I get a "getting samples error".

I found this related discussion (from about 3 years ago), which suggests that the AD7606 no-OS driver only supports serial mode:Cannot initialize EVAL-AD7606B-FMCZ (no-OS project) - Q&A - FPGA Reference Designs - EngineerZone. I also noticed the following comment in the source code:

/* Driver currently supports only serial interface, therefore, ... */

So I would like to confirm:

  1. Is the parallel interface still not supported in the current no-OS driver, or has this been updated/fixed in newer versions?
  2. If parallel mode is now supported, are there any additional configurations or required changes (especially for porting to another device like ZC702)?

Any clarification would be appreciated.

Thanks.

Thread Notes

Parents Reply Children
  • Hello thanks for reply,

    I am using the newest version of HDL and no-OS Github, I have already verified the serial mode but failed in the parallel module. I ported the project by following the instruction.

    Do you have any suggestions for inspections?

  • Hello, some supplement:

    Here are the ILA results in Vivado, I set a break point after sentence " ret = ad7606_capture_pre_enable(dev);", where I think all initialization is done and I see signals in this figure. I think the only problem that there is no valid data, so reading process is running but data is not sent through DMA to memory. I am a bit confused here, because I basically don't change much in Vivado during porting as I only deleted some hdmi and other input definition, which should not influence ADC structure

  • Hello,

    Unfortunately we've had multiple problems with this driver, so we are starting an internal process to see if we can find and fix these issues. This may take a while, so in the meantime feel free to ask any other questions in our forums.

    Thank you for your patience,

    Eric

  • Hi,

    Thanks for feedback!

    I would like to share my current status, as the figure shows the ADC IPs are working correcting. I suspect the problems are located at the function " ret = ad7606_read_samples(dev, buf, AD7606X_FMC_SAMPLE_NO);" in no-OS codes. As a writing done flag should be sent and data will be written into DDR in my understanding, however what I observe is in the function "ret = axi_dmac_transfer_wait_completion(axi->dmac, 1000)" transfer cannot be completed and finally communication fails.

    Thanks

  • Hi,
    Thank you for the detailed explanation. We've managed to reproduce the bug and will assign someone to solve it as soon as possible.

    Thank you for your patience,
    Eric

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.