Post Go back to editing

EVAL-AD7606 no-OS: Parallel Interface Support Status and "getting samples error" on ZC702

Category: Hardware
Product Number: EVAL-AD7606

Hi,

I tested the EVAL-AD7606CFMCZ and then ported the design to ZC702.

For the serial interface, the no-OS driver works correctly and I can read valid data.

For the parallel interface, the initialization completes successfully, but when trying to acquire samples I get a "getting samples error".

I found this related discussion (from about 3 years ago), which suggests that the AD7606 no-OS driver only supports serial mode:Cannot initialize EVAL-AD7606B-FMCZ (no-OS project) - Q&A - FPGA Reference Designs - EngineerZone. I also noticed the following comment in the source code:

/* Driver currently supports only serial interface, therefore, ... */

So I would like to confirm:

  1. Is the parallel interface still not supported in the current no-OS driver, or has this been updated/fixed in newer versions?
  2. If parallel mode is now supported, are there any additional configurations or required changes (especially for porting to another device like ZC702)?

Any clarification would be appreciated.

Thanks.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.