Post Go back to editing

Issues in building NO-OS driver.

Thread Summary

The user encountered build errors for the no-OS project on a ZCU102 board with the ADRV9001 transceiver due to Windows compatibility issues. The solution involved removing the --transform 's/^(\.\/|\.)//' option from two tar commands in xilinx.mk. After this change, the project built successfully.
AI Generated Content
Category: Software

Hi,

While building no-os project for zcu102 with adrv9001 transceiver,  i'm getting below error msgs. I am also attaching the ss of the error. Kindly look into it.

Error msgs:

[00:00:00] [CC] no_os_util.c
[00:00:00] [LD] no_os_gpio.o no_os_spi.o axi_adc_core.o axi_dac_core.o axi_dmac.o xilinx_axi_io.o xilinx_delay.o xilinx_gpio.o xilinx_spi.o adrv9002.o adrv9002_conv.o adi_common_error.o adi_common_hal_wrapper.o adi_common_log.o adrv9001_arm.o adrv9001_bf_hal.o adrv9001_crc32.o adrv9001_gpio.o adrv9001_init.o adrv9001_rx.o adrv9001_validators.o adi_adrv9001.o adi_adrv9001_arm.o adi_adrv9001_auxadc.o adi_adrv9001_auxdac.o adi_adrv9001_bbdc.o adi_adrv9001_cals.o adi_adrv9001_common.o adi_adrv9001_dpd.o adi_adrv9001_fh.o adi_adrv9001_gpio.o adi_adrv9001_mcs.o adi_adrv9001_orx.o adi_adrv9001_powermanagement.o adi_adrv9001_powersavingandmonitormode.o adi_adrv9001_profileutil.o adi_adrv9001_radio.o adi_adrv9001_rx.o adi_adrv9001_rx_gaincontrol.o adi_adrv9001_spi.o adi_adrv9001_ssi.o adi_adrv9001_stream.o adi_adrv9001_tx.o adi_adrv9001_utilities.o jsmn.o headless.o no_os_platform.o no_os_alloc.o no_os_clk.o no_os_mutex.o no_os_util.o
make[2]: Nothing to be done for 'post_build'.
[00:00:00] Creating BOOT.BIN and archive with files
'\.\)' is not recognized as an internal or external command,
operable program or batch file.
make[1]: *** [D:/Vivado-proj/no-OS/tools/scripts/xilinx.mk:243: create_boot_bin] Error 255
make: *** [../../tools/scripts/generic.mk:334: all] Error 2



regards,
Anurag

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.