Post Go back to editing

Issues in building NO-OS driver.

Thread Summary

The user encountered build errors for the no-OS project on a ZCU102 board with the ADRV9001 transceiver due to Windows compatibility issues. The solution involved removing the --transform 's/^(\.\/|\.)//' option from two tar commands in xilinx.mk. After this change, the project built successfully.
AI Generated Content
Category: Software

Hi,

While building no-os project for zcu102 with adrv9001 transceiver,  i'm getting below error msgs. I am also attaching the ss of the error. Kindly look into it.

Error msgs:

[00:00:00] [CC] no_os_util.c
[00:00:00] [LD] no_os_gpio.o no_os_spi.o axi_adc_core.o axi_dac_core.o axi_dmac.o xilinx_axi_io.o xilinx_delay.o xilinx_gpio.o xilinx_spi.o adrv9002.o adrv9002_conv.o adi_common_error.o adi_common_hal_wrapper.o adi_common_log.o adrv9001_arm.o adrv9001_bf_hal.o adrv9001_crc32.o adrv9001_gpio.o adrv9001_init.o adrv9001_rx.o adrv9001_validators.o adi_adrv9001.o adi_adrv9001_arm.o adi_adrv9001_auxadc.o adi_adrv9001_auxdac.o adi_adrv9001_bbdc.o adi_adrv9001_cals.o adi_adrv9001_common.o adi_adrv9001_dpd.o adi_adrv9001_fh.o adi_adrv9001_gpio.o adi_adrv9001_mcs.o adi_adrv9001_orx.o adi_adrv9001_powermanagement.o adi_adrv9001_powersavingandmonitormode.o adi_adrv9001_profileutil.o adi_adrv9001_radio.o adi_adrv9001_rx.o adi_adrv9001_rx_gaincontrol.o adi_adrv9001_spi.o adi_adrv9001_ssi.o adi_adrv9001_stream.o adi_adrv9001_tx.o adi_adrv9001_utilities.o jsmn.o headless.o no_os_platform.o no_os_alloc.o no_os_clk.o no_os_mutex.o no_os_util.o
make[2]: Nothing to be done for 'post_build'.
[00:00:00] Creating BOOT.BIN and archive with files
'\.\)' is not recognized as an internal or external command,
operable program or batch file.
make[1]: *** [D:/Vivado-proj/no-OS/tools/scripts/xilinx.mk:243: create_boot_bin] Error 255
make: *** [../../tools/scripts/generic.mk:334: all] Error 2



regards,
Anurag

Parents
  • Hello,

    It looks like you are trying to build from Windows, while no-OS build system assumes a Linux environment, so we can see some compatibility issues. 

    What you can try is to remove the --transform 's/^\(\.\/\|\.\)//' option from two tar commands in xilinx.mk: line 323 and 330, should look something like this:

    	$(call copy_file,$(HARDWARE),$(BOOT_BIN_DIR)) $(HIDE)
    	$(call copy_file,$(FSBL_PATH),$(BOOT_BIN_DIR)) $(HIDE)
    	$(call copy_file,$(BINARY),$(BOOT_BIN_DIR)) $(HIDE)
    	tar -czvf $(BUILD_DIR)/bootgen_sysfiles.tar.gz --force-local --exclude 'BOOT.BIN' -C $(BOOT_BIN_DIR) . $(HIDE)
    else
    	$(call print,Creating archive with files)
    	$(call remove_dir,$(BUILD_DIR)/boot_files) $(HIDE)
    	$(call mk_dir,$(BUILD_DIR)/boot_files) $(HIDE)
    	$(call copy_file,$(HARDWARE),$(BUILD_DIR)/boot_files) $(HIDE)
    	$(call copy_file,$(BINARY),$(BUILD_DIR)/boot_files) $(HIDE)
    	tar -czvf $(BUILD_DIR)/bootgen_sysfiles.tar.gz --force-local -C $(BUILD_DIR)/boot_files . $(HIDE)
    endif

    I think the  --transform 's/^\(\.\/\|\.\)//' is purely cosmetic. If it works, for you, I will provide a permanent fix.

  • Hi  

    I removed the --transform 's/^\(\.\/\|\.\)//' options from two tar commands in xilinx.mk. After doing this the project got build correctly. Now can i proceed further ? or else you would provide a permanent fix?

    regards,
    Anurag

Reply Children
  • Please proceed. I will provide a fix, but needs to get through the internal review first and it might take a couple of days until it is approved and merged on the mainline. 

  • Hi  

    I have successfully built the HDL and NO-OS project in two different environments: Vivado/SDK 2019.1 and Vivado/Vitis 2022.2.

    The Problem:
    Upon launching the code on the hardware, the initialization sequence appears successful. The Vitis/SDK serial terminal shows the expected prints and initialization logs. However, when monitoring the output via a Signal Analyzer at the desired carrier frequency, there is no signal detected (only LO leakage is seen at the carrier frequency).

    Hardware Setup:

    • Carrier Board: [ZCU102]

    • RF Transceiver: [ADRV9002]

    Observations:

    1. Software: The No-OS state machine completes without returning error codes.

    2. RF Output: No signal at the SMA connectors. I have verified the cables and the signal analyzer settings.

      I have attached the headless main.c files for both versions and the corresponding Vitis terminal logs. I am concerned that I may be missing a critical function call required to transition the signal from the 'Ready' state to Transmitting. Kindly look into it.

      Headless_2019:

      /***************************************************************************//**
       *   @file   headless.c
       *   @brief  adrv9002 main project file.
       *   @author Darius Berghe (darius.berghe@analog.com)
      ********************************************************************************
       * Copyright 2020(c) Analog Devices, Inc.
       *
       * All rights reserved.
       *
       * Redistribution and use in source and binary forms, with or without
       * modification, are permitted provided that the following conditions are met:
       *  - Redistributions of source code must retain the above copyright
       *    notice, this list of conditions and the following disclaimer.
       *  - Redistributions in binary form must reproduce the above copyright
       *    notice, this list of conditions and the following disclaimer in
       *    the documentation and/or other materials provided with the
       *    distribution.
       *  - Neither the name of Analog Devices, Inc. nor the names of its
       *    contributors may be used to endorse or promote products derived
       *    from this software without specific prior written permission.
       *  - The use of this software may or may not infringe the patent rights
       *    of one or more patent holders.  This license does not release you
       *    from the requirement that you obtain separate licenses from these
       *    patent holders to use this software.
       *  - Use of the software either in source or binary form, must be run
       *    on or directly connected to an Analog Devices Inc. component.
       *
       * THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR
       * IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT,
       * MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
       * IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT,
       * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
       * LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR
       * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER
       * CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
       * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
       * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
      *******************************************************************************/
      #include <stdio.h>
      #include <stdlib.h>
      #include <string.h>
      
      #include "xil_cache.h"
      
      #include "error.h"
      #include "util.h"
      #include "spi.h"
      
      #include "axi_adc_core.h"
      #include "axi_dac_core.h"
      #include "axi_dmac.h"
      
      #include "parameters.h"
      
      #ifdef IIO_SUPPORT
      #include "app_iio.h"
      #include "xil_cache.h"
      #endif
      
      #include "adrv9002.h"
      #include "adi_adrv9001.h"
      #include "adi_adrv9001_arm.h"
      #include "adi_adrv9001_radio.h"
      #include "adi_adrv9001_tx.h"
      
      int get_sampling_frequency(struct axi_adc *dev, uint32_t chan,
      			   uint64_t *sampling_freq_hz)
      {
      	if (!dev || !sampling_freq_hz)
      		return -EINVAL;
      
      	*sampling_freq_hz =
      		adrv9002_init_get()->rx.rxChannelCfg[chan].profile.rxOutputRate_Hz;
      	return SUCCESS;
      }
      
      int main(void)
      {
      	int ret;
      	struct adi_common_ApiVersion api_version;
      	struct adi_adrv9001_ArmVersion arm_version;
      	struct adi_adrv9001_SiliconVersion silicon_version;
      	struct adrv9002_rf_phy phy;
      
      	struct axi_adc_init rx1_adc_init = {
      		"axi-adrv9002-rx-lpc",
      		RX1_ADC_BASEADDR,
      #ifndef ADRV9002_RX2TX2
      		ADRV9001_NUM_SUBCHANNELS,
      #else
      		ADRV9001_NUM_CHANNELS,
      #endif
      	};
      
      	struct axi_dac_channel  tx1_dac_channels[2];
      	tx1_dac_channels[0].sel = AXI_DAC_DATA_SEL_DMA;
      	tx1_dac_channels[1].sel = AXI_DAC_DATA_SEL_DMA;
      
      	struct axi_dac_init tx1_dac_init = {
      		"axi-adrv9002-tx-lpc",
      		TX1_DAC_BASEADDR,
      #ifndef ADRV9002_RX2TX2
      		ADRV9001_NUM_SUBCHANNELS,
      #else
      		ADRV9001_NUM_CHANNELS,
      #endif
      		tx1_dac_channels,
      	};
      
      #ifndef ADRV9002_RX2TX2
      	struct axi_adc_init rx2_adc_init = {
      		"axi-adrv9002-rx2-lpc",
      		RX2_ADC_BASEADDR,
      		ADRV9001_NUM_SUBCHANNELS,
      	};
      
      	struct axi_dac_channel  tx2_dac_channels[2];
      	tx2_dac_channels[0].sel = AXI_DAC_DATA_SEL_DMA;
      	tx2_dac_channels[1].sel = AXI_DAC_DATA_SEL_DMA;
      
      	struct axi_dac_init tx2_dac_init = {
      		"axi-adrv9002-tx2-lpc",
      		TX2_DAC_BASEADDR,
      		ADRV9001_NUM_SUBCHANNELS,
      		tx2_dac_channels,
      	};
      #endif
      	struct axi_dmac_init rx1_dmac_init = {
      		"rx_dmac",
      		RX1_DMA_BASEADDR,
      		DMA_DEV_TO_MEM,
      		0
      	};
      
      	struct axi_dmac_init tx1_dmac_init = {
      		"tx_dmac",
      		TX1_DMA_BASEADDR,
      		DMA_MEM_TO_DEV,
      		DMA_CYCLIC,
      	};
      
      #ifndef ADRV9002_RX2TX2
      	struct axi_dmac_init rx2_dmac_init = {
      		"rx_dmac",
      		RX2_DMA_BASEADDR,
      		DMA_DEV_TO_MEM,
      		0
      	};
      
      	struct axi_dmac_init tx2_dmac_init = {
      		"tx_dmac",
      		TX2_DMA_BASEADDR,
      		DMA_MEM_TO_DEV,
      		DMA_CYCLIC,
      	};
      #endif
      
      	Xil_ICacheEnable();
      	Xil_DCacheEnable();
      
      	printf("Hello\n");
      
      	memset(&phy, 0, sizeof(struct adrv9002_rf_phy));
      
      #if defined(ADRV9002_RX2TX2)
      	phy.rx2tx2 = true;
      #endif
      
      	ret = adrv9002_setup(&phy, adrv9002_init_get());
      	if (ret)
      		return ret;
      
      	adi_adrv9001_ApiVersion_Get(phy.adrv9001, &api_version);
      	adi_adrv9001_arm_Version(phy.adrv9001, &arm_version);
      	adi_adrv9001_SiliconVersion_Get(phy.adrv9001, &silicon_version);
      
      	printf("%s Rev %d.%d, Firmware %u.%u.%u.%u API version: %u.%u.%u successfully initialized\n",
      	       "ADRV9002", silicon_version.major, silicon_version.minor,
      	       arm_version.majorVer, arm_version.minorVer,
      	       arm_version.maintVer, arm_version.rcVer, api_version.major,
      	       api_version.minor, api_version.patch);
      
      	/* Initialize the ADC/DAC cores */
      	ret = axi_adc_init(&phy.rx1_adc, &rx1_adc_init);
      	if (ret) {
      		printf("axi_adc_init() failed with status %d\n", ret);
      		goto error;
      	}
      
      	ret = axi_dac_init(&phy.tx1_dac, &tx1_dac_init);
      	if (ret) {
      		printf("axi_dac_init() failed with status %d\n", ret);
      		goto error;
      	}
      	phy.tx1_dac->clock_hz = adrv9002_init_get()->tx.txProfile[0].txInputRate_Hz;
      #ifndef ADRV9002_RX2TX2
      	ret = axi_adc_init(&phy.rx2_adc, &rx2_adc_init);
      	if (ret) {
      		printf("axi_adc_init() failed with status %d\n", ret);
      		goto error;
      	}
      
      	ret = axi_dac_init(&phy.tx2_dac, &tx2_dac_init);
      	if (ret) {
      		printf("axi_dac_init() failed with status %d\n", ret);
      		goto error;
      	}
      	phy.tx2_dac->clock_hz = adrv9002_init_get()->tx.txProfile[1].txInputRate_Hz;
      #endif
      
      	/* Post AXI DAC/ADC setup, digital interface tuning */
      	ret = adrv9002_post_setup(&phy);
      	if (ret) {
      		printf("adrv9002_post_setup() failed with status %d\n", ret);
      		goto error;
      	}
      
      	/* TODO: Remove this when it gets fixed in the API. */
      	adi_adrv9001_Radio_Channel_ToState(phy.adrv9001, ADI_RX,
      					   ADI_CHANNEL_1, ADI_ADRV9001_CHANNEL_PRIMED);
      	adi_adrv9001_Radio_Channel_ToState(phy.adrv9001, ADI_RX,
      					   ADI_CHANNEL_1, ADI_ADRV9001_CHANNEL_RF_ENABLED);
      	adi_adrv9001_Radio_Channel_ToState(phy.adrv9001, ADI_RX,
      					   ADI_CHANNEL_2, ADI_ADRV9001_CHANNEL_PRIMED);
      	adi_adrv9001_Radio_Channel_ToState(phy.adrv9001, ADI_RX,
      					   ADI_CHANNEL_2, ADI_ADRV9001_CHANNEL_RF_ENABLED);
      
      	/* Initialize the AXI DMA Controller cores */
      	ret = axi_dmac_init(&phy.tx1_dmac, &tx1_dmac_init);
      	if (ret) {
      		printf("axi_dmac_init() failed with status %d\n", ret);
      		goto error;
      	}
      
      	ret = axi_dmac_init(&phy.rx1_dmac, &rx1_dmac_init);
      	if (ret) {
      		printf("axi_dmac_init() failed with status %d\n", ret);
      		goto error;
      	}
      #ifndef ADRV9002_RX2TX2
      	ret = axi_dmac_init(&phy.tx2_dmac, &tx2_dmac_init);
      	if (ret) {
      		printf("axi_dmac_init() failed with status %d\n", ret);
      		goto error;
      	}
      
      	ret = axi_dmac_init(&phy.rx2_dmac, &rx2_dmac_init);
      	if (ret) {
      		printf("axi_dmac_init() failed with status %d\n", ret);
      		goto error;
      	}
      #endif
      
      	//adi_adrv9001_Radio_Channel_ToRfEnabled(&phy.adrv9001, 1, 0x2);
      	//adi_adrv9001_Tx_AttenuationMode_Set(&phy.adrv9001,0x1, 1);
      	//adi_adrv9001_Tx_Attenuation_Set(&phy.adrv9001, 0x1, 20000 );
      
      
      #ifdef DAC_DMA_EXAMPLE
      	axi_dac_load_custom_data(phy.tx1_dac, sine_lut_iq,
      				 ARRAY_SIZE(sine_lut_iq),
      				 DAC1_DDR_BASEADDR);
      #ifndef ADRV9002_RX2TX2
      	axi_dac_load_custom_data(phy.tx2_dac, sine_lut_iq,
      				 ARRAY_SIZE(sine_lut_iq),
      				 DAC2_DDR_BASEADDR);
      #endif
      	Xil_DCacheFlush();
      
      	axi_dmac_transfer(phy.tx1_dmac, DAC1_DDR_BASEADDR, sizeof(sine_lut_iq));
      #ifndef ADRV9002_RX2TX2
      	axi_dmac_transfer(phy.tx2_dmac, DAC2_DDR_BASEADDR, sizeof(sine_lut_iq));
      #endif
      
      	mdelay(1000);
      
      	/* Transfer 16384 samples from ADC to MEM */
      	axi_dmac_transfer(phy.rx1_dmac,
      			  ADC1_DDR_BASEADDR,
      			  16384 * /* nr of samples */
      #ifndef ADRV9002_RX2TX2
      			  ADRV9001_NUM_SUBCHANNELS * /* rx1 i/q */
      #else
      			  ADRV9001_NUM_CHANNELS * /* rx1 i/q, rx2 i/q*/
      #endif
      			  2 /* bytes per sample */);
      	Xil_DCacheInvalidateRange(ADC1_DDR_BASEADDR,
      				  16384 * /* nr of samples */
      #ifndef ADRV9002_RX2TX2
      				  ADRV9001_NUM_SUBCHANNELS * /* rx1 i/q */
      #else
      				  ADRV9001_NUM_CHANNELS * /* rx1 i/q, rx2 i/q*/
      #endif
      				  2 /* bytes per sample */);
      #ifndef ADRV9002_RX2TX2
      	axi_dmac_transfer(phy.rx2_dmac,
      			  ADC2_DDR_BASEADDR,
      			  16384 * /* nr of samples */
      			  ADRV9001_NUM_SUBCHANNELS * /* nr of channels */
      			  2 /* bytes per sample */);
      	Xil_DCacheInvalidateRange(ADC2_DDR_BASEADDR,
      				  16384 * /* nr of samples */
      				  ADRV9001_NUM_SUBCHANNELS * /* nr of channels */
      				  2 /* bytes per sample */);
      #endif
      #endif
      
      #ifdef IIO_SUPPORT
      	printf("The board accepts libiio clients connections through the serial backend.\n");
      
      	struct iio_axi_adc_init_param iio_axi_adc1_init_par = {
      		.rx_adc = phy.rx1_adc,
      		.rx_dmac = phy.rx1_dmac,
      		.dcache_invalidate_range = (void (*)(uint32_t, uint32_t))Xil_DCacheInvalidateRange,
      		.get_sampling_frequency = get_sampling_frequency,
      	};
      
      	struct iio_axi_dac_init_param iio_axi_dac1_init_par = {
      		.tx_dac = phy.tx1_dac,
      		.tx_dmac = phy.tx1_dmac,
      		.dcache_flush_range = (void (*)(uint32_t, uint32_t))Xil_DCacheFlushRange,
      	};
      #ifndef ADRV9002_RX2TX2
      	struct iio_axi_adc_init_param iio_axi_adc2_init_par = {
      		.rx_adc = phy.rx2_adc,
      		.rx_dmac = phy.rx2_dmac,
      		.dcache_invalidate_range = (void (*)(uint32_t, uint32_t))Xil_DCacheInvalidateRange,
      		.get_sampling_frequency = get_sampling_frequency,
      	};
      
      	struct iio_axi_dac_init_param iio_axi_dac2_init_par = {
      		.tx_dac = phy.tx2_dac,
      		.tx_dmac = phy.tx2_dmac,
      		.dcache_flush_range = (void (*)(uint32_t, uint32_t))Xil_DCacheFlushRange,
      	};
      	ret = iio_server_init(&iio_axi_adc1_init_par,
      			      &iio_axi_adc2_init_par,
      			      &iio_axi_dac1_init_par,
      			      &iio_axi_dac2_init_par);
      #else
      	ret = iio_server_init(&iio_axi_adc1_init_par,
      			      NULL,
      			      &iio_axi_dac1_init_par,
      			      NULL);
      #endif
      #endif
      	printf("Bye\n");
      
      
      
      
      
      error:
      	adi_adrv9001_HwClose(phy.adrv9001);
      	axi_adc_remove(phy.rx1_adc);
      	axi_dac_remove(phy.tx1_dac);
      	axi_adc_remove(phy.rx2_adc);
      	axi_dac_remove(phy.tx2_dac);
      	axi_dmac_remove(phy.rx1_dmac);
      	axi_dmac_remove(phy.tx1_dmac);
      	axi_dmac_remove(phy.rx2_dmac);
      	axi_dmac_remove(phy.tx2_dmac);
      	return ret;
      }
      


      Headless_2022:

      /***************************************************************************//**
       *   @file   headless.c
       *   @brief  adrv9002 main project file.
       *   @author Darius Berghe (darius.berghe@analog.com)
      ********************************************************************************
       * Copyright 2020(c) Analog Devices, Inc.
       *
       * All rights reserved.
       *
       * Redistribution and use in source and binary forms, with or without
       * modification, are permitted provided that the following conditions are met:
       *  - Redistributions of source code must retain the above copyright
       *    notice, this list of conditions and the following disclaimer.
       *  - Redistributions in binary form must reproduce the above copyright
       *    notice, this list of conditions and the following disclaimer in
       *    the documentation and/or other materials provided with the
       *    distribution.
       *  - Neither the name of Analog Devices, Inc. nor the names of its
       *    contributors may be used to endorse or promote products derived
       *    from this software without specific prior written permission.
       *  - The use of this software may or may not infringe the patent rights
       *    of one or more patent holders.  This license does not release you
       *    from the requirement that you obtain separate licenses from these
       *    patent holders to use this software.
       *  - Use of the software either in source or binary form, must be run
       *    on or directly connected to an Analog Devices Inc. component.
       *
       * THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR
       * IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT,
       * MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
       * IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT,
       * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
       * LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR
       * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER
       * CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
       * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
       * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
      *******************************************************************************/
      #include <stdio.h>
      #include <stdlib.h>
      #include <string.h>
      #include <inttypes.h>
      #include <stdint.h>
      
      #ifdef XILINX_PLATFORM
      #include "xil_cache.h"
      #endif /* XILINX_PLATFORM */
      
      #include "no_os_error.h"
      #include "no_os_util.h"
      #include "no_os_spi.h"
      
      #include "axi_adc_core.h"
      #include "axi_dac_core.h"
      #include "axi_dmac.h"
      
      #include "parameters.h"
      
      #ifdef IIO_SUPPORT
      #include "iio_app.h"
      #include "iio_axi_adc.h"
      #include "iio_axi_dac.h"
      #include "xilinx_uart.h"
      #endif
      
      #include "adrv9002.h"
      #include "adi_adrv9001.h"
      #include "adi_adrv9001_arm.h"
      #include "adi_adrv9001_radio.h"
      #include "adi_adrv9001_profileutil.h"
      //#include "Navassa_CMOS_profile.h"
      #include "Navassa_LVDS_profile.h"
      
      /* ADC/DAC Buffers */
      #if defined(DMA_EXAMPLE) || defined(IIO_SUPPORT)
      static uint32_t dac_buffers[IIO_DEV_COUNT][DAC_BUFFER_SAMPLES]
      __attribute__((aligned));
      static uint16_t adc_buffers[IIO_DEV_COUNT][ADC_BUFFER_SAMPLES]
      __attribute__((aligned));
      #endif
      
      uint64_t sampling_freq;
      
      int get_sampling_frequency(struct axi_adc *dev, uint32_t chan,
      			   uint64_t *sampling_freq_hz)
      {
      	if (!dev || !sampling_freq_hz)
      		return -EINVAL;
      
      	*sampling_freq_hz = sampling_freq;
      	return 0;
      }
      
      static struct adi_adrv9001_SpiSettings spiSettings = {
      	.msbFirst = 1,
      	.enSpiStreaming = 0,
      	.autoIncAddrUp = 1,
      	.fourWireMode = 1,
      	.cmosPadDrvStrength = ADI_ADRV9001_CMOSPAD_DRV_STRONG,
      };
      
      struct adi_adrv9001_SpiSettings *adrv9002_spi_settings_get(void)
      {
      	return &spiSettings;
      }
      
      enum adi_adrv9001_SsiType adrv9002_ssi_type_detect(struct adrv9002_rf_phy *phy)
      {
      	enum adi_adrv9001_SsiType ssi, ssi2;
      	char *ssi_str[3] = {
      		"[SSI Disabled]",
      		"CMOS",
      		"LVDS"
      	};
      
      	ssi = adrv9002_axi_ssi_type_get(phy);
      
      	ssi2 = phy->curr_profile->rx.rxChannelCfg[0].profile.rxSsiConfig.ssiType;
      	if (ssi != ssi2) {
      		printf("SSI mismatch: detected %s in HDL and %s in profile.\n", ssi_str[ssi],
      		       ssi_str[ssi2]);
      		return ADI_ADRV9001_SSI_TYPE_DISABLE;
      	}
      
      	return ssi;
      }
      
      static struct adi_adrv9001_GainControlCfg agc_defaults = {
      	.peakWaitTime = 4,
      	.maxGainIndex = ADI_ADRV9001_RX_GAIN_INDEX_MAX,
      	.minGainIndex = ADI_ADRV9001_RX_GAIN_INDEX_MIN,
      	.gainUpdateCounter = 11520,
      	.attackDelay_us = 10,
      	.lowThreshPreventGainInc = false,
      	.slowLoopSettlingDelay = 16,
      	.changeGainIfThreshHigh = 3,
      	.agcMode = 1,
      	.resetOnRxon = false,
      	.resetOnRxonGainIndex = ADI_ADRV9001_RX_GAIN_INDEX_MAX,
      	.enableSyncPulseForGainCounter = false,
      	.enableFastRecoveryLoop = false,
      	.power = {
      		.powerEnableMeasurement = true,
      		.underRangeHighPowerThresh = 10,
      		.underRangeLowPowerThresh = 4,
      		.underRangeHighPowerGainStepRecovery = 2,
      		.underRangeLowPowerGainStepRecovery = 4,
      		.powerMeasurementDuration = 10,
      		.powerMeasurementDelay = 2,
      		.rxTddPowerMeasDuration = 0,
      		.rxTddPowerMeasDelay = 0,
      		.overRangeHighPowerThresh = 0,
      		.overRangeLowPowerThresh = 7,
      		.overRangeHighPowerGainStepAttack = 4,
      		.overRangeLowPowerGainStepAttack = 4,
      		.feedback_inner_high_inner_low = ADI_ADRV9001_GPIO_PIN_CRUMB_UNASSIGNED,
      		.feedback_apd_high_apd_low = ADI_ADRV9001_GPIO_PIN_CRUMB_UNASSIGNED,
      	},
      	.peak = {
      		.agcUnderRangeLowInterval = 50,
      		.agcUnderRangeMidInterval = 2,
      		.agcUnderRangeHighInterval = 4,
      		.apdHighThresh = 21,
      		.apdLowThresh = 12,
      		.apdUpperThreshPeakExceededCount = 6,
      		.apdLowerThreshPeakExceededCount = 3,
      		.apdGainStepAttack = 2,
      		.apdGainStepRecovery = 0,
      		.enableHbOverload = true,
      		.hbOverloadDurationCount = 1,
      		.hbOverloadThreshCount = 1,
      		.hbHighThresh = 13044,
      		.hbUnderRangeLowThresh = 5826,
      		.hbUnderRangeMidThresh = 8230,
      		.hbUnderRangeHighThresh = 7335,
      		.hbUpperThreshPeakExceededCount = 6,
      		.hbUnderRangeHighThreshExceededCount = 3,
      		.hbGainStepHighRecovery = 2,
      		.hbGainStepLowRecovery = 6,
      		.hbGainStepMidRecovery = 4,
      		.hbGainStepAttack = 2,
      		.hbOverloadPowerMode = 0,
      		.hbUnderRangeMidThreshExceededCount = 3,
      		.hbUnderRangeLowThreshExceededCount = 3,
      		.feedback_apd_low_hb_low = ADI_ADRV9001_GPIO_PIN_CRUMB_UNASSIGNED,
      		.feedback_apd_high_hb_high = ADI_ADRV9001_GPIO_PIN_CRUMB_UNASSIGNED,
      	},
      };
      
      #ifdef IIO_SUPPORT
      
      static int32_t iio_run(struct iio_axi_adc_init_param *adc_pars,
      		       struct iio_axi_dac_init_param *dac_pars)
      {
      	struct iio_axi_adc_desc *adcs[IIO_DEV_COUNT];
      	struct iio_axi_dac_desc *dacs[IIO_DEV_COUNT];
      	struct iio_data_buffer iio_dac_buffers[IIO_DEV_COUNT];
      	struct iio_data_buffer iio_adc_buffers[IIO_DEV_COUNT];
      	struct iio_device *iio_descs[IIO_DEV_COUNT * 2];
      	struct iio_app_device app_devices[IIO_DEV_COUNT * 2] = {0};
      	struct xil_uart_init_param platform_uart_init_par = {
      		.type = UART_PS,
      		.irq_id = UART_IRQ_ID
      	};
      
      	struct no_os_uart_init_param iio_uart_ip = {
      		.device_id = UART_DEVICE_ID,
      		.irq_id = UART_IRQ_ID,
      		.baud_rate = UART_BAUDRATE,
      		.size = NO_OS_UART_CS_8,
      		.parity = NO_OS_UART_PAR_NO,
      		.stop = NO_OS_UART_STOP_1_BIT,
      		.extra = &platform_uart_init_par,
      		.platform_ops = &xil_uart_ops
      	};
      
      	struct iio_app_desc *app;
      	struct iio_app_init_param app_init_param = { 0 };
      	int32_t i, ret;
      	int32_t a; // linear iterator for iio_descs and app_devices flat arrays
      
      	for (i = 0; i < IIO_DEV_COUNT; i++) {
      		/* ADC setup */
      		iio_adc_buffers[i].buff = adc_buffers[i];
      		iio_adc_buffers[i].size = sizeof(adc_buffers[i]);
      		ret = iio_axi_adc_init(&adcs[i], &adc_pars[i]);
      		if (ret < 0)
      			return ret;
      		a = 2 * i;
      		iio_axi_adc_get_dev_descriptor(adcs[i], &iio_descs[a]);
      		app_devices[a].name = adc_pars[i].rx_adc->name;
      		app_devices[a].dev = adcs[i];
      		app_devices[a].dev_descriptor = iio_descs[a];
      		app_devices[a].read_buff = &iio_adc_buffers[i];
      
      		/* DAC setup */
      		iio_dac_buffers[i].buff = dac_buffers[i];
      		iio_dac_buffers[i].size = sizeof(dac_buffers[i]);
      		ret = iio_axi_dac_init(&dacs[i], &dac_pars[i]);
      		if (ret < 0)
      			return ret;
      		a = 2 * i + 1;
      		iio_axi_dac_get_dev_descriptor(dacs[i], &iio_descs[a]);
      		app_devices[a].name = dac_pars[i].tx_dac->name;
      		app_devices[a].dev = dacs[i];
      		app_devices[a].dev_descriptor = iio_descs[a];
      		app_devices[a].write_buff = &iio_dac_buffers[i];
      	}
      
      	app_init_param.devices = app_devices;
      	app_init_param.nb_devices = NO_OS_ARRAY_SIZE(app_devices);
      	app_init_param.uart_init_params = iio_uart_ip;
      
      	ret = iio_app_init(&app, app_init_param);
      	if (ret)
      		return ret;
      
      	return iio_app_run(app);
      }
      #endif
      
      int main(void)
      {
      	int ret;
      	struct adi_common_ApiVersion api_version;
      	struct adi_adrv9001_ArmVersion arm_version;
      	struct adi_adrv9001_SiliconVersion silicon_version;
      	struct adi_adrv9001_Device adrv9001_device = {0};
      	struct adrv9002_chip_info chip = {0};
      	struct adrv9002_rf_phy phy = {0};
      	unsigned int c;
      
      	struct axi_adc_init rx1_adc_init = {
      		.name = "axi-adrv9002-rx-lpc",
      		.base = RX1_ADC_BASEADDR,
      		.num_channels = ADRV9001_I_Q_CHANNELS,
      	};
      
      	struct axi_dac_channel  tx1_dac_channels[2];
      	tx1_dac_channels[0].sel = AXI_DAC_DATA_SEL_DDS ;// AXI_DAC_DATA_SEL_DMA;
      	tx1_dac_channels[1].sel = AXI_DAC_DATA_SEL_DDS;
      
      	struct axi_dac_init tx1_dac_init = {
      		.name = "axi-adrv9002-tx-lpc",
      		.base = TX1_DAC_BASEADDR,
      		.num_channels = ADRV9001_I_Q_CHANNELS,
      		.channels = tx1_dac_channels,
      		.rate = 3
      	};
      
      #ifndef ADRV9002_RX2TX2
      	struct axi_adc_init rx2_adc_init = {
      		.name = "axi-adrv9002-rx2-lpc",
      		.base = RX2_ADC_BASEADDR,
      		.num_channels = ADRV9001_I_Q_CHANNELS,
      	};
      
      	struct axi_dac_channel  tx2_dac_channels[2];
      	tx2_dac_channels[0].sel = AXI_DAC_DATA_SEL_DMA;
      	tx2_dac_channels[1].sel = AXI_DAC_DATA_SEL_DMA;
      
      	struct axi_dac_init tx2_dac_init = {
      		.name = "axi-adrv9002-tx2-lpc",
      		.base = TX2_DAC_BASEADDR,
      		.num_channels = ADRV9001_I_Q_CHANNELS,
      		.channels = tx2_dac_channels,
      		.rate = 3
      	};
      #endif
      	struct axi_dmac_init rx1_dmac_init = {
      		"rx_dmac",
      		RX1_DMA_BASEADDR,
      		IRQ_DISABLED
      	};
      
      	struct axi_dmac_init tx1_dmac_init = {
      		"tx_dmac",
      		TX1_DMA_BASEADDR,
      		IRQ_DISABLED
      	};
      
      #ifndef ADRV9002_RX2TX2
      	struct axi_dmac_init rx2_dmac_init = {
      		"rx_dmac",
      		RX2_DMA_BASEADDR,
      		IRQ_DISABLED
      	};
      
      	struct axi_dmac_init tx2_dmac_init = {
      		"tx_dmac",
      		TX2_DMA_BASEADDR,
      		IRQ_DISABLED
      	};
      #endif
      
      #ifdef XILINX_PLATFORM
      	Xil_ICacheEnable();
      	Xil_DCacheEnable();
      #endif /* XILINX_PLATFORM */
      
      	printf("Hello\n");
      
      #if defined(ADRV9002_RX2TX2)
      	phy.rx2tx2 = true;
      #endif
      
      	phy.adrv9001 = &adrv9001_device;
      
      	/* ADRV9002 */
      	chip.cmos_profile = "Navassa_CMOS_profile.json";
      	chip.lvd_profile = "Navassa_LVDS_profile.json";
      	chip.name = "adrv9002-phy";
      	chip.n_tx = ADRV9002_CHANN_MAX;
      
      	phy.chip = &chip;
      
      	ret = adi_adrv9001_profileutil_Parse(phy.adrv9001, &phy.profile,
      					     (char *)json_profile, strlen(json_profile));
      	if (ret)
      		goto error;
      
      	phy.curr_profile = &phy.profile;
      
      	sampling_freq = phy.curr_profile->rx.rxChannelCfg[0].profile.rxOutputRate_Hz;
      	printf("%" PRIu64 "\n", sampling_freq);
      
      	/* Initialize the ADC/DAC cores */
      	ret = axi_adc_init_begin(&phy.rx1_adc, &rx1_adc_init);
      	if (ret) {
      		printf("axi_adc_init_begin() failed with status %d\n", ret);
      		goto error;
      	}
      
      	ret = axi_dac_init_begin(&phy.tx1_dac, &tx1_dac_init);
      	if (ret) {
      		printf("axi_dac_init_begin() failed with status %d\n", ret);
      		goto error;
      	}
      #ifndef ADRV9002_RX2TX2
      	ret = axi_adc_init_begin(&phy.rx2_adc, &rx2_adc_init);
      	if (ret) {
      		printf("axi_adc_init_begin() failed with status %d\n", ret);
      		goto error;
      	}
      
      	ret = axi_dac_init_begin(&phy.tx2_dac, &tx2_dac_init);
      	if (ret) {
      		printf("axi_dac_init_begin() failed with status %d\n", ret);
      		goto error;
      	}
      #endif
      
      	phy.ssi_type = adrv9002_ssi_type_detect(&phy);
      	if (phy.ssi_type == ADI_ADRV9001_SSI_TYPE_DISABLE)
      		goto error;
      
      	/* Initialize AGC */
      	for (c = 0; c < ADRV9002_CHANN_MAX; c++) {
      		phy.rx_channels[c].agc = agc_defaults;
      	}
      
      	ret = adrv9002_setup(&phy);
      	if (ret)
      		return ret;
      
      	adi_adrv9001_ApiVersion_Get(phy.adrv9001, &api_version);
      	adi_adrv9001_arm_Version(phy.adrv9001, &arm_version);
      	adi_adrv9001_SiliconVersion_Get(phy.adrv9001, &silicon_version);
      
      	printf("%s Rev %d.%d, Firmware %u.%u.%u.%u API version: %u.%u.%u successfully initialized\n",
      	       "ADRV9002", silicon_version.major, silicon_version.minor,
      	       arm_version.majorVer, arm_version.minorVer,
      	       arm_version.maintVer, arm_version.rcVer, api_version.major,
      	       api_version.minor, api_version.patch);
      
      	/* Post AXI DAC/ADC setup, digital interface tuning */
      	ret = adrv9002_post_setup(&phy);
      	if (ret) {
      		printf("adrv9002_post_setup() failed with status %d\n", ret);
      		goto error;
      	}
      
      	/* Finalize the ADC/DAC cores initialization */
      	ret = axi_adc_init_finish(phy.rx1_adc);
      	if (ret) {
      		printf("axi_adc_init_finish() failed with status %d\n", ret);
      		goto error;
      	}
      
      	ret = axi_dac_init_finish(phy.tx1_dac);
      	if (ret) {
      		printf("axi_dac_init_finish() failed with status %d\n", ret);
      		goto error;
      	}
      	phy.tx1_dac->clock_hz = phy.curr_profile->tx.txProfile[0].txInputRate_Hz;
      #ifndef ADRV9002_RX2TX2
      	ret = axi_adc_init_finish(phy.rx2_adc);
      	if (ret) {
      		printf("axi_adc_init_finish() failed with status %d\n", ret);
      		goto error;
      	}
      
      	ret = axi_dac_init_finish(phy.tx2_dac);
      	if (ret) {
      		printf("axi_dac_init_finish() failed with status %d\n", ret);
      		goto error;
      	}
      	phy.tx2_dac->clock_hz = phy.curr_profile->tx.txProfile[1].txInputRate_Hz;
      #endif
      
      	/* Initialize the AXI DMA Controller cores */
      	ret = axi_dmac_init(&phy.tx1_dmac, &tx1_dmac_init);
      	if (ret) {
      		printf("axi_dmac_init() failed with status %d\n", ret);
      		goto error;
      	}
      
      	ret = axi_dmac_init(&phy.rx1_dmac, &rx1_dmac_init);
      	if (ret) {
      		printf("axi_dmac_init() failed with status %d\n", ret);
      		goto error;
      	}
      #ifndef ADRV9002_RX2TX2
      	ret = axi_dmac_init(&phy.tx2_dmac, &tx2_dmac_init);
      	if (ret) {
      		printf("axi_dmac_init() failed with status %d\n", ret);
      		goto error;
      	}
      
      	ret = axi_dmac_init(&phy.rx2_dmac, &rx2_dmac_init);
      	if (ret) {
      		printf("axi_dmac_init() failed with status %d\n", ret);
      		goto error;
      	}
      #endif
      
      #ifdef DMA_EXAMPLE
      	axi_dac_load_custom_data(phy.tx1_dac, sine_lut_iq,
      				 NO_OS_ARRAY_SIZE(sine_lut_iq),
      				 (uintptr_t)dac_buffers[0]);
      #ifndef ADRV9002_RX2TX2
      	axi_dac_load_custom_data(phy.tx2_dac, sine_lut_iq,
      				 NO_OS_ARRAY_SIZE(sine_lut_iq),
      				 (uintptr_t)dac_buffers[1]);
      #endif
      #ifdef XILINX_PLATFORM
      	Xil_DCacheFlush();
      #endif /* XILINX_PLATFORM */
      
      	struct axi_dma_transfer transfer1 = {
      		// Number of bytes to write/read
      		.size = sizeof(sine_lut_iq),
      		// Transfer done flag
      		.transfer_done = 0,
      		// Signal transfer mode
      		.cyclic = CYCLIC,
      		// Address of data source
      		.src_addr = (uintptr_t)dac_buffers[0],
      		// Address of data destination
      		.dest_addr = 0
      	};
      	axi_dmac_transfer_start(phy.tx1_dmac, &transfer1);
      #ifndef ADRV9002_RX2TX2
      	struct axi_dma_transfer transfer2 = {
      		// Number of bytes to write/read
      		.size = sizeof(sine_lut_iq),
      		// Transfer done flag
      		.transfer_done = 0,
      		// Signal transfer mode
      		.cyclic = CYCLIC,
      		// Address of data source
      		.src_addr = (uintptr_t)dac_buffers[1],
      		// Address of data destination
      		.dest_addr = 0
      	};
      	axi_dmac_transfer_start(phy.tx2_dmac, &transfer2);
      #endif
      
      #ifdef XILINX_PLATFORM
      	Xil_DCacheInvalidateRange((uintptr_t)adc_buffers[0], sizeof(sine_lut_iq));
      #ifndef ADRV9002_RX2TX2
      	Xil_DCacheInvalidateRange((uintptr_t)adc_buffers[1], sizeof(sine_lut_iq));
      #endif
      #endif /* XILINX_PLATFORM */
      
      	no_os_mdelay(1000);
      
      	struct axi_dma_transfer read_transfer1 = {
      		// Number of bytes to write/read
      		.size = ADC_BUFFER_SAMPLES * ADRV9001_I_Q_CHANNELS * 2, /* nr of samples * rx1 i/q, rx2 i/q * bytes per sample */
      		// Transfer done flag
      		.transfer_done = 0,
      		// Signal transfer mode
      		.cyclic = NO,
      		// Address of data source
      		.src_addr = 0,
      		// Address of data destination
      		.dest_addr = (uintptr_t)adc_buffers[0]
      	};
      	/* Transfer ADC_BUFFER_SAMPLES samples from ADC to MEM */
      #ifdef ADRV9002_RX2TX2
      	axi_adc_update_active_channels(phy.rx1_adc, 0xf);
      #else
      	axi_adc_update_active_channels(phy.rx1_adc, 0x3);
      #endif
      	axi_dmac_transfer_start(phy.rx1_dmac, &read_transfer1);
      	ret = axi_dmac_transfer_wait_completion(phy.rx1_dmac, 500);
      	if(ret)
      		return ret;
      #ifdef XILINX_PLATFORM
      	Xil_DCacheInvalidateRange((uintptr_t)adc_buffers[0],
      				  ADC_BUFFER_SAMPLES * /* nr of samples */
      				  ADRV9001_I_Q_CHANNELS * /* rx1 i/q, rx2 i/q*/
      				  2 /* bytes per sample */);
      #endif /* XILINX_PLATFORM */
      #ifndef ADRV9002_RX2TX2
      	struct axi_dma_transfer read_transfer2 = {
      		// Number of bytes to write/read
      		.size = ADC_BUFFER_SAMPLES * ADRV9001_I_Q_CHANNELS * 2, /* nr of samples * rx1 i/q, rx2 i/q * bytes per sample */
      		// Transfer done flag
      		.transfer_done = 0,
      		// Signal transfer mode
      		.cyclic = NO,
      		// Address of data source
      		.src_addr = 0,
      		// Address of data destination
      		.dest_addr = (uintptr_t)adc_buffers[1]
      	};
      	axi_adc_update_active_channels(phy.rx2_adc, 0x3);
      	axi_dmac_transfer_start(phy.rx2_dmac,&read_transfer2);
      	ret = axi_dmac_transfer_wait_completion(phy.rx2_dmac, 500);
      	if(ret)
      		return ret;
      #ifdef XILINX_PLATFORM
      	Xil_DCacheInvalidateRange((uintptr_t)adc_buffers[1],
      				  ADC_BUFFER_SAMPLES * /* nr of samples */
      				  ADRV9001_I_Q_CHANNELS * /* nr of channels */
      				  2 /* bytes per sample */);
      #endif /* XILINX_PLATFORM */
      	printf("DMA_EXAMPLE: address=%#lx samples=%lu channels=%u bits=%lu\n",
      	       (uintptr_t)adc_buffers[1], ADC_BUFFER_SAMPLES * rx2_adc_init.num_channels,
      	       rx2_adc_init.num_channels, 8 * sizeof(adc_buffers[1][0]));
      #endif
      	printf("DMA_EXAMPLE: address=%#lx samples=%lu channels=%u bits=%lu\n",
      	       (uintptr_t)adc_buffers[0], ADC_BUFFER_SAMPLES * rx1_adc_init.num_channels,
      	       rx1_adc_init.num_channels, 8 * sizeof(adc_buffers[0][0]));
      #endif
      
      #ifdef IIO_SUPPORT
      	struct iio_axi_adc_init_param iio_axi_adcs_init_par[] = {{
      			.rx_adc = phy.rx1_adc,
      			.rx_dmac = phy.rx1_dmac,
      #ifdef XILINX_PLATFORM
      			.dcache_invalidate_range = (void (*)(uint32_t, uint32_t))Xil_DCacheInvalidateRange,
      #endif /* XILINX_PLATFORM */
      			.get_sampling_frequency = get_sampling_frequency,
      		},
      #ifndef ADRV9002_RX2TX2
      		{
      			.rx_adc = phy.rx2_adc,
      			.rx_dmac = phy.rx2_dmac,
      #ifdef XILINX_PLATFORM
      			.dcache_invalidate_range = (void (*)(uint32_t, uint32_t))Xil_DCacheInvalidateRange,
      #endif /* XILINX_PLATFORM */
      			.get_sampling_frequency = get_sampling_frequency,
      		}
      #endif
      	};
      
      	struct iio_axi_dac_init_param iio_axi_dacs_init_par[] = {{
      			.tx_dac = phy.tx1_dac,
      			.tx_dmac = phy.tx1_dmac,
      #ifdef XILINX_PLATFORM
      			.dcache_flush_range = (void (*)(uint32_t, uint32_t))Xil_DCacheFlushRange,
      #endif /* XILINX_PLATFORM */
      		},
      #ifndef ADRV9002_RX2TX2
      		{
      			.tx_dac = phy.tx2_dac,
      			.tx_dmac = phy.tx2_dmac,
      #ifdef XILINX_PLATFORM
      			.dcache_flush_range = (void (*)(uint32_t, uint32_t))Xil_DCacheFlushRange,
      #endif /* XILINX_PLATFORM */
      		}
      #endif
      	};
      
      	ret = iio_run(iio_axi_adcs_init_par, iio_axi_dacs_init_par);
      	if (ret < 0) {
      		printf("iio_run() failed with status %d\n", ret);
      		goto error;
      	}
      #endif
      	printf("Bye\n");
      
      error:
      	adi_adrv9001_HwClose(phy.adrv9001);
      	axi_adc_remove(phy.rx1_adc);
      	axi_dac_remove(phy.tx1_dac);
      	axi_adc_remove(phy.rx2_adc);
      	axi_dac_remove(phy.tx2_dac);
      	axi_dmac_remove(phy.rx1_dmac);
      	axi_dmac_remove(phy.tx1_dmac);
      	axi_dmac_remove(phy.rx2_dmac);
      	axi_dmac_remove(phy.tx2_dmac);
      	return ret;
      }
      


      Vitis/SDK prints:

  • Hello, 

    Could you please open a new EZ thread regarding this topic? This seems to be a different issue not related to the initial no-Os driver not building. Therefore, we can consider this thread closed.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.