Post Go back to editing

How to change the sampling rate of FMCOMMS3 + ZCU104 (NO OS)

Thread Summary

The user is configuring the FMCOMMS3 + ZCU104 setup to run at 1.28 MSamples/s for baseband signal processing. The final answer confirms that no HDL changes are needed, and the user should update the no-OS configuration with the exported filter coefficients and settings. The ADC/DAC runs at 61.44 MSamples/s, and the analog filter cutoff frequency (0.85391 MHz) should be updated using the `ad9361_set_tx_rf_bandwidth` function if necessary.
AI Generated Content
Category: Software
Software Version: 2024.1

Hi,

My setup is FMCOMMS3 + ZCU104.

For HDL, I started from the FMCOMMS3 + ZCU102 and modified the HDL to suit ZCU104.

For software, I am using no OS of AD9361 and I am using the DMA example. Again, I have modified the no OS to suit ZCU104. The default example works fine.

I would like to implement a waveform and run the baseband signal processing of the Tx and Rx at 1.28Msamples/s. The default sampling rate in the example I am using is 30.72 MSamples/s so I need to change it to 1.28MSamples/s.

I have been reading different Analog Devices docs and discussions in the forms about related topics. Here is the list of steps that I think I need to do. Could you please have a look at them and let me know if they are right or I am missing something?  Thank you!

Step 1- I used the Filter Wizard to configure the sampling rates and the filters of the Tx and Rx chains. Please, find attached the a screen shot of the filter wizard. 

Q1/ According to this configuration, I assume that the ADC/DAC runs at 61.44MSamples/s, right?

Q2/ I assume that the baseband logic runs at 1.28MSamples/s, right?

Step 2/

I have exported the coefficients and configs to no-OS and got the followings:

------------------------------

AD9361_RXFIRConfig rx_fir_config = {
    3, // rx
    -12, // rx_gain
    4, // rx_dec
    {100,-44,170,-17,122,-49,-17,-184,-204,-324,-308,-320,-212,-121,34,129,209,187,121,-24,-160,-284,-316,-269,-118,74,273,393,408,281,55,-224,-454,-569,-505,-273,83,448,714,773,586,177,-340,-815,-1080,-1024,-614,62,822,1426,1650,1350,531,-642,-1853,-2713,-2845,-1994,-102,2651,5867,9007,11503,12884,12884,11503,9007,5867,2651,-102,-1994,-2845,-2713,-1853,-642,531,1350,1650,1426,822,62,-614,-1024,-1080,-815,-340,177,586,773,714,448,83,-273,-505,-569,-454,-224,55,281,408,393,273,74,-118,-269,-316,-284,-160,-24,121,187,209,129,34,-121,-212,-320,-308,-324,-204,-184,-17,-49,122,-17,170,-44,100}, // rx_coef[128]
    128, // rx_coef_size
    {983040000,61440000,20480000,10240000,5120000,1280000}, // rx_path_clks[6]
    1068442 // rx_bandwidth
};

AD9361_TXFIRConfig tx_fir_config = {
    3, // tx
    0, // tx_gain
    4, // tx_int
    {27,-27,20,-62,-63,-158,-201,-290,-324,-355,-317,-253,-131,-5,128,212,246,201,101,-42,-176,-270,-283,-212,-63,117,281,369,350,215,-3,-245,-433,-503,-416,-186,133,445,650,666,467,89,-367,-762,-958,-865,-471,138,795,1292,1439,1126,369,-672,-1717,-2423,-2468,-1639,102,2588,5463,8254,10464,11685,11685,10464,8254,5463,2588,102,-1639,-2468,-2423,-1717,-672,369,1126,1439,1292,795,138,-471,-865,-958,-762,-367,89,467,666,650,445,133,-186,-416,-503,-433,-245,-3,215,350,369,281,117,-63,-212,-283,-270,-176,-42,101,201,246,212,128,-5,-131,-253,-317,-355,-324,-290,-201,-158,-63,-62,20,-27,27}, // tx_coef[128]
    128, // tx_coef_size
    {983040000,61440000,20480000,10240000,5120000,1280000}, // tx_path_clks[6]
    1255167 // tx_bandwidth
};

-------------------------------------------------------------

Q3/ I assume that I can use the above exported configs and coeffs to update "default_init_param" in main.c., right?

Q4/ In the exported coeffs and configs above, nothing covers updating the analog filter cut freq. According to the filter wizard GUI, the Fcutoff (analog) is 0.85391 MHz. Do I need to update it? How? Should I use "ad9361_seet_tx_rf_bandwidth" function call?

Q5/ Do I need to update anything in the HDL design in order to run the new sampling rate? Or it is going to be updated by the software changes I am making according to the steps above?

Q6/ In the HDL design, what is the new l_clk frequency?

Thread Notes

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.