Post Go back to editing

AD9434 FMC on ZedBoard – DMA capture completed but sampled data seems incorrect

Thread Summary

The user is experiencing issues with incorrect ADC data capture on a ZedBoard with an AD9434 FMC board, despite successful DMA transfer. The final answer suggests trying a clock frequency below 464 MHz, as the ZedBoard has a limitation on the BUFG input clock frequency. The accompanying answers note that the relevant support team is currently unavailable due to the holiday season and the thread has been moved to the Microcontroller no-OS Drivers forum for further support.
AI Generated Content
Category: Software
Product Number: AD9434BCPZ-370, AD9434
Software Version: Vitis 2023.2

Hello,

I am currently working on a project using a ZedBoard with an AD9434 FMC board and I am having an issue with the captured ADC data. I started this work by following the Analog Devices documentation available here:
https://analogdevicesinc.github.io/hdl/projects/ad9434_fmc/index.html
This page is what guided me to the HDL reference design used for this project.

I then used the official Analog Devices HDL project for the ZedBoard with Vivado 2023.2 on Linux:
https://github.com/analogdevicesinc/hdl/tree/main/projects/ad9434_fmc/zed

The bitstream was generated successfully and I exported the hardware including the bitstream, which produced an .xsa file.

On the software side, I am also using Vitis 2023.2 on Linux. I created a platform project from the generated .xsa file. For the application, I used the no-OS project provided by Analog Devices:
https://github.com/analogdevicesinc/no-OS/tree/main/projects/ad9434-fmc-500ebz/src

I built the project following the instructions from:
https://wiki.analog.com/resources/no-os/build

This allowed me to generate a valid .elf file. In Vitis, I used a simple example application (HelloWorld) and replaced its ELF file with the one generated by the no-OS build in order to run the application on the board.

For the ADC input, I am using a function generator with a sinusoidal signal at 20 MHz and 1.5 Vpp. The AD9434 is configured to use its internal clock at 500 MSPS (datasheet: https://www.analog.com/media/en/technical-documentation/data-sheets/ad9434.pdf).

The capture process seems to work correctly. In the terminal, I can see the “capture done” message at the end of the execution, which suggests that the DMA transfer completed successfully.

However, the captured values do not match what I expect at all. I added some debug code in the application just after the following line (around line 168 in the no-OS project):

Xil_DCacheInvalidateRange((uintptr_t)ADC_DDR_BASEADDR, 16384 * 2);

The purpose of this code is simply to read back the ADC samples written by the DMA into DDR and print some of them for inspection. The code I added is the following:

/* ## DISPLAY AD9434 ADC VALUES (12-bit two's complement) */

uint16_t *adc_data_ptr = (uint16_t *)ADC_DDR_BASEADDR;

uint32_t samples_to_display = 10600;

pr_info("----- START ADC DATA DISPLAY (12-bit Two's Complement) -----\n");

for (uint32_t i = 10000; i < samples_to_display; i++) {
        uint16_t raw_value = adc_data_ptr[i];
        raw_value &= 0x0FFF;
        int16_t raw_signed = (int16_t)(raw_value);
        int16_t final_sample;

        if (raw_value & 0x0800) {
                final_sample = (int16_t)(raw_value | 0xF000);
        } else {
                final_sample = (int16_t)raw_value;
        }

        pr_info("Sample[%lu] = %d (Raw hex: 0x%03X), raw dec = %d\n", i, final_sample, raw_value, raw_signed);
}
pr_info("----- END ADC DATA DISPLAY -----\n");

pr_info("ADC base address: %p\n", adc_data_ptr);

/* ## END DISPLAY */

The ADC base address printed by the software is:
ADC base address: 0x1000000

I also wrote a small Python script to plot the captured samples. Instead of obtaining a sine wave similar to the input signal, I get a completely incorrect waveform (see attached image). Moreover, when I change the input signal (frequency or amplitude), the output waveform remains almost the same. This makes me think that the values I am printing might not actually correspond to the real ADC samples, or that there is an issue with data format, alignment, or memory mapping.

At this point, I am not sure where the problem comes from or why I am not visualizing the correct ADC values. Any help or guidance on what to check next would be greatly appreciated.

Thank you.

Thread Notes

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.