Post Go back to editing

ADRV9026 no-OS project for ZCU102 on Windows (Vitis 2025.1) Error [PLM-2]/[PLM-3]

Thread Summary

The user encountered errors while building the ADRV9026 no-OS example project for the ZCU102 platform using Vitis 2025.1 on Windows. The issue was resolved by using the last Eclipse-based Vitis (2023.2) instead of the VS Code-based version. The user also tried setting the environment variable `ADI_IGNORE_VERSION_CHECK=1` to avoid version mismatch issues but still faced `make run` errors. Further assistance was requested to troubleshoot the `make run` errors.
AI Generated Content
Category: Software
Product Number: ADRV9026
Software Version: Vitis 2025.1

Hello,

I am trying to build the ADRV9026 no-OS example project for the ZCU102 platform on Windows using Vitis 2025.1.

  • I successfully built the HDL reference design and generated the bitstream (.xsa and .bit files).

  • Followed the official no-OS build guide: https://wiki.analog.com/resources/no-os/build.

  • no-OS repository is on the main branch (cloned with --recursive).

  • Verified all tools are installed and available in Git Bash: make, xsct, grep.

  • Environment variables are set by sourcing Vitis/settings64.sh.

  • Copied the system_top.xsa into no-OS/projects/adrv902x/.

  • Tried both .xsa files: one from the .sdk folder and one from “Export Bitstream.”

  • Verified by opening the .xsa in Vitis that it targets ZCU102, not Versal.'

    When I run make, I get this error:

    $ make
    [12:16:59] Building for xilinx
    [12:17:02] Creating and configuring the IDE project
    grep: /etc/os-release: No such file or directory
    grep: /etc/os-release: No such file or directory
    ERROR: [PLM-2] Libraries compilation failed during versal PLM application generation due to avbuf"
    ERROR: [PLM-3] Versal PLM application compilation failed
    ERROR: [Hsi 55-1450] Error: running generate_bsp.
    make[1]: *** [C:/VivadoProjects/adi/no-OS/tools/scripts/xilinx.mk:238: xilinx_project] Error 1
    make: *** [../../tools/scripts/generic.mk:273: all] Error 2
    I have asked before about which vivado/vitis version I should use to build the HDL reference design and I was told it's 2025.1. 
    Is this a known issue for Vitis 2025.1 and no-OS on windows? Any help will be much appreciated!
    Thank you,
    Best regards,
    Farouk

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.