Post Go back to editing

NO_OS Example for CN0585 using AD3552r driver

Category: Software
Product Number: CN0585

I'm having an issue using the no_os AD3552r example for the CN0585 design since there is no no_os project for CN0585. I get an error that the AD3552r is failing the scratch pad test. I ported the AD3552r_fmcz project for the CN0585 by updating the following base addresses and copying the CN0585 HDL xsa file into the project. Note this is just for the first AD3552r of the two for now. Any idea why my implementation wouldn't be talking to the AD3552r?

#define TX_CORE_BASEADDR XPAR_AXI_AD35XXR_0_BASEADDR
#define TX_DMA_BASEADDR XPAR_AXI_DAC_0_DMA_BASEADDR
#define TX_CLKGEN_BASEADDR XPAR_AXI_CLKGEN_BASEADDR

I'm also unsure how the GPIO bank indexes in the no_os driver relate to the zync pin numbers so I can update the reset and LDAC GPIO offsets accordingly. 

Parents
  • Hello,

    I'll try to cover the HDL side of your question.

    1) Can you give us more details about how exactly did you port the HDL design? What did you modify?

    2) Regarding the GPIO offset, check here, in the "GPIOs" subsection. The Zynq offset in no-os is +54.

    Regards,

    Stanca

  • I modified "parameters.h" to update the appropriate RESET, LDAC and ALERT pins for the CN0585 design based on that offset table you sent me. Also updated the base addresses as I mentioned in the original post. Updated common_data.c with the updated GPIO macros. Removed unnecessary LED functionality from ax_qspi_example.c. 

    I did get this hardware setup working with the iio_oscilloscope after getting the linux build and boot files loaded correctly for CN0585. Confirmed DACs are working.

Reply
  • I modified "parameters.h" to update the appropriate RESET, LDAC and ALERT pins for the CN0585 design based on that offset table you sent me. Also updated the base addresses as I mentioned in the original post. Updated common_data.c with the updated GPIO macros. Removed unnecessary LED functionality from ax_qspi_example.c. 

    I did get this hardware setup working with the iio_oscilloscope after getting the linux build and boot files loaded correctly for CN0585. Confirmed DACs are working.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.