Post Go back to editing
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

In the no os environment, when initializing AD9988 RX Link print the status sometimes in DATA sometimes in CGS and ILAS

Category: Software
Product Number: AD9988
Software Version: no-os r2021-1

In the no os environment, when initializing AD9988, the TX link can be configured normally every time, but sometimes the RX link may print and enter the DATA stage, and sometimes it may get stuck in the CGS and ILAS stages.

What is this related to?


I am using XILINX's IP and comparing two projects. One is the ADI project and the other is the project I built myself. The ADI project always enters the DATA phase correctly, but sometimes the project I built myself may not enter the DATA state.


What are the reasons that may affect me?

thanks a lot!

Edit Notes


[locked by: buha at 7:53 AM (GMT -5) on 4 Mar 2025]
Parents Reply Children
No Data