Post Go back to editing

ADRV9008-2 ORX at 491.42MSPS whit noise and DC

Thread Summary

The user encountered high noise and DC component issues when using ADRV9008-2 at 491.52 MSPS for ORX. The problem was resolved by using the main branch for both HDL and no-OS projects, setting the correct ORx FIR coefficients, and ensuring the ORx uses lanes 2 and 3 (FRAMER B settings). The final configuration file and stream binary provided by the support engineer resulted in the desired flat response over the 450 MHz band.
AI Generated Content
Category: Hardware
Product Number: ADRV9008-2

Hello,

I want to use ADRV9008-2 at 491.52 MSPS for TX and ORX.

I'm working on EVAL-TPG-ZYNQ3 + ADRV9008-2 W/PCBZ boards, with no-OS firmware.

If I look at the data received from ORX input I see some noise and a DC component quite high.

I already looked at "ADRV9008-2: problem with 491.52 MSPS profile" thread, but I see something that is different.

Looking at the spectrum I get without input signal (see figure) I note that at central frequencies the noise is higher than reported in that thread, and above all I have a DC component very high.


This is the configuration file I used (is what comes with no-OS release):

/**
 * \file adrv9009/profiles/tx_bw400_ir491p52_rx_bw200_or245p76_orx_bw400_or491p52_dc245p76/talise_config.c
 * \brief Contains Talise configuration settings for the Talise API
 *
 * Copyright 2015-2017 Analog Devices Inc.
 * Released under the AD9378-AD9379 API license, for more information see the "LICENSE.txt" file in this zip file.
 *
 * The top level structure taliseDevice_t talDevice uses keyword
 * extern to allow the application layer main() to have visibility
 * to these settings.
 *
 * This file may not be fully complete for the end user application and
 * may need to updated for AGC, GPIO, and DAC full scale settings.
 * To create a full initialisation routine, the user should also refer to the
 * Iron Python initialisation routine generated by the GUI, and also the Talise User Guide.
 *
 */

#include "talise_types.h"
#include "talise_config.h"
#include "talise_error.h"
#include "talise_agc.h"
#ifdef ADI_ZYNQ_PLATFORM
#include "zynq_platform.h"
#endif

int16_t txFirCoefs[20] = {32, -76, 124, -160, 176, -121, -145, 1031, -3015, 20138, -3015, 1031, -145, -121, 176, -160, 124, -76, 32, 0};

int16_t rxFirCoefs[24] = {-194, -715, 777, 907, -1163, -1890, 2240, 3306, -4068, -7024, 9205, 31112, 31112, 9205, -7024, -4068, 3306, 2240, -1890, -1163, 907, 777, -715, -194};

int16_t obsrxFirCoefs[24] = {-44, 22,-18, -1, 32, -75, 83, -81, -15, 354, -1940, 19672, -1940, 354, -15, -81, 83, -75, 32, -1, -18, 22, -44, 0};

#ifdef ADI_ZYNQ_PLATFORM /** < Insert Customer Platform HAL State Container here>*/
/*
 * Platform Layer SPI settings - this structure is specific to ADI's platform layer code.
 * User should replace with their own structure or settings for their hardware
 */
zynqSpiSettings_t spiDev1 = {
	.chipSelectIndex = 1,
	.writeBitPolarity = 0,
	.longInstructionWord = 1,
	.CPHA = 0,
	.CPOL = 0,
	.mode = 0,
	.spiClkFreq_Hz = 25000000
};

/*
 * Platform Layer settings - this structure is specific to ADI's platform layer code.
 * User should replace with their own structure or settings for their hardware
 * The structure is held in taliseDevice_t below as a void pointer, allowing
 * the customer to pass any information for their specific hardware down to the
 * hardware layer code.
 */
zynqAdiDev_t talDevHalInfo = {
	.devIndex = 1,
	.spiSettings = &spiDev1,
	.spiErrCode = 0,
	.timerErrCode = 0,
	.gpioErrCode = 0,
	.logLevel = ADIHAL_LOG_ALL
};
#endif
/**
 *  TalDevice a structure used by the Talise API to hold the platform hardware
 *  structure information, as well as an internal Talise API state container
 *  (devStateInfo) of runtime information used by the API.
 **/
taliseDevice_t talDevice = {
#ifdef ADI_ZYNQ_PLATFORM
	/* Void pointer of users platform HAL settings to pass to HAL layer calls
	 * Talise API does not use the devHalInfo member */
	.devHalInfo = &talDevHalInfo,
#else
	.devHalInfo = NULL,     /* < Insert Customer Platform HAL State Container here>*/
#endif
	/* devStateInfo is maintained internal to the Talise API, just create the memory */
	.devStateInfo = {0}

};

taliseInit_t talInit = {
	/* SPI settings */
	.spiSettings =
	{
		.MSBFirst            = 1,  /* 1 = MSBFirst, 0 = LSBFirst */
		.enSpiStreaming      = 0,  /* Not implemented in ADIs platform layer. SW feature to improve SPI throughput */
		.autoIncAddrUp       = 1,  /* Not implemented in ADIs platform layer. For SPI Streaming, set address increment direction. 1= next addr = addr+1, 0:addr=addr-1 */
		.fourWireMode        = 1,  /* 1: Use 4-wire SPI, 0: 3-wire SPI (SDIO pin is bidirectional). NOTE: ADI's FPGA platform always uses 4-wire mode */
		.cmosPadDrvStrength  = TAL_CMOSPAD_DRV_2X /* Drive strength of CMOS pads when used as outputs (SDIO, SDO, GP_INTERRUPT, GPIO 1, GPIO 0) */
	},

	/* Rx settings */
	.rx =
	{
		.rxProfile =
		{
			.rxFir =
			{
				.gain_dB = -6,                /* filter gain */
				.numFirCoefs = 24,            /* number of coefficients in the FIR filter */
				.coefs = &rxFirCoefs[0]
			},
			.rxFirDecimation = 2,            /* Rx FIR decimation (1,2,4) */
			.rxDec5Decimation = 4,            /* Decimation of Dec5 or Dec4 filter (5,4) */
			.rhb1Decimation = 1,            /* RX Half band 1 decimation (1 or 2) */
			.rxOutputRate_kHz = 245760,            /* Rx IQ data rate in kHz */
			.rfBandwidth_Hz = 200000000,    /* The Rx RF passband bandwidth for the profile */
			.rxBbf3dBCorner_kHz = 200000,    /* Rx BBF 3dB corner in kHz */
			.rxAdcProfile = {185, 141, 172, 90, 1280, 942, 1332, 90, 1368, 46, 1016, 19, 48, 48, 37, 208, 0, 0, 0, 0, 52, 0, 7, 6, 42, 0, 7, 6, 42, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 31, 905},            /* pointer to custom ADC profile */
			.rxDdcMode = TAL_RXDDC_BYPASS,   /* Rx DDC mode */
			.rxNcoShifterCfg =
			{
				.bandAInputBandWidth_kHz = 0,
				.bandAInputCenterFreq_kHz = 0,
				.bandANco1Freq_kHz = 0,
				.bandANco2Freq_kHz = 0,
				.bandBInputBandWidth_kHz = 0,
				.bandBInputCenterFreq_kHz = 0,
				.bandBNco1Freq_kHz = 0,
				.bandBNco2Freq_kHz = 0
			}
		},
		.framerSel = TAL_FRAMER_A,            /* Rx JESD204b framer configuration */
		.rxGainCtrl =
		{
			.gainMode = TAL_MGC,            /* taliserxGainMode_t gainMode */
			.rx1GainIndex = 255,            /* uint8_t rx1GainIndex */
			.rx2GainIndex = 255,            /* uint8_t rx2GainIndex */
			.rx1MaxGainIndex = 255,            /* uint8_t rx1MaxGainIndex */
			.rx1MinGainIndex = 195,            /* uint8_t rx1MinGainIndex */
			.rx2MaxGainIndex = 255,            /* uint8_t rx2MaxGainIndex */
			.rx2MinGainIndex = 195            /* uint8_t rx2MinGainIndex */
		},
		.rxChannels = TAL_RX1RX2,                /* The desired Rx Channels to enable during initialization */
	},


	/* Tx settings */
	.tx =
	{
		.txProfile =
		{
			.dacDiv = 1,                        /* The divider used to generate the DAC clock */
			.txFir =
			{
				.gain_dB = 0,                        /* filter gain */
				.numFirCoefs = 20,                    /* number of coefficients in the FIR filter */
				.coefs = &txFirCoefs[0]
			},
			.txFirInterpolation = 1,                    /* The Tx digital FIR filter interpolation (1,2,4) */
			.thb1Interpolation = 2,                    /* Tx Halfband1 filter interpolation (1,2) */
			.thb2Interpolation = 2,                    /* Tx Halfband2 filter interpolation (1,2)*/
			.thb3Interpolation = 1,                    /* Tx Halfband3 filter interpolation (1,2)*/
			.txInt5Interpolation = 1,                    /* Tx Int5 filter interpolation (1,5) */
			.txInputRate_kHz = 491520,                    /* Primary Signal BW */
			.primarySigBandwidth_Hz = 150000000,    /* The Rx RF passband bandwidth for the profile */
			.rfBandwidth_Hz = 400000000,            /* The Tx RF passband bandwidth for the profile */
			.txDac3dBCorner_kHz = 400000,                /* The DAC filter 3dB corner in kHz */
			.txBbf3dBCorner_kHz = 200000,                /* The BBF 3dB corner in kHz */
			.loopBackAdcProfile = {186, 148, 176, 90, 1280, 901, 1479, 225, 1401, 85, 995, 21, 48, 48, 36, 207, 0, 0, 0, 0, 52, 0, 0, 6, 24, 0, 0, 6, 24, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 15, 905}
		},
		.deframerSel = TAL_DEFRAMER_A,                    /* Talise JESD204b deframer config for the Tx data path */
		.txChannels = TAL_TX1TX2,                            /* The desired Tx channels to enable during initialization */
		.txAttenStepSize = TAL_TXATTEN_0P05_DB,            /* Tx Attenuation step size */
		.tx1Atten_mdB = 10000,                            /* Initial Tx1 Attenuation */
		.tx2Atten_mdB = 10000,                            /* Initial Tx2 Attenuation */
		.disTxDataIfPllUnlock = TAL_TXDIS_TX_RAMP_DOWN_TO_ZERO    /* Options to disable the transmit data when the RFPLL unlocks. */
	},


	/* ObsRx settings */
	.obsRx =
	{
		.orxProfile =
		{
			.rxFir =
			{
				.gain_dB = 6,                /* filter gain */
				.numFirCoefs = 24,            /* number of coefficients in the FIR filter */
				.coefs = &obsrxFirCoefs[0]
			},
			.rxFirDecimation = 1,            /* Rx FIR decimation (1,2,4) */
			.rxDec5Decimation = 4,            /* Decimation of Dec5 or Dec4 filter (5,4) */
			.rhb1Decimation = 1,            /* RX Half band 1 decimation (1 or 2) */
			.orxOutputRate_kHz = 491520,            /* Rx IQ data rate in kHz */
			.rfBandwidth_Hz = 400000000,    /* The Rx RF passband bandwidth for the profile */
			.rxBbf3dBCorner_kHz = 225000,    /* Rx BBF 3dB corner in kHz */
			.orxLowPassAdcProfile = {113, 171, 181, 90, 1280, 1737, 1574, 839, 1305, 297, 846, 74, 30, 41, 32, 193, 0, 0, 0, 0, 48, 0, 0, 0, 24, 0, 0, 0, 24, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 15, 905},
			.orxBandPassAdcProfile = {113, 171, 181, 90, 1280, 1737, 1574, 839, 1305, 297, 846, 74, 30, 41, 32, 193, 0, 0, 0, 0, 48, 0, 0, 0, 24, 0, 0, 0, 24, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 15, 905},
			.orxDdcMode = TAL_ORXDDC_DISABLED,   /* ORx DDC mode */
            .orxMergeFilter  = {-167, 419, -208, -498, 968, -320, -1273, 2154, -402, -4155, 9170, 21413}
		},
		.orxGainCtrl =
		{
			.gainMode = TAL_MGC,
			.orx1GainIndex = 255,
			.orx2GainIndex = 255,
			.orx1MaxGainIndex = 255,
			.orx1MinGainIndex = 195,
			.orx2MaxGainIndex = 255,
			.orx2MinGainIndex = 195
		},
		.framerSel = TAL_FRAMER_B,                /* ObsRx JESD204b framer configuration */
		.obsRxChannelsEnable = TAL_ORX1,        /* The desired ObsRx Channels to enable during initialization */
		.obsRxLoSource = TAL_OBSLO_RF_PLL                /* The ORx mixers can use the TX_PLL */
	},

	/* Digital Clock Settings */
	.clocks =
	{
		.deviceClock_kHz = 245760,            /* CLKPLL and device reference clock frequency in kHz */
		.clkPllVcoFreq_kHz = 9830400,        /* CLKPLL VCO frequency in kHz */
		.clkPllHsDiv = TAL_HSDIV_2P5,            /* CLKPLL high speed clock divider */
		.rfPllUseExternalLo = 0,                /* 1= Use external LO for RF PLL, 0 = use internal LO generation for RF PLL */
		.rfPllPhaseSyncMode = TAL_RFPLLMCS_NOSYNC                /* RFPLL MCS (Phase sync) mode */
	},

	/* JESD204B settings */
	.jesd204Settings =
	{
		/* Framer A settings */
		.framerA =
		{
			.bankId = 1,                    /* JESD204B Configuration Bank ID -extension to Device ID (Valid 0..15) */
			.deviceId = 0,                    /* JESD204B Configuration Device ID - link identification number. (Valid 0..255) */
			.lane0Id = 0,                    /* JESD204B Configuration starting Lane ID.  If more than one lane used, each lane will increment from the Lane0 ID. (Valid 0..31) */
			.M = 2,                            /* number of ADCs (0, 2, or 4) - 2 ADCs per receive chain */
			.K = 32,                        /* number of frames in a multiframe (default=32), F*K must be a multiple of 4. (F=2*M/numberOfLanes) */
			.F = 2,                            /* F (number of bytes per frame) */
			.Np = 16,                            /* Np (converter sample resolution) */
			.scramble = 1,                    /* scrambling off if framerScramble= 0, if framerScramble>0 scramble is enabled. */
			.externalSysref = 1,            /* 0=use internal SYSREF, 1= use external SYSREF */
			.serializerLanesEnabled = 0x03,    /* serializerLanesEnabled - bit per lane, [0] = Lane0 enabled, [1] = Lane1 enabled */
			.serializerLaneCrossbar = 0xE4,    /* serializerLaneCrossbar */
			.lmfcOffset = 31,                /* lmfcOffset - LMFC offset value for deterministic latency setting */
			.newSysrefOnRelink = 0,            /* newSysrefOnRelink */
			.syncbInSelect = 0,                /* syncbInSelect; */
			.overSample = 0,                    /* 1=overSample, 0=bitRepeat */
			.syncbInLvdsMode = 1,
			.syncbInLvdsPnInvert = 0,
			.enableManualLaneXbar = 0 /* 0=auto, 1=manual */
		},
		/* Framer B settings */
		.framerB =
		{
			.bankId = 0,                    /* JESD204B Configuration Bank ID -extension to Device ID (Valid 0..15) */
			.deviceId = 0,                    /* JESD204B Configuration Device ID - link identification number. (Valid 0..255) */
			.lane0Id = 0,                    /* JESD204B Configuration starting Lane ID.  If more than one lane used, each lane will increment from the Lane0 ID. (Valid 0..31) */
			.M = 2,                            /* number of ADCs (0, 2, or 4) - 2 ADCs per receive chain */
			.K = 32,                        /* number of frames in a multiframe (default=32), F*K must be a multiple of 4. (F=2*M/numberOfLanes) */
			.F = 2,                            /* F (number of bytes per frame) */
			.Np = 16,                            /* Np (converter sample resolution) */
			.scramble = 1,                    /* scrambling off if framerScramble= 0, if framerScramble>0 scramble is enabled. */
			.externalSysref = 1,            /* 0=use internal SYSREF, 1= use external SYSREF */
			.serializerLanesEnabled = 0x0C,    /* serializerLanesEnabled - bit per lane, [0] = Lane0 enabled, [1] = Lane1 enabled */
			.serializerLaneCrossbar = 0xE4,    /* serializerLaneCrossbar */
			.lmfcOffset = 31,                /* lmfcOffset - LMFC offset value for deterministic latency setting */
			.newSysrefOnRelink = 0,            /* newSysrefOnRelink */
			.syncbInSelect = 1,                /* syncbInSelect; */
			.overSample = 0,                    /* 1=overSample, 0=bitRepeat */
			.syncbInLvdsMode = 1,
			.syncbInLvdsPnInvert = 0,
			.enableManualLaneXbar = 0 /* 0=auto, 1=manual */
		},
		/* Deframer A settings */
		.deframerA =
		{
			.bankId = 0,                    /* bankId extension to Device ID (Valid 0..15) */
			.deviceId = 0,                    /* deviceId  link identification number. (Valid 0..255) */
			.lane0Id = 0,                    /* lane0Id Lane0 ID. (Valid 0..31) */
			.M = 4,                            /* M  number of DACss (0, 2, or 4) - 2 DACs per transmit chain */
			.K = 32,                        /* K  #frames in a multiframe (default=32), F*K=multiple of 4. (F=2*M/numberOfLanes) */
			.scramble = 1,                    /* scramble  scrambling off if scramble= 0 */
			.externalSysref = 1,            /* externalSysref  0= use internal SYSREF, 1= external SYSREF */
			.deserializerLanesEnabled = 0x0F,    /* deserializerLanesEnabled  bit per lane, [0] = Lane0 enabled */
			.deserializerLaneCrossbar = 0xE4,    /* deserializerLaneCrossbar */
			.lmfcOffset = 17,                /* lmfcOffset	 LMFC offset value to adjust deterministic latency */
			.newSysrefOnRelink = 0,            /* newSysrefOnRelink */
			.syncbOutSelect = 0,                /* SYNCBOUT0/1 select */
			.Np = 16,                /* Np (converter sample resolution) */
			.syncbOutLvdsMode = 1,
			.syncbOutLvdsPnInvert = 0,
			.syncbOutCmosSlewRate = 0,
			.syncbOutCmosDriveLevel = 0,
			.enableManualLaneXbar = 0 /* 0=auto, 1=manual */
		},
		/* Deframer B settings */
		.deframerB =
		{
			.bankId = 0,                    /* bankId extension to Device ID (Valid 0..15) */
			.deviceId = 0,                    /* deviceId  link identification number. (Valid 0..255) */
			.lane0Id = 0,                    /* lane0Id Lane0 ID. (Valid 0..31) */
			.M = 0,                            /* M  number of DACss (0, 2, or 4) - 2 DACs per transmit chain */
			.K = 32,                        /* K  #frames in a multiframe (default=32), F*K=multiple of 4. (F=2*M/numberOfLanes) */
			.scramble = 1,                    /* scramble  scrambling off if scramble= 0 */
			.externalSysref = 1,            /* externalSysref  0= use internal SYSREF, 1= external SYSREF */
			.deserializerLanesEnabled = 0x00,    /* deserializerLanesEnabled  bit per lane, [0] = Lane0 enabled */
			.deserializerLaneCrossbar = 0xE4,    /* deserializerLaneCrossbar */
			.lmfcOffset = 0,                /* lmfcOffset	 LMFC offset value to adjust deterministic latency */
			.newSysrefOnRelink = 0,            /* newSysrefOnRelink */
			.syncbOutSelect = 1,                /* SYNCBOUT0/1 select */
			.Np = 16,                /* Np (converter sample resolution) */
			.syncbOutLvdsMode = 1,
			.syncbOutLvdsPnInvert = 0,
			.syncbOutCmosSlewRate = 0,
			.syncbOutCmosDriveLevel = 0,
			.enableManualLaneXbar = 0 /* 0=auto, 1=manual */
		},
		.serAmplitude = 15,                    /* Serializer amplitude setting. Default = 15. Range is 0..15 */
		.serPreEmphasis = 1,                /* Serializer pre-emphasis setting. Default = 1 Range is 0..4 */
		.serInvertLanePolarity = 0,            /* Serializer Lane PN inversion select. Default = 0. Where, bit[0] = 1 will invert lane [0], bit[1] = 1 will invert lane 1, etc. */
		.desInvertLanePolarity = 0,            /* Deserializer Lane PN inversion select.  bit[0] = 1 Invert PN of Lane 0, bit[1] = Invert PN of Lane 1, etc */
		.desEqSetting = 1,                    /* Deserializer Equalizer setting. Applied to all deserializer lanes. Range is 0..4 */
		.sysrefLvdsMode = 1,                /* Use LVDS inputs on Talise for SYSREF */
		.sysrefLvdsPnInvert = 0              /*0= Do not PN invert SYSREF */
	}
};

//Only needs to be called if user wants to setup AGC parameters
static taliseAgcCfg_t rxAgcCtrl = {
	4,
	255,
	195,
	255,
	195,
	30720,  /* AGC gain update time in us (125us-250us - based on IQ data rate - set for 125us @ 245.76 Mhz) */
	10,
	10,
	16,
	0,
	1,
	0,
	0,
	0,
	1,
	31,
	246,
	4,
	1,          /*!<1- bit field to enable the multiple time constants in AGC loop for fast attack and fast recovery to max gain. */
	/* agcPower */
	{
		1,      /*!<1-bit field, enables the Rx power measurement block. */
		1,      /*!<1-bit field, allows using Rx PFIR for power measurement. */
		0,      /*!<1-bit field, allows to use the output of the second digital offset block in the Rx datapath for power measurement. */
		9,      /*!<AGC power measurement detect lower 0 threshold. Default = -12dBFS == 5, 7-bit register value where max = 0x7F, min = 0x00 */
		2,      /*!<AGC power measurement detect lower 1 threshold. Default = (offset) 4dB == 0, 4-bit register value where  max = 0xF, min = 0x00 */
		4,      /*!<AGC power measurement detect lower 0 recovery gain step. Default = 2dB - based on gain table step  size, 5-bit register value where max = 0x1F, min = 0x00 */
		4,      /*!<AGC power measurement detect lower 1 recovery gain step. Default = 4dB - based on gain table step size, 5-bit register value where max = 0x1F, min = 0x00 */
		5,      /*!< power measurement duration used by the decimated power block. Default = 0x05, 5-bit register value where max = 0x1F, min = 0x00 */
		5,      /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
		1,      /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
		5,      /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
		1,      /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
		2,      /*!<Default value should be 2*/
		0,
		0
	},
	/* agcPeak */
	{
		205,        /*!<1st update interval for the multiple time constant in AGC loop mode, Default:205. */
		2,          /*!<sets the 2nd update interval for the multiple time constant in AGC loop mode. Calculated as a multiple of  agcUnderRangeLowInterval  , Default: 4 */
		4,          /*!<sets the 3rd update interval for the multiple time constant in AGC loop mode. Calculated as a multiple of agcUnderRangeMidInterval and agcUnderRangeLowInterval, Default: 4 */
		39,         /*!<AGC APD high threshold. Default=0x1F, 6-bit register value where max=0x3F, min =0x00 */
		49,         /*!<AGC APD peak detect high threshold. default = 0x1F, 6-bit register value where max = 0x3F, min = 0x00.  Set to 3dB below apdHighThresh */
		23,         /*!<AGC APD peak detect low threshold. default = 3dB below high threshold, 6-bit register value where max =0x3F, min = 0x00 */
		19,         /*!<AGC APD peak detect low threshold. default = 3dB below high threshold, 6-bit register value where max = 0x3F, min = 0x00 . Set to 3dB below apdLowThresh  */
		6,          /*!<AGC APD peak detect upper threshold count. Default = 0x06 8-bit register value where max = 0xFF, min = 0x20  */
		3,          /*!<AGC APD peak detect lower threshold count. Default = 0x03, 8-bit register value where max = 0xFF, min = 0x00  */
		4,          /*!<AGC APD peak detect attack gain step. Default = 2dB step - based on gain table step size, 5-bit register  value, where max = 0x1F, min = 0x00  */
		2,          /*!<AGC APD gain index step size. Recommended to be same as hb2GainStepRecovery. Default = 0x00, 5-bit register value where max = 0x1F, min = 0x00  */
		1,          /*!<1-bit field, enables or disables the HB2 overload detector.  */
		1,          /*!<3-bit field. Sets the window of clock cycles (at the HB2 output rate) to meet the overload count. */
		1,          /*!<4-bit field. Sets the number of actual overloads required to trigger the overload signal.  */
		181,        /*!<AGC decimator output high threshold. Default = 0xB5, 8-bit register value where max = 0xFF, min = 0x00 */
		45,         /*!<AGC decimator output low threshold. Default = 0x80, 8-bit register value where max = 0xFF, min = 0x00 */
		90,         /*!<AGC decimator output low threshold. Default = 0x80, 8-bit register value where max = 0xFF, min = 0x00 */
		128,        /*!<AGC decimator output low threshold. Default = 0x80, 8-bit register value where max = 0xFF, min = 0x00 */
		6,          /*!<AGC HB2 output upper threshold count. Default = 0x06, 8-bit register value where max = 0xFF, min =  0x20 */
		3,          /*!<AGC HB2 output lower threshold count. Default = 0x03, 8-bit register value where max = 0xFF, min = 0x00 */
		2,          /*!<AGC decimator gain index step size. Default = 0x00, 5-bit register value where max = 0x1F, min = 0x00 */
		4,          /*!<AGC HB2 gain index step size, when the HB2 Low Overrange interval 0 triggers a programmable number  of times. Default = 0x08, 5-bit register value where max = 0x1F, min = 0x00 */
		8,          /*!<AGC HB2 gain index step size, when the HB2 Low Overrange interval 1 triggers a programmable number of times. Default = 0x04, 5-bit register value where max = 0x1F, min = 0x00 */
		4,          /*!<AGC decimator output attack gain step. Default = 2dB step - based on gain table step size, 5-bit register value, where max = 0x1F, min = 0x00 */
		1,
		0,
		0
	}
};

I've seen that also the ORX input chain has a DC correction block that may be bypassed, but I don't know how to activate it.

Thank you

Maurizio

Edit Notes

deleted replicated file
[edited by: maurizio.sonzogni@abe.it at 2:42 PM (GMT -5) on 21 Feb 2024]

Thread Notes

Parents
  • can you please share the setup connection that you are using, did you connect the feedback signal to ORx? Please share these details to understand more about the issue.

    Use the below API to enable the ORX DC offset.

  • Thank you RR4,

    I'm using this environment:

    - FPGA project is the adrv9009/zc706 project from hdl repository. I've made a little modification sending data to TX channels from a block memory ROM, and looking for ORX data with an ILA.

    - Software project is the adrv9009 project from no-OS repository, the DMA_EXAMPLE option.

    I generate a single side-band sine waveform on both TX1 and TX2, and the spectrum in the above image is calculated from the captured data in ILA when the ORX1 input is not connected to any signal (the input has a 50 ohm clamp).

    I see the same behavior if I put the TX1 signal on ORX1 (via a 20 dB attenuator): in this case I see the correct signal plus the noise and DC component as in the above figure.

    I've tried to make a call to the suggested API: I've made the call to this API after the call to the TALISE_enableTrackingCals API, and before the calls to the TALISE_radioOn and the TALISE_setRxTxEnable APIs in the talise_setup function, but the result is very strange, as you can see in this picture:

    The signal goes from -32768 to 32767 and sometimes around tho 0 value but with some noise and some DC component.

    Is there something else to do when calling the TALISE_setDigDcOffsetEn API?

    Thank you

    Maurizio

  • Search this thread for "The boot log of the board with the SD card is:", it's from one of your replies where immediately after you pasted a linux boot log from the SD card. That is a linux boot log, not a no-OS boot log. There is no way that card contains a no-OS release.

  • Yes, I used the pre-compiled solution on the SD card and that is the log I see when using the SD card. You can find the results of this arrangement with the same profile above in this thread in my post on March 14 2024, 11:39 AM

  • and the ORx is:

    This is not the expected behavior, can you please share the profile that you used for the testing, and what is attenuation used between the Tx output and ORx input?

  • If you read this thread you will find the answers to your questions.

  • Hi  Need your help on below customer issues with the 491.52 MHz profile.

    I have generated the custom profile by enabling ORx stitching profile with 491.52Msps for the ADRV9008-2 device. Customer used the same profile and tested the ORx capture and below are the results.

    Transmitter Section:

    ORx Capture:

    the performance in TES GUI is good and the noise floor, LO leakage is expected.

    1. Now customer proceeded to next step, generated the configuration files with TES GUI. Attached Config_Files.zip. Below is the error 

    Please note that the talise_config.c file still contains an error at line 29:

            int16_t rxFirCoefs[0] = {

    I think the above error due to the device used "ADRV9008-2" is the Tx only and that is why it shows rxFirCoefs are zero.

    2. Customer used the newly created config files in th no-OS environment.

    With the created headless.c file the program stops at the first command line:

        talAction = TALISE_openHw(&talDevice);

    and goes in the Xil_DataAbortHandler routine.

    3. When the customer use the headless.c from the DMA_Example I got this message at the end: “Rx obs Error transferring data using DMA.” and no data output.

    4. when the customer use configuration files from the no-OS DMA_Example (that are in the working_config_files.zip attachment), with the created headless.c file, the program stops at the first command line:  talAction = TALISE_openHw(&talDevice); while with the DMA_example headless.c file 

    They are able to see the ORx capture but with the high LO leakage and rise in noise floor, where as TES GUI shows better response. Below is the graph.

    Customer is using the EVAL-TPG-ZYNQ3 + ADRV9008-2 W/PCBZ boards for the above testing,

  • Hi ,

    The main branch  now supports ADRV9008-2 profiles. When creating profiles, you have to make sure that ORx uses lanes 2 and 3 (FRAMER B settings .serializerLanesEnabled = 0x0C), because the HDL is built according to this lane ordering.

    Regards,

    George

  • Hi danmois rr4,

    I've recompiled the main branch as you said, but I found these problem in order to achieve the goal of make it working @ 491.52 MSPS:

    1. I had to put change a line in the headless.c file to " no_os_gpio_direction_output(gpio_plddrbypass, 0);"
    2. I had to change a line in the "struct adxcvr_init rx_os_adxcvr_init" variable to ".sys_clk_sel = ADXCVR_SYS_CLK_QPLL0,"
    3. In any case I continue to have large DC component and noise. You can see what I get from the DMA data with the scripts capture.tcl and plot.py:

    If I put no signal on the ORX input I get this result:

    where is obvious the presence of a large DC component an noise.

    I then recompiled the HDL with the last release without adding anything, but I obtained the same result.

    Please, someone can test the full project with the same environment as mine (EVAL-TPG-ZYNQ3 + ADRV9008-2 W/PCBZ boards, with no-OS firmware) and show me his results and how to achieve them?

    Thank you,

    Maurizio Sonzogni

  • Hi ,

    We will perform the tests using an ADRV9008-2 board as soon as we receive the hardware.

    As this forum is targeted to the no-OS framework and to API integration issues, the  Support ADRV9008x/ADRV9009  forum is more suitable for finding a solution your last question, that is concerned with the presence of the DC component and noise on the ORx input.

    Regards,

    George

  • Hi Danmois,

    I was back in the no-OS thread because I had no answers from the other forum, and they said that maybe the problem is in the software.

    Thank you

    Maurizio

  • Hi Danmois,

    have you succeeded in performing the test with the ADRV9008-2 board? My boss is pressing me to solve this issue.

    Thank you

    Maurizio

Reply Children
  • We encountered a similar problem and recommended closing the launch channel.

  • Hi ,

    Can you, please, share the GUI setup you used in TES for testing? We can now replicate your setup.

    Regards,

    George

  • Using TES and the pre-compiled SD card program running on the EVAL-TPG-ZYNQ3 all is OK.

    If I save the profile to use with no-OS there is no way to get any result: the compilation gives syntax errors, and after correcting the wrong line, the program stops at the first command line:
    talAction = TALISE_openHw(&talDevice);

    If I use the talise_config.c file that comes with the no-OS release in the tx_bw400_ir491p52_rx_bw200_or245p76_orx_bw400_or491p52_dc245p76 folder, I get some data, but is affected by large DC and noise.

    You can see in this thread the profile files generated by the Talise Configuration Wizard and then by TES program.

    Thank you

    Maurizio

  • Hi ,

    The reason for asking for the GUI setup was because I use TES ver 3.6.2.1 and the profile generated is ok to use in no-OS. However, I get another weird response (below, left part). By the way, I get that by compiling the project with the IIOD=y flag and use IIO Oscilloscope to visualize data.

    The generated headless file cannot run because it need additional routines for setting the low-level functions. Therefore, a comparison between this headless file and the headless.c file in the no-OS project is needed (they should perform the same steps in terms of API calls).

    From my point of view, it is clear that we are missing something when setting the device to work in stitching mode (other profiles work ok also on no-OS). I will get back soon with more information.

    Regards,

    George 

  • Hi ,

    We have found the source for the spikes in the FFT above. It is caused by a problem in the ADC buffer (see images below).

    We will return with a fix for this discontinuities in the ADC signal.

    Regards,

    George

  • Hi  ,

    The problem seems to be in the Rx buffer on ZC706, that cannot keep pace with the data rate. We will provide a fix for the HDL project.

    In the picture you can see the data acquired through loopback between Tx2 and ORx1.

    Testing with an ADRV9009 or ADRV9008-2 gives similar results.

    Regards,

    George

  • Hi ,

    The modifications that fix the problem are now in the HDL main branch. Working with both the current main branches for no-OS and HDL solves the issue.

    Regards,

    George

  • Hi George,

    I've rebuilt the HDL project and the no-OS project with the IIOD=y flag, and then uncommenting the #define ADRV9008_2 line (we have ADRV9008-2 as transceiver).

    I'm running the software in debug in a Vitis Classic 2023.2 environment.

    If I use the pre-defined profile (in the tx_bw100_ir122p88_rx_bw100_or122p88_orx_bw100_or122p88_dc122p88 folder) all is OK and I can get the received data with an IIO oscilloscope program, but if I use the profile file (in the tx_bw400_ir491p52_rx_bw200_or245p76_orx_bw400_or491p52_dc245p76 folder) provided with the no-OS project, I get this console output:

    Hello
    tx_clkgen: MMCM-PLL locked (245760000 Hz)
    rx_os_clkgen: MMCM-PLL locked (245760000 Hz)
    error: rx_os_adxcvr: adxcvr_init() failed
    Bye

    Note that with the previous version the provided talise_config.c file for 491.52MSPS (that is the same as the actual) was the only running, although with unexpected noise and DC.

    Then I found that a problem I already mentioned is still alive: in the struct adxcvr_init rx_os_adxcvr_init the .sys_clk_sel must be ADXCVR_SYS_CLK_QPLL0, because with ADXCVR_SYS_CLK_CPLL the fpga_xcvr_init cannot be done with the requested frequencies.

    In this case the result is:

    I tried also the 245.76 MSPS profile provided with the no-OS and I get this wit CPLL:

    and this with QPLL:

    with CPLL I got these errors in the console log:

    ERR: ../noos/drivers/axi_core/jesd204/axi_adxcvr.c:513:adxcvr_clk_enable(): adxcvr_clk_enable: CPLL RX buffer underflow error, status: 0x61
    ERR: ../noos/drivers/axi_core/jesd204/axi_adxcvr.c:520:adxcvr_clk_enable(): adxcvr_clk_enable: CPLL RX buffer overflow error, status: 0x61

    Can you please provide the talise_config.c tat's working for 491.52 MSPS with ADRV9008-2?

    Thank you,

    Maurizio

  • Hi  ,

    You will still need to set ADXCVR_SYS_CLK_QPLL0 for sys_clk_sel in the Observation Rx ADXCVR initialization structure (modification required for this setting):

    https://github.com/analogdevicesinc/no-OS/blob/001f8bcdce255922dc28197f6d2edb7a9c0b9926/projects/adrv9009/src/app/app_transceiver.c#L120

    I used the profile you provided, with the error on line 29. From this profile I removed the rxFirCoefs array on that line and I set serializerLanesEnabled = 0x0C for framerB. You can see the result below:

    Regards,

    George

  • Hi George,

    finally something seems to work.

    There is still a little difference in the spectrum that you can see in the following figures:

    I cannot imagine what is the cause of this difference: maybe some filter.

    I used the configuration file I posted in this thread on march 14 with the modifications you said. In any case this result is the same as that of TES program for the same profile.

    Thank you very much for your help in this item.

    Maurizio