Post Go back to editing

USRP E312 (AD9361) - IIO Oscilloscope doesn't work

Category: Software
Product Number: USRP E312 (AD9361) from Ettus
Software Version: WSL 2: Ubuntu-20.04, Kernel 5.10.102.1, hdl: master, no-OS master

I tried using IIO oscilloscope with the SDR E312 from Ettus, I use the code from my previous thread USRP E312 (AD9361) - ad9361_dig_tune_delay: Tuning RX FAILED!  thanks to   with this commit.

Then I enable IIO_SUPPORT, it works with the following result: 

cf-ad9361-lpc: Successfully initialized (61439514 Hz)
ad9361_init : AD936x Rev 2 successfully initialized
Sampling frequency is: 30720000
New sampling frequency is: 15360000
LO frequency of TX is: 1000000000
Output port TX: 0
Power state of Tx: 1
cf-ad9361-dds-core-lpc: Successfully initialized (30718994 Hz)
�Running TinyIIOD server...
If successful, you may connect an IIO client application by:
1. Disconnecting the serial terminal you use to view this message.
2. Connecting the IIO client application using the serial backend configured as shown:
Baudrate: 921600
Data size: 8 bits
Parity: none
Stop bits: 1
Flow control: none

However, on my computer IIO Oscilloscope doesn't work. I have the same problems than   in this thread  serial connection with iio oscilloscope .

For example when installing IIO oscilloscope with this link IIO Oscilloscope , i can't choose Serial Content.

According to  ,  I reinstalled libiio with the command:

analog@precision:~/libiio$ mkdir build
analog@precision:~/libiio/build$ cd build
analog@precision:~/libiio/build$ cmake ../ -DWITH_SERIAL_BACKEND=ON
analog@precision:~/libiio/build$ make -j
analog@precision:~/libiio/build$ sudo make instal

Thus, i have the error Could not get IIO Context: inappropriate ioctl for device ...

So I tried to build libserialport with the link https://sigrok.org/wiki/Libserialport and the post of   with the command:

$ ./autogen.sh
$ ./configure --prefix=/usr
$ make
$ sudo make instal

but I'm stuck at ./autogen.sh, I get the following error:

/path/to/libserialport$ ./autogen.sh
/bin/sh: 0: Illegal option -

How can we solve this problem?
Thank you very much for your time,

Regards,

Rémi



Modification
[edited by: RemiL at 12:58 PM (GMT -4) on 13 Jul 2023]
Parents
  • Hi Rémi,

    Could you try to install libserialport via the package manager rather than building it  from source ? 

    Try :  apt-get install libserialport-dev

    After you have installed this package, you will need to rebuild libiio with the serial backend enabled. Then, you will also have to rebuild iio-oscilloscope.

    Let us know if this works for you.

    -Cristina

  • HI  ,

    Thank you for your reply.

    I installed as you said libserialport-dev. But I get exactly the same error.

    Here are the results of some commands if you need them:

    path/to/libiio/build$ cmake ../ -DWITH_SERIAL_BACKEND=ON

    -- cmake version: 3.16.3
    -- The C compiler identification is GNU 9.4.0
    -- Check for working C compiler: /usr/bin/cc
    -- Check for working C compiler: /usr/bin/cc -- works
    -- Detecting C compiler ABI info
    -- Detecting C compiler ABI info - done
    -- Detecting C compile features
    -- Detecting C compile features - done
    -- Performing Test HAS_WPEDANTIC
    -- Performing Test HAS_WPEDANTIC - Success
    -- Performing Test HAS_WSHADOW
    -- Performing Test HAS_WSHADOW - Success
    -- Looking for strdup
    -- Looking for strdup - found
    -- Looking for strndup
    -- Looking for strndup - found
    -- Looking for strerror_r
    -- Looking for strerror_r - found
    -- Looking for strtok_r
    -- Looking for strtok_r - found
    -- Looking for newlocale
    -- Looking for newlocale - found
    -- Looking for in6addr_any
    -- Looking for in6addr_any - found
    -- Found PkgConfig: /usr/bin/pkg-config (found version "0.29.1")
    -- Checking for module 'libusb-1.0'
    --   Found libusb-1.0, version 1.0.23
    -- Looking for libusb_get_version
    -- Looking for libusb_get_version - found
    -- Found Git: /usr/bin/git (found version "2.25.1")
    -- Looking for libserialport : Found
    -- Performing Test WITH_NETWORK_EVENTFD
    -- Performing Test WITH_NETWORK_EVENTFD - Success
    -- Found LibXml2: /usr/lib/x86_64-linux-gnu/libxml2.so (found version "2.9.10")
    -- Found BISON: /usr/bin/bison (found version "3.5.1")
    -- Found FLEX: /usr/bin/flex (found version "2.6.4")
    -- Looking for pthread_setname_np
    -- Looking for pthread_setname_np - found
    -- Looking for sys/types.h
    -- Looking for sys/types.h - found
    -- Looking for stdint.h
    -- Looking for stdint.h - found
    -- Looking for stddef.h
    -- Looking for stddef.h - found
    -- Check size of struct usb_functionfs_descs_head_v2
    -- Check size of struct usb_functionfs_descs_head_v2 - done
    -- Features enabled : xml network dns-sd avahi ipv6 serial local local-mmap hwmon usb utils iiod udev-rule iiod-serial iiod-aio iiod-usb man-utils
    -- Features disabled: zstd bonjour examples c++-bindings iiod-systemd iiod-sysvinit iiod-upstart doc man python-bindings c#-bindings
    -- Configuring done
    -- Generating done
    -- Build files have been written to :path/to/liibio/build
    

    path/to/libiio/build$ sudo make install

    path/to/libiio/build$ sudo make install
    [ 41%] Built target iio
    [ 47%] Built target iio_tests_helper
    [ 52%] Built target iio_genxml
    [ 56%] Built target iio_writedev
    [ 60%] Built target iio_stresstest
    [ 64%] Built target iio_info
    [ 68%] Built target iio_attr
    [ 72%] Built target iio_readdev
    [ 77%] Built target iio_reg
    [100%] Built target iiod
    Install the project...
    -- Install configuration: "RelWithDebInfo"
    -- Installing: /usr/lib/x86_64-linux-gnu/pkgconfig/libiio.pc
    -- Installing: /usr/lib/x86_64-linux-gnu/libiio.so.0.25
    -- Up-to-date: /usr/lib/x86_64-linux-gnu/libiio.so.0
    -- Up-to-date: /usr/lib/x86_64-linux-gnu/libiio.so
    -- Installing: /usr/include/iio.h
    -- Installing: /lib/udev/rules.d/90-libiio.rules
    -- Installing: /usr/bin/iio_genxml
    -- Set runtime path of "/usr/bin/iio_genxml" to ""
    -- Installing: /usr/bin/iio_info
    -- Set runtime path of "/usr/bin/iio_info" to ""
    -- Installing: /usr/bin/iio_attr
    -- Set runtime path of "/usr/bin/iio_attr" to ""
    -- Installing: /usr/bin/iio_readdev
    -- Set runtime path of "/usr/bin/iio_readdev" to ""
    -- Installing: /usr/bin/iio_reg
    -- Set runtime path of "/usr/bin/iio_reg" to ""
    -- Installing: /usr/bin/iio_writedev
    -- Set runtime path of "/usr/bin/iio_writedev" to ""
    -- Installing: /usr/bin/iio_stresstest
    -- Set runtime path of "/usr/bin/iio_stresstest" to ""
    -- Installing: /usr/sbin/iiod
    -- Set runtime path of "/usr/sbin/iiod" to ""

    path/to/iio-oscilloscope/build$ cmake ../ && make -j $(nproc)

    path/to/iio-oscilloscope/build$ cmake ../ && make -j $(nproc)
    -- The C compiler identification is GNU 9.4.0
    -- Check for working C compiler: /usr/bin/cc
    -- Check for working C compiler: /usr/bin/cc -- works
    -- Detecting C compiler ABI info
    -- Detecting C compiler ABI info - done
    -- Detecting C compile features
    -- Detecting C compile features - done
    -- Found Git: /usr/bin/git (found version "2.25.1")
    -- Found PkgConfig: /usr/bin/pkg-config (found version "0.29.1")
    -- Checking for module 'glib-2.0'
    --   Found glib-2.0, version 2.64.6
    -- Checking for module 'gtk+-3.0'
    --   Found gtk+-3.0, version 3.24.20
    -- Checking for module 'gthread-2.0'
    --   Found gthread-2.0, version 2.64.6
    -- Checking for module 'gtkdatabox'
    --   Found gtkdatabox, version 1.0.0
    -- Checking for module 'fftw3'
    --   Found fftw3, version 3.3.8
    -- Checking for module 'libxml-2.0'
    --   Found libxml-2.0, version 2.9.10
    -- Checking for module 'libcurl'
    --   Found libcurl, version 7.68.0
    -- Checking for module 'jansson'
    --   Found jansson, version 2.12
    -- Checking for module 'matio'
    --   Found matio, version 1.5.17
    -- Configuring done
    -- Generating done
    -- Build files have been written to: /path/to/iio-oscilloscope/build
    Scanning dependencies of target osc
    [  1%] Building C object CMakeFiles/osc.dir/osc.c.o
    [  8%] Building C object CMakeFiles/osc.dir/datatypes.c.o
    [  8%] Building C object CMakeFiles/osc.dir/oscplot.c.o
    [  8%] Building C object CMakeFiles/osc.dir/iio_utils.c.o
    [  8%] Building C object CMakeFiles/osc.dir/fru.c.o
    [  8%] Building C object CMakeFiles/osc.dir/iio_widget.c.o
    [  9%] Building C object CMakeFiles/osc.dir/dialogs.c.o
    [  9%] Building C object CMakeFiles/osc.dir/trigger_dialog.c.o
    [ 10%] Building C object CMakeFiles/osc.dir/xml_utils.c.o
    [ 12%] Building C object CMakeFiles/osc.dir/libini/libini.c.o
    [ 13%] Building C object CMakeFiles/osc.dir/libini2.c.o
    [ 14%] Building C object CMakeFiles/osc.dir/phone_home.c.o
    [ 15%] Building C object CMakeFiles/osc.dir/plugins/dac_data_manager.c.o
    [ 16%] Building C object CMakeFiles/osc.dir/plugins/fir_filter.c.o
    [ 18%] Building C object CMakeFiles/osc.dir/eeprom.c.o
    [ 19%] Building C object CMakeFiles/osc.dir/osc_preferences.c.o
    [ 20%] Linking C shared library libosc.so
    [ 20%] Built target osc
    Scanning dependencies of target adrv9002
    Scanning dependencies of target ad6676
    Scanning dependencies of target fmcadc3
    Scanning dependencies of target cf_axi_tdd
    Scanning dependencies of target ad9371_adv
    Scanning dependencies of target xmw
    Scanning dependencies of target fmcomms6
    Scanning dependencies of target oscmain
    [ 21%] Building C object plugins/CMakeFiles/xmw.dir/xmw.c.o
    [ 22%] Building C object plugins/CMakeFiles/cf_axi_tdd.dir/cf_axi_tdd.c.o
    [ 28%] Building C object plugins/CMakeFiles/fmcadc3.dir/fmcadc3.c.o
    [ 28%] Building C object plugins/CMakeFiles/adrv9002.dir/adrv9002.c.o
    [ 28%] Building C object plugins/CMakeFiles/fmcomms6.dir/fmcomms6.c.o
    [ 28%] Building C object CMakeFiles/oscmain.dir/oscmain.c.o
    [ 28%] Building C object plugins/CMakeFiles/ad6676.dir/ad6676.c.o
    [ 30%] Building C object plugins/CMakeFiles/ad9371_adv.dir/ad9371_adv.c.o
    [ 31%] Linking C shared library cf_axi_tdd.so
    [ 32%] Linking C shared library xmw.so
    [ 33%] Linking C shared library fmcadc3.so
    [ 34%] Linking C shared library fmcomms6.so
    [ 36%] Linking C shared library ad6676.so
    [ 37%] Linking C executable osc
    [ 38%] Linking C shared library ad9371_adv.so
    [ 38%] Built target cf_axi_tdd
    [ 38%] Built target fmcadc3
    [ 38%] Built target xmw
    [ 38%] Built target fmcomms6
    Scanning dependencies of target adrv9009_adv
    Scanning dependencies of target lidar
    Scanning dependencies of target fmcomms2_adv
    Scanning dependencies of target fmcomms11
    [ 38%] Built target ad6676
    Scanning dependencies of target pr_config
    [ 39%] Linking C shared library adrv9002.so
    [ 39%] Built target ad9371_adv
    Scanning dependencies of target fmcomms1
    [ 39%] Built target adrv9002
    Scanning dependencies of target adrv9009
    [ 39%] Built target oscmain
    Scanning dependencies of target fmcomms5
    [ 40%] Building C object plugins/CMakeFiles/lidar.dir/lidar.c.o
    [ 42%] Building C object plugins/CMakeFiles/adrv9009_adv.dir/adrv9009_adv.c.o
    [ 44%] Building C object plugins/CMakeFiles/fmcomms11.dir/fmcomms11.c.o
    [ 44%] Building C object plugins/CMakeFiles/fmcomms2_adv.dir/fmcomms2_adv.c.o
    [ 45%] Building C object plugins/CMakeFiles/pr_config.dir/pr_config.c.o
    [ 46%] Building C object plugins/CMakeFiles/fmcomms1.dir/fmcomms1.c.o
    [ 48%] Building C object plugins/CMakeFiles/adrv9009.dir/adrv9009.c.o
    [ 49%] Building C object plugins/CMakeFiles/fmcomms5.dir/fmcomms5.c.o
    [ 50%] Linking C shared library lidar.so
    [ 51%] Linking C shared library fmcomms11.so
    [ 53%] Linking C shared library pr_config.so
    [ 54%] Linking C shared library adrv9009_adv.so
    [ 55%] Linking C shared library fmcomms2_adv.so
    [ 55%] Built target lidar
    [ 55%] Built target fmcomms11
    Scanning dependencies of target cn0540
    [ 55%] Built target pr_config
    Scanning dependencies of target generic_dac
    [ 55%] Built target adrv9009_adv
    Scanning dependencies of target ad9371
    Scanning dependencies of target scpi
    [ 55%] Built target fmcomms2_adv
    Scanning dependencies of target ad9739a
    [ 56%] Linking C shared library fmcomms1.so
    [ 57%] Linking C shared library adrv9009.so
    [ 59%] Linking C shared library fmcomms5.so
    [ 59%] Built target fmcomms1
    [ 59%] Built target adrv9009
    Scanning dependencies of target daq2
    Scanning dependencies of target dmm
    [ 59%] Built target fmcomms5
    Scanning dependencies of target AD5628_1
    [ 60%] Building C object plugins/CMakeFiles/cn0540.dir/cn0540.c.o
    [ 61%] Building C object plugins/CMakeFiles/generic_dac.dir/generic_dac.c.o
    [ 62%] Building C object plugins/CMakeFiles/scpi.dir/scpi.c.o
    [ 63%] Building C object plugins/CMakeFiles/ad9371.dir/ad9371.c.o
    [ 65%] Building C object plugins/CMakeFiles/ad9739a.dir/ad9739a.c.o
    [ 66%] Linking C shared library generic_dac.so
    [ 67%] Linking C shared library cn0540.so
    [ 67%] Built target generic_dac
    Scanning dependencies of target fmcomms2
    [ 68%] Linking C shared library scpi.so
    [ 69%] Linking C shared library ad9739a.so
    [ 69%] Built target cn0540
    [ 71%] Building C object plugins/CMakeFiles/dmm.dir/dmm.c.o
    [ 72%] Building C object plugins/CMakeFiles/daq2.dir/daq2.c.o
    Scanning dependencies of target spectrum_analyzer
    [ 73%] Building C object plugins/CMakeFiles/AD5628_1.dir/AD5628_1.c.o
    [ 74%] Linking C shared library ad9371.so
    [ 74%] Built target scpi
    Scanning dependencies of target cn0357
    [ 74%] Built target ad9739a
    Scanning dependencies of target cn0508
    [ 75%] Linking C shared library AD5628_1.so
    [ 75%] Built target ad9371
    [ 77%] Linking C shared library dmm.so
    Scanning dependencies of target ad9084
    [ 78%] Linking C shared library daq2.so
    [ 78%] Built target AD5628_1
    [ 78%] Built target dmm
    Scanning dependencies of target ad9081
    Scanning dependencies of target cn0511
    [ 78%] Built target daq2
    Scanning dependencies of target motor_control
    [ 79%] Building C object plugins/CMakeFiles/fmcomms2.dir/fmcomms2.c.o
    [ 80%] Building C object plugins/CMakeFiles/spectrum_analyzer.dir/spectrum_analyzer.c.o
    [ 81%] Building C object plugins/CMakeFiles/cn0357.dir/cn0357.c.o
    [ 83%] Building C object plugins/CMakeFiles/cn0508.dir/cn0508.c.o
    [ 84%] Linking C shared library spectrum_analyzer.so
    [ 85%] Building C object plugins/CMakeFiles/ad9084.dir/ad9084.c.o
    [ 86%] Linking C shared library cn0357.so
    [ 89%] Building C object plugins/CMakeFiles/ad9081.dir/ad9081.c.o
    [ 89%] Building C object plugins/CMakeFiles/cn0511.dir/cn0511.c.o
    [ 90%] Linking C shared library cn0508.so
    [ 90%] Built target spectrum_analyzer
    Scanning dependencies of target debug
    [ 91%] Building C object plugins/CMakeFiles/motor_control.dir/motor_control.c.o
    [ 92%] Linking C shared library fmcomms2.so
    [ 92%] Built target cn0357
    [ 92%] Built target cn0508
    [ 93%] Linking C shared library ad9084.so
    [ 95%] Linking C shared library cn0511.so
    [ 95%] Built target fmcomms2
    [ 96%] Linking C shared library ad9081.so
    [ 96%] Built target ad9084
    [ 96%] Built target cn0511
    [ 96%] Built target ad9081
    [ 97%] Linking C shared library motor_control.so
    [ 97%] Built target motor_control
    [ 98%] Building C object plugins/CMakeFiles/debug.dir/debug.c.o
    [100%] Linking C shared library debug.so
    [100%] Built target debug

    Do you have any other possible solutions to this problem?

    I also tried to install IIO oscilloscope with this link on a windows laptop but I get the following error:

    Is there any other software to install or is the problem with the USRP E312?


    Thank you very much,

    Regards,

    Rémi

Reply
  • HI  ,

    Thank you for your reply.

    I installed as you said libserialport-dev. But I get exactly the same error.

    Here are the results of some commands if you need them:

    path/to/libiio/build$ cmake ../ -DWITH_SERIAL_BACKEND=ON

    -- cmake version: 3.16.3
    -- The C compiler identification is GNU 9.4.0
    -- Check for working C compiler: /usr/bin/cc
    -- Check for working C compiler: /usr/bin/cc -- works
    -- Detecting C compiler ABI info
    -- Detecting C compiler ABI info - done
    -- Detecting C compile features
    -- Detecting C compile features - done
    -- Performing Test HAS_WPEDANTIC
    -- Performing Test HAS_WPEDANTIC - Success
    -- Performing Test HAS_WSHADOW
    -- Performing Test HAS_WSHADOW - Success
    -- Looking for strdup
    -- Looking for strdup - found
    -- Looking for strndup
    -- Looking for strndup - found
    -- Looking for strerror_r
    -- Looking for strerror_r - found
    -- Looking for strtok_r
    -- Looking for strtok_r - found
    -- Looking for newlocale
    -- Looking for newlocale - found
    -- Looking for in6addr_any
    -- Looking for in6addr_any - found
    -- Found PkgConfig: /usr/bin/pkg-config (found version "0.29.1")
    -- Checking for module 'libusb-1.0'
    --   Found libusb-1.0, version 1.0.23
    -- Looking for libusb_get_version
    -- Looking for libusb_get_version - found
    -- Found Git: /usr/bin/git (found version "2.25.1")
    -- Looking for libserialport : Found
    -- Performing Test WITH_NETWORK_EVENTFD
    -- Performing Test WITH_NETWORK_EVENTFD - Success
    -- Found LibXml2: /usr/lib/x86_64-linux-gnu/libxml2.so (found version "2.9.10")
    -- Found BISON: /usr/bin/bison (found version "3.5.1")
    -- Found FLEX: /usr/bin/flex (found version "2.6.4")
    -- Looking for pthread_setname_np
    -- Looking for pthread_setname_np - found
    -- Looking for sys/types.h
    -- Looking for sys/types.h - found
    -- Looking for stdint.h
    -- Looking for stdint.h - found
    -- Looking for stddef.h
    -- Looking for stddef.h - found
    -- Check size of struct usb_functionfs_descs_head_v2
    -- Check size of struct usb_functionfs_descs_head_v2 - done
    -- Features enabled : xml network dns-sd avahi ipv6 serial local local-mmap hwmon usb utils iiod udev-rule iiod-serial iiod-aio iiod-usb man-utils
    -- Features disabled: zstd bonjour examples c++-bindings iiod-systemd iiod-sysvinit iiod-upstart doc man python-bindings c#-bindings
    -- Configuring done
    -- Generating done
    -- Build files have been written to :path/to/liibio/build
    

    path/to/libiio/build$ sudo make install

    path/to/libiio/build$ sudo make install
    [ 41%] Built target iio
    [ 47%] Built target iio_tests_helper
    [ 52%] Built target iio_genxml
    [ 56%] Built target iio_writedev
    [ 60%] Built target iio_stresstest
    [ 64%] Built target iio_info
    [ 68%] Built target iio_attr
    [ 72%] Built target iio_readdev
    [ 77%] Built target iio_reg
    [100%] Built target iiod
    Install the project...
    -- Install configuration: "RelWithDebInfo"
    -- Installing: /usr/lib/x86_64-linux-gnu/pkgconfig/libiio.pc
    -- Installing: /usr/lib/x86_64-linux-gnu/libiio.so.0.25
    -- Up-to-date: /usr/lib/x86_64-linux-gnu/libiio.so.0
    -- Up-to-date: /usr/lib/x86_64-linux-gnu/libiio.so
    -- Installing: /usr/include/iio.h
    -- Installing: /lib/udev/rules.d/90-libiio.rules
    -- Installing: /usr/bin/iio_genxml
    -- Set runtime path of "/usr/bin/iio_genxml" to ""
    -- Installing: /usr/bin/iio_info
    -- Set runtime path of "/usr/bin/iio_info" to ""
    -- Installing: /usr/bin/iio_attr
    -- Set runtime path of "/usr/bin/iio_attr" to ""
    -- Installing: /usr/bin/iio_readdev
    -- Set runtime path of "/usr/bin/iio_readdev" to ""
    -- Installing: /usr/bin/iio_reg
    -- Set runtime path of "/usr/bin/iio_reg" to ""
    -- Installing: /usr/bin/iio_writedev
    -- Set runtime path of "/usr/bin/iio_writedev" to ""
    -- Installing: /usr/bin/iio_stresstest
    -- Set runtime path of "/usr/bin/iio_stresstest" to ""
    -- Installing: /usr/sbin/iiod
    -- Set runtime path of "/usr/sbin/iiod" to ""

    path/to/iio-oscilloscope/build$ cmake ../ && make -j $(nproc)

    path/to/iio-oscilloscope/build$ cmake ../ && make -j $(nproc)
    -- The C compiler identification is GNU 9.4.0
    -- Check for working C compiler: /usr/bin/cc
    -- Check for working C compiler: /usr/bin/cc -- works
    -- Detecting C compiler ABI info
    -- Detecting C compiler ABI info - done
    -- Detecting C compile features
    -- Detecting C compile features - done
    -- Found Git: /usr/bin/git (found version "2.25.1")
    -- Found PkgConfig: /usr/bin/pkg-config (found version "0.29.1")
    -- Checking for module 'glib-2.0'
    --   Found glib-2.0, version 2.64.6
    -- Checking for module 'gtk+-3.0'
    --   Found gtk+-3.0, version 3.24.20
    -- Checking for module 'gthread-2.0'
    --   Found gthread-2.0, version 2.64.6
    -- Checking for module 'gtkdatabox'
    --   Found gtkdatabox, version 1.0.0
    -- Checking for module 'fftw3'
    --   Found fftw3, version 3.3.8
    -- Checking for module 'libxml-2.0'
    --   Found libxml-2.0, version 2.9.10
    -- Checking for module 'libcurl'
    --   Found libcurl, version 7.68.0
    -- Checking for module 'jansson'
    --   Found jansson, version 2.12
    -- Checking for module 'matio'
    --   Found matio, version 1.5.17
    -- Configuring done
    -- Generating done
    -- Build files have been written to: /path/to/iio-oscilloscope/build
    Scanning dependencies of target osc
    [  1%] Building C object CMakeFiles/osc.dir/osc.c.o
    [  8%] Building C object CMakeFiles/osc.dir/datatypes.c.o
    [  8%] Building C object CMakeFiles/osc.dir/oscplot.c.o
    [  8%] Building C object CMakeFiles/osc.dir/iio_utils.c.o
    [  8%] Building C object CMakeFiles/osc.dir/fru.c.o
    [  8%] Building C object CMakeFiles/osc.dir/iio_widget.c.o
    [  9%] Building C object CMakeFiles/osc.dir/dialogs.c.o
    [  9%] Building C object CMakeFiles/osc.dir/trigger_dialog.c.o
    [ 10%] Building C object CMakeFiles/osc.dir/xml_utils.c.o
    [ 12%] Building C object CMakeFiles/osc.dir/libini/libini.c.o
    [ 13%] Building C object CMakeFiles/osc.dir/libini2.c.o
    [ 14%] Building C object CMakeFiles/osc.dir/phone_home.c.o
    [ 15%] Building C object CMakeFiles/osc.dir/plugins/dac_data_manager.c.o
    [ 16%] Building C object CMakeFiles/osc.dir/plugins/fir_filter.c.o
    [ 18%] Building C object CMakeFiles/osc.dir/eeprom.c.o
    [ 19%] Building C object CMakeFiles/osc.dir/osc_preferences.c.o
    [ 20%] Linking C shared library libosc.so
    [ 20%] Built target osc
    Scanning dependencies of target adrv9002
    Scanning dependencies of target ad6676
    Scanning dependencies of target fmcadc3
    Scanning dependencies of target cf_axi_tdd
    Scanning dependencies of target ad9371_adv
    Scanning dependencies of target xmw
    Scanning dependencies of target fmcomms6
    Scanning dependencies of target oscmain
    [ 21%] Building C object plugins/CMakeFiles/xmw.dir/xmw.c.o
    [ 22%] Building C object plugins/CMakeFiles/cf_axi_tdd.dir/cf_axi_tdd.c.o
    [ 28%] Building C object plugins/CMakeFiles/fmcadc3.dir/fmcadc3.c.o
    [ 28%] Building C object plugins/CMakeFiles/adrv9002.dir/adrv9002.c.o
    [ 28%] Building C object plugins/CMakeFiles/fmcomms6.dir/fmcomms6.c.o
    [ 28%] Building C object CMakeFiles/oscmain.dir/oscmain.c.o
    [ 28%] Building C object plugins/CMakeFiles/ad6676.dir/ad6676.c.o
    [ 30%] Building C object plugins/CMakeFiles/ad9371_adv.dir/ad9371_adv.c.o
    [ 31%] Linking C shared library cf_axi_tdd.so
    [ 32%] Linking C shared library xmw.so
    [ 33%] Linking C shared library fmcadc3.so
    [ 34%] Linking C shared library fmcomms6.so
    [ 36%] Linking C shared library ad6676.so
    [ 37%] Linking C executable osc
    [ 38%] Linking C shared library ad9371_adv.so
    [ 38%] Built target cf_axi_tdd
    [ 38%] Built target fmcadc3
    [ 38%] Built target xmw
    [ 38%] Built target fmcomms6
    Scanning dependencies of target adrv9009_adv
    Scanning dependencies of target lidar
    Scanning dependencies of target fmcomms2_adv
    Scanning dependencies of target fmcomms11
    [ 38%] Built target ad6676
    Scanning dependencies of target pr_config
    [ 39%] Linking C shared library adrv9002.so
    [ 39%] Built target ad9371_adv
    Scanning dependencies of target fmcomms1
    [ 39%] Built target adrv9002
    Scanning dependencies of target adrv9009
    [ 39%] Built target oscmain
    Scanning dependencies of target fmcomms5
    [ 40%] Building C object plugins/CMakeFiles/lidar.dir/lidar.c.o
    [ 42%] Building C object plugins/CMakeFiles/adrv9009_adv.dir/adrv9009_adv.c.o
    [ 44%] Building C object plugins/CMakeFiles/fmcomms11.dir/fmcomms11.c.o
    [ 44%] Building C object plugins/CMakeFiles/fmcomms2_adv.dir/fmcomms2_adv.c.o
    [ 45%] Building C object plugins/CMakeFiles/pr_config.dir/pr_config.c.o
    [ 46%] Building C object plugins/CMakeFiles/fmcomms1.dir/fmcomms1.c.o
    [ 48%] Building C object plugins/CMakeFiles/adrv9009.dir/adrv9009.c.o
    [ 49%] Building C object plugins/CMakeFiles/fmcomms5.dir/fmcomms5.c.o
    [ 50%] Linking C shared library lidar.so
    [ 51%] Linking C shared library fmcomms11.so
    [ 53%] Linking C shared library pr_config.so
    [ 54%] Linking C shared library adrv9009_adv.so
    [ 55%] Linking C shared library fmcomms2_adv.so
    [ 55%] Built target lidar
    [ 55%] Built target fmcomms11
    Scanning dependencies of target cn0540
    [ 55%] Built target pr_config
    Scanning dependencies of target generic_dac
    [ 55%] Built target adrv9009_adv
    Scanning dependencies of target ad9371
    Scanning dependencies of target scpi
    [ 55%] Built target fmcomms2_adv
    Scanning dependencies of target ad9739a
    [ 56%] Linking C shared library fmcomms1.so
    [ 57%] Linking C shared library adrv9009.so
    [ 59%] Linking C shared library fmcomms5.so
    [ 59%] Built target fmcomms1
    [ 59%] Built target adrv9009
    Scanning dependencies of target daq2
    Scanning dependencies of target dmm
    [ 59%] Built target fmcomms5
    Scanning dependencies of target AD5628_1
    [ 60%] Building C object plugins/CMakeFiles/cn0540.dir/cn0540.c.o
    [ 61%] Building C object plugins/CMakeFiles/generic_dac.dir/generic_dac.c.o
    [ 62%] Building C object plugins/CMakeFiles/scpi.dir/scpi.c.o
    [ 63%] Building C object plugins/CMakeFiles/ad9371.dir/ad9371.c.o
    [ 65%] Building C object plugins/CMakeFiles/ad9739a.dir/ad9739a.c.o
    [ 66%] Linking C shared library generic_dac.so
    [ 67%] Linking C shared library cn0540.so
    [ 67%] Built target generic_dac
    Scanning dependencies of target fmcomms2
    [ 68%] Linking C shared library scpi.so
    [ 69%] Linking C shared library ad9739a.so
    [ 69%] Built target cn0540
    [ 71%] Building C object plugins/CMakeFiles/dmm.dir/dmm.c.o
    [ 72%] Building C object plugins/CMakeFiles/daq2.dir/daq2.c.o
    Scanning dependencies of target spectrum_analyzer
    [ 73%] Building C object plugins/CMakeFiles/AD5628_1.dir/AD5628_1.c.o
    [ 74%] Linking C shared library ad9371.so
    [ 74%] Built target scpi
    Scanning dependencies of target cn0357
    [ 74%] Built target ad9739a
    Scanning dependencies of target cn0508
    [ 75%] Linking C shared library AD5628_1.so
    [ 75%] Built target ad9371
    [ 77%] Linking C shared library dmm.so
    Scanning dependencies of target ad9084
    [ 78%] Linking C shared library daq2.so
    [ 78%] Built target AD5628_1
    [ 78%] Built target dmm
    Scanning dependencies of target ad9081
    Scanning dependencies of target cn0511
    [ 78%] Built target daq2
    Scanning dependencies of target motor_control
    [ 79%] Building C object plugins/CMakeFiles/fmcomms2.dir/fmcomms2.c.o
    [ 80%] Building C object plugins/CMakeFiles/spectrum_analyzer.dir/spectrum_analyzer.c.o
    [ 81%] Building C object plugins/CMakeFiles/cn0357.dir/cn0357.c.o
    [ 83%] Building C object plugins/CMakeFiles/cn0508.dir/cn0508.c.o
    [ 84%] Linking C shared library spectrum_analyzer.so
    [ 85%] Building C object plugins/CMakeFiles/ad9084.dir/ad9084.c.o
    [ 86%] Linking C shared library cn0357.so
    [ 89%] Building C object plugins/CMakeFiles/ad9081.dir/ad9081.c.o
    [ 89%] Building C object plugins/CMakeFiles/cn0511.dir/cn0511.c.o
    [ 90%] Linking C shared library cn0508.so
    [ 90%] Built target spectrum_analyzer
    Scanning dependencies of target debug
    [ 91%] Building C object plugins/CMakeFiles/motor_control.dir/motor_control.c.o
    [ 92%] Linking C shared library fmcomms2.so
    [ 92%] Built target cn0357
    [ 92%] Built target cn0508
    [ 93%] Linking C shared library ad9084.so
    [ 95%] Linking C shared library cn0511.so
    [ 95%] Built target fmcomms2
    [ 96%] Linking C shared library ad9081.so
    [ 96%] Built target ad9084
    [ 96%] Built target cn0511
    [ 96%] Built target ad9081
    [ 97%] Linking C shared library motor_control.so
    [ 97%] Built target motor_control
    [ 98%] Building C object plugins/CMakeFiles/debug.dir/debug.c.o
    [100%] Linking C shared library debug.so
    [100%] Built target debug

    Do you have any other possible solutions to this problem?

    I also tried to install IIO oscilloscope with this link on a windows laptop but I get the following error:

    Is there any other software to install or is the problem with the USRP E312?


    Thank you very much,

    Regards,

    Rémi

Children