Post Go back to editing

Using MAX30003 with MAX32630

Thread Summary

The user inquired about software drivers for the MAX30003 with the MAX32630. The support engineer confirmed that no official driver or project exists for this combination, and the MAX32630 is not supported by the Maxim Micros SDK. The user encountered issues with the MAX_IOT_KIT project and Mbed Studio, but no specific solutions were provided for these issues.
AI Generated Content
Category: Software
Product Number: MAX30003 MAX32630

Hi Support team,

My customer is using MAX30003 with MAX32630, but they can't find a right software driver.

1. Do we provide workable software driver project with source codes for MAX30003 with MAX32630?

2. Do we provide workable binary or hex file?

The customer tried "MAX_IOT_KIT" project on ARM official website and Keil Studio Online. They can build the project successfully, but can't load or run on the board. It shows "DAP-link" issues.

They also tried "Mbed studio" but the compile error message is "[ERROR] cannot use a string pattern on a bytes-like object"

Thank you.

BR, William

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.