Post Go back to editing

Error occurs in generic.mk, Failure of the SDK project, no-OS (2019_r2)

Category: Software
Product Number: AD9467_EVAL_BOARD
Software Version: NO_OS (2019_R2)

Greetings, Microcontroller Team

Additionally, we attempted to create the no-OS (2019.1) project in the SDK using both the command line window and the Xilinx Software Command Line Tool 2019.1.


However, we are also having problems with the *generic.mk* file located in the *no-OS/tools/scripts* directory.

We also turn on the Zynq7020 Xilinx carrier and the AD9467 FMC 250 EBZ.

Please take a look at my problems with the SDK project failure creation.



Thanks

Abbas Ali

FPGA Engineer