Post Go back to editing
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Running ad9467_fmc_ebz.c test cases and most of tests are failing

Category: Software
Product Number: AD9467_EVAL_BOARD
Software Version: NO_OS (2018_R2)

We are using the following hardware:

  1. ADC9467 Eval board:
  2. Software: Xilinx SDK 2018.2
  3. Version: NO_OS (2018_R2) 

We take input from discovery 2 waveforms software setup shown below


SDK Terminal shows below response

*****************************************************

*****************************************************


ADI AD9467-FMC-EBZ Reference Design


AD9467 CHIP ID: 0x50


AD9467 CHIP GRADE: 0x20


AD9517 CHIP ID: 0x4d3d3d3


*****************************************************

adc_setup adc core initialized (1 MHz).
AD9467[0x016]: 00

adc_delay: setting zero error delay (5)

Error field (0=success, 1=fail):
00000000000011111111111111111111
ADC Test: mode - MIDSCALE


format - OFFSET BINARY


Test passed


ADC Test: mode - MIDSCALE


format - TWOS_COMPLEMENT


ERROR[ 0]: rcv(80008000), exp(00000000)


ERROR[ 1]: rcv(80008000), exp(00000000)

ERROR[ 2]: rcv(80008000), exp(00000000)


ERROR[ 3]: rcv(80008000), exp(00000000)


ERROR[ 4]: rcv(80008000), exp(00000000)


ERROR[ 5]: rcv(80008000), exp(00000000)

ERROR[ 6]: rcv(80008000), exp(00000000)


ERROR[ 7]: rcv(80008000), exp(00000000)

ERROR[ 8]: rcv(80008000), exp(00000000)


ERROR[ 9]: rcv(80008000), exp(00000000)


ERROR[10]: rcv(80008000), exp(00000000)


ERROR[11]: rcv(80008000), exp(00000000)

ERROR[12]: rcv(80008000), exp(00000000)

ERROR[13]: rcv(80008000), exp(00000000)

ERROR[14]: rcv(80008000), exp(00000000)

ERROR[15]: rcv(80008000), exp(00000000)

ERROR[16]: rcv(80008000), exp(00000000)

ERROR[17]: rcv(80008000), exp(00000000)


ERROR[18]: rcv(80008000), exp(00000000)


ERROR[19]: rcv(80008000), exp(00000000)


ERROR[20]: rcv(80008000), exp(00000000)

ERROR[21]: rcv(80008000), exp(00000000)


ERROR[22]: rcv(80008000), exp(00000000)


ERROR[23]: rcv(80008000), exp(00000000)


ERROR[24]: rcv(80008000), exp(00000000)


ERROR[25]: rcv(80008000), exp(00000000)

ERROR[26]: rcv(80008000), exp(00000000)


ERROR[27]: rcv(80008000), exp(00000000)


ERROR[28]: rcv(80008000), exp(00000000)


ERROR[29]: rcv(80008000), exp(00000000)


ERROR[30]: rcv(80008000), exp(00000000)


ERROR[31]: rcv(80008000), exp(00000000)

Testing done.

Start capturing data...

Done.

-----------------------------------------------------

We successfully generated bitstream from the hdl_2018_R2 from https://github.com/analogdevicesinc/hdl/tree/hdl_2018_r2. 

Kindly inform tell us about the Error shown in the SDK terminal.

Plz help ASAP




[locked by: buha at 1:24 PM (GMT -5) on 24 Feb 2023]
Parents Reply Children
No Data