AD7771
Recommended for New Designs
The AD7771 is an 8-channel, simultaneous sampling analog-to-digital converter (ADC). Eight full Σ-Δ ADCs are on-chip. The AD7771 provides an ultralow...
Datasheet
AD7771 on Analog.com
Hello Team,
Can anyone send me sample project to interface AD7771 to STM32 platform for my reference
With Regards,
Aalakh
I am using no_os ad7779 driver with STM32H745 MCU
Facing following issues in stm32_spi.c source file.
'SPI_CR1_BR_Pos' undeclared (first use in this function); did you mean 'SPI_CFG1_MBR_Pos'?
'SPI_SR_RXNE' undeclared (first use in this function); did you mean 'SPI_SR_RXWNE'?
'SPI_SR_TXE' undeclared (first use in this function); did you mean 'SPI_SR_TXP'?
'SPI_TypeDef' has no member named 'DR'; did you mean 'SR'?
Macros are not defined in stm32h7xx_hal.h
DR is not a member in SPI_TypeDef
Can you please check and confirm whether these drivers supports stm32H7 platform
Hi Aalakh ,
I believe the drivers do not support the STM32H7 platform.
But as a temporary solution, the macro SPI_CR1_BR_Pos can be replaced with the SPI_CFG1_MBR_Pos.
The stm32_spi_write_and_read() function can be replaced with the following:
int32_t stm32_spi_write_and_read(struct spi_desc *desc, uint8_t *data, uint16_t bytes_number) { int32_t ret; struct stm32_spi_desc *sdesc; if (!desc || !desc->extra || !data) return -EINVAL; if (!bytes_number) return 0; sdesc = desc->extra; ret = gpio_set_value(sdesc->chip_select, GPIO_LOW); if (ret < 0) goto error; ret = HAL_SPI_TransmitReceive(&sdesc->hspi, data, data, bytes_number, HAL_MAX_DELAY); if (ret != HAL_OK) { if (ret == HAL_TIMEOUT) ret = -ETIMEDOUT; else ret = -EIO; } error: return gpio_set_value(sdesc->chip_select, GPIO_HIGH); }
Hi can you provide conversion of raw ADC counts to input voltage formula for bipolar input configuration?
Hi Aalakh ,
The data output format for this part is Two's complement. The following thread might help more on this.
Right now it is developed for polling method.
Do you have driver with DMA method or any suggestion to make it work with DMA
Aalakh - we do not have this implementation using SPI DMA.
The TDM Mode in this code works with the support of DMA
Aalakh - we do not have this implementation using SPI DMA.
The TDM Mode in this code works with the support of DMA