Post Go back to editing

AD7771 STM32 sample project example

Thread Summary

The user requested a sample project to interface the AD7771 with the STM32 platform. The final answer provided a link to a thread discussing the data output format in Two's complement and suggested a temporary workaround for macro and member issues in the STM32H745 MCU by replacing specific SPI macros and using the HAL_SPI_TransmitReceive function. The user also inquired about converting raw ADC counts to input voltage for bipolar input configuration and asked for a DMA-based driver, but no such implementation was available. Additionally, the user sought resources for interfacing the ESP32 with the AD4111 IC, but no specific resources were provided.
AI Generated Content
Category: Software
Product Number: AD7771

Hello Team,

Can anyone send me sample project to interface AD7771 to STM32 platform for my reference

With Regards,

Aalakh

Parents Reply
  • I am using no_os ad7779 driver with STM32H745 MCU

    Facing following issues in stm32_spi.c source file.

    'SPI_CR1_BR_Pos' undeclared (first use in this function); did you mean 'SPI_CFG1_MBR_Pos'?

    'SPI_SR_RXNE' undeclared (first use in this function); did you mean 'SPI_SR_RXWNE'?

    'SPI_SR_TXE' undeclared (first use in this function); did you mean 'SPI_SR_TXP'?  

    'SPI_TypeDef' has no member named 'DR'; did you mean 'SR'?    

     

    Macros are not defined in stm32h7xx_hal.h

    DR is not a member in SPI_TypeDef

     

    Can you please check and confirm whether these drivers supports stm32H7 platform

Children