Post Go back to editing

AD9081 reset/init error with custom som

Category: Hardware

Hi,

We are trying to run the AD9081 zcu102 reference design on the som we just received.

The only difference between the chip on the som and the chip on the zcu102 is grade. Chip on som = XCZU9EG-2FFVB1156I , on zcu102 = XCZU9EG-2FFVB1156E.

After opening the reference design we produced for the zcu102, we changed the chip part from the project setting menu.
When I tried with psu_init.tcl instead of FSBL, I was able to run it without any errors. However, this time I got the ad9081 reset/init fail error.

I will be glad if you can help me solve this error. Also, if you have a suggested method to transfer the design to som, please share it.
Any help will be appreciated.

Som User manual : all pin definitions are here.(fmc etc.)

som user manual

FMC xdc which i use for som.

#
## mxfe
#

set_property         -dict {PACKAGE_PIN Y5   IOSTANDARD LVCMOS18                                     } [get_ports agc0[0]          ]    ; ## FMC0_LA17_CC_P      IO_L13P_T2L_N0_GC_QBC_67   
set_property         -dict {PACKAGE_PIN AA5   IOSTANDARD LVCMOS18                                     } [get_ports agc0[1]          ]    ; ## FMC0_LA17_CC_N      IO_L13N_T2L_N1_GC_QBC_67
set_property         -dict {PACKAGE_PIN Y8    IOSTANDARD LVCMOS18                                     } [get_ports agc1[0]          ]    ; ## FMC0_LA18_CC_P      IO_L16P_T2U_N6_QBC_AD3P_67
set_property         -dict {PACKAGE_PIN Y7    IOSTANDARD LVCMOS18                                     } [get_ports agc1[1]          ]    ; ## FMC0_LA18_CC_N      IO_L16N_T2U_N7_QBC_AD3N_67
set_property         -dict {PACKAGE_PIN V2   IOSTANDARD LVCMOS18                                     } [get_ports agc2[0]          ]    ; ## FMC0_LA20_P         IO_L22P_T3U_N6_DBC_AD0P_67
set_property         -dict {PACKAGE_PIN V1   IOSTANDARD LVCMOS18                                     } [get_ports agc2[1]          ]    ; ## FMC0_LA20_N         IO_L22N_T3U_N7_DBC_AD0N_67
set_property         -dict {PACKAGE_PIN Y2   IOSTANDARD LVCMOS18                                     } [get_ports agc3[0]          ]    ; ## FMC0_LA21_P         IO_L21P_T3L_N4_AD8P_67
set_property         -dict {PACKAGE_PIN Y1   IOSTANDARD LVCMOS18                                     } [get_ports agc3[1]          ]    ; ## FMC0_LA21_N         IO_L21N_T3L_N5_AD8N_67
set_property         -dict {PACKAGE_PIN R8    IOSTANDARD LVDS     DIFF_TERM_ADV TERM_100 DQS_BIAS TRUE} [get_ports clkin10_n        ]    ; ## FMC0_CLK2_IO_N      IO_L13N_T2L_N1_GC_QBC_66 
set_property         -dict {PACKAGE_PIN T8    IOSTANDARD LVDS     DIFF_TERM_ADV TERM_100 DQS_BIAS TRUE} [get_ports clkin10_p        ]    ; ## FMC0_CLK2_IO_P      IO_L13P_T2L_N0_GC_QBC_66 
set_property         -dict {PACKAGE_PIN Y3    IOSTANDARD LVDS     DIFF_TERM_ADV TERM_100 DQS_BIAS TRUE} [get_ports clkin6_n         ]    ; ## FMC0_CLK1_M2C_N     IO_L12N_T1U_N11_GC_67
set_property         -dict {PACKAGE_PIN Y4    IOSTANDARD LVDS     DIFF_TERM_ADV TERM_100 DQS_BIAS TRUE} [get_ports clkin6_p         ]    ; ## FMC0_CLK1_M2C_P     IO_L12P_T1U_N10_GC_67
set_property         -dict {PACKAGE_PIN G28                                                            } [get_ports fpga_refclk_in_n ]    ; ## FMC0_GBTCLK0_M2C_N  MGTREFCLK0N_229
set_property         -dict {PACKAGE_PIN G27                                                            } [get_ports fpga_refclk_in_p ]    ; ## FMC0_GBTCLK0_M2C_P  MGTREFCLK0P_229
set_property  -quiet -dict {PACKAGE_PIN C32                                                            } [get_ports rx_data_n[2]     ]    ; ## FMC0_DP2_M2C_N      MGTHRXN3_229    FPGA_SERDIN_0_N
set_property  -quiet -dict {PACKAGE_PIN C31                                                            } [get_ports rx_data_p[2]     ]    ; ## FMC0_DP2_M2C_P      MGTHRXP3_229    FPGA_SERDIN_0_P
set_property  -quiet -dict {PACKAGE_PIN E32                                                            } [get_ports rx_data_n[0]     ]    ; ## FMC0_DP0_M2C_N      MGTHRXN2_229    FPGA_SERDIN_1_N
set_property  -quiet -dict {PACKAGE_PIN E31                                                            } [get_ports rx_data_p[0]     ]    ; ## FMC0_DP0_M2C_P      MGTHRXP2_229    FPGA_SERDIN_1_P
set_property  -quiet -dict {PACKAGE_PIN F34                                                            } [get_ports rx_data_n[7]     ]    ; ## FMC0_DP7_M2C_N      MGTHRXN2_228    FPGA_SERDIN_2_N
set_property  -quiet -dict {PACKAGE_PIN F33                                                            } [get_ports rx_data_p[7]     ]    ; ## FMC0_DP7_M2C_P      MGTHRXP2_228    FPGA_SERDIN_2_P
set_property  -quiet -dict {PACKAGE_PIN H34                                                            } [get_ports rx_data_n[6]     ]    ; ## FMC0_DP6_M2C_N      MGTHRXN0_228    FPGA_SERDIN_3_N
set_property  -quiet -dict {PACKAGE_PIN H33                                                            } [get_ports rx_data_p[6]     ]    ; ## FMC0_DP6_M2C_P      MGTHRXP0_228    FPGA_SERDIN_3_P
set_property  -quiet -dict {PACKAGE_PIN K34                                                            } [get_ports rx_data_n[5]     ]    ; ## FMC0_DP5_M2C_N      MGTHRXN1_228    FPGA_SERDIN_4_N
set_property  -quiet -dict {PACKAGE_PIN K33                                                            } [get_ports rx_data_p[5]     ]    ; ## FMC0_DP5_M2C_P      MGTHRXP1_228    FPGA_SERDIN_4_P
set_property  -quiet -dict {PACKAGE_PIN L32                                                            } [get_ports rx_data_n[4]     ]    ; ## FMC0_DP4_M2C_N      MGTHRXN3_228    FPGA_SERDIN_5_N
set_property  -quiet -dict {PACKAGE_PIN L31                                                            } [get_ports rx_data_p[4]     ]    ; ## FMC0_DP4_M2C_P      MGTHRXP3_228    FPGA_SERDIN_5_P
set_property  -quiet -dict {PACKAGE_PIN B34                                                            } [get_ports rx_data_n[3]     ]    ; ## FMC0_DP3_M2C_N      MGTHRXN0_229    FPGA_SERDIN_6_N
set_property  -quiet -dict {PACKAGE_PIN B33                                                            } [get_ports rx_data_p[3]     ]    ; ## FMC0_DP3_M2C_P      MGTHRXP0_229    FPGA_SERDIN_6_P
set_property  -quiet -dict {PACKAGE_PIN D34                                                            } [get_ports rx_data_n[1]     ]    ; ## FMC0_DP1_M2C_N      MGTHRXN1_229    FPGA_SERDIN_7_N
set_property  -quiet -dict {PACKAGE_PIN D33                                                            } [get_ports rx_data_p[1]     ]    ; ## FMC0_DP1_M2C_P      MGTHRXP1_229    FPGA_SERDIN_7_P
set_property  -quiet -dict {PACKAGE_PIN F30                                                            } [get_ports tx_data_n[0]     ]    ; ## FMC0_DP0_C2M_N      MGTHTXN2_229    FPGA_SERDOUT_0_N
set_property  -quiet -dict {PACKAGE_PIN F29                                                            } [get_ports tx_data_p[0]     ]    ; ## FMC0_DP0_C2M_P      MGTHTXP2_229    FPGA_SERDOUT_0_P
set_property  -quiet -dict {PACKAGE_PIN B30                                                            } [get_ports tx_data_n[2]     ]    ; ## FMC0_DP2_C2M_N      MGTHTXN3_229    FPGA_SERDOUT_1_N
set_property  -quiet -dict {PACKAGE_PIN B29                                                            } [get_ports tx_data_p[2]     ]    ; ## FMC0_DP2_C2M_P      MGTHTXP3_229    FPGA_SERDOUT_1_P
set_property  -quiet -dict {PACKAGE_PIN G32                                                            } [get_ports tx_data_n[7]     ]    ; ## FMC0_DP7_C2M_N      MGTHTXN2_228    FPGA_SERDOUT_2_N
set_property  -quiet -dict {PACKAGE_PIN G31                                                            } [get_ports tx_data_p[7]     ]    ; ## FMC0_DP7_C2M_P      MGTHTXP2_228    FPGA_SERDOUT_2_P
set_property  -quiet -dict {PACKAGE_PIN H30                                                            } [get_ports tx_data_n[6]     ]    ; ## FMC0_DP6_C2M_N      MGTHTXN0_228    FPGA_SERDOUT_3_N
set_property  -quiet -dict {PACKAGE_PIN H29                                                            } [get_ports tx_data_p[6]     ]    ; ## FMC0_DP6_C2M_P      MGTHTXP0_228    FPGA_SERDOUT_3_P
set_property  -quiet -dict {PACKAGE_PIN D30                                                            } [get_ports tx_data_n[1]     ]    ; ## FMC0_DP1_C2M_N      MGTHTXN1_229    FPGA_SERDOUT_4_N
set_property  -quiet -dict {PACKAGE_PIN D29                                                            } [get_ports tx_data_p[1]     ]    ; ## FMC0_DP1_C2M_P      MGTHTXP1_229    FPGA_SERDOUT_4_P
set_property  -quiet -dict {PACKAGE_PIN J32                                                            } [get_ports tx_data_n[5]     ]    ; ## FMC0_DP5_C2M_N      MGTHTXN1_228    FPGA_SERDOUT_5_N
set_property  -quiet -dict {PACKAGE_PIN J31                                                            } [get_ports tx_data_p[5]     ]    ; ## FMC0_DP5_C2M_P      MGTHTXP1_228    FPGA_SERDOUT_5_P
set_property  -quiet -dict {PACKAGE_PIN K30                                                            } [get_ports tx_data_n[4]     ]    ; ## FMC0_DP4_C2M_N      MGTHTXN3_228    FPGA_SERDOUT_6_N
set_property  -quiet -dict {PACKAGE_PIN K29                                                            } [get_ports tx_data_p[4]     ]    ; ## FMC0_DP4_C2M_P      MGTHTXP3_228    FPGA_SERDOUT_6_P
set_property  -quiet -dict {PACKAGE_PIN A32                                                            } [get_ports tx_data_n[3]     ]    ; ## FMC0_DP3_C2M_N      MGTHTXN0_229    FPGA_SERDOUT_7_N
set_property  -quiet -dict {PACKAGE_PIN A31                                                            } [get_ports tx_data_p[3]     ]    ; ## FMC0_DP3_C2M_P      MGTHTXP0_229    FPGA_SERDOUT_7_P
set_property  -quiet -dict {PACKAGE_PIN T6    IOSTANDARD LVDS     DIFF_TERM_ADV TERM_100              } [get_ports fpga_syncin_0_n  ]    ; ## FMC0_LA02_N         IO_L23N_T3U_N9_66
set_property  -quiet -dict {PACKAGE_PIN T7    IOSTANDARD LVDS     DIFF_TERM_ADV TERM_100              } [get_ports fpga_syncin_0_p  ]    ; ## FMC0_LA02_P         IO_L23P_T3U_N8_66
set_property  -quiet -dict {PACKAGE_PIN K12    IOSTANDARD LVCMOS18                                     } [get_ports fpga_syncin_1_n  ]    ; ## FMC0_LA03_N         IO_L22N_T3U_N7_DBC_AD0N_66
set_property  -quiet -dict {PACKAGE_PIN L12    IOSTANDARD LVCMOS18                                     } [get_ports fpga_syncin_1_p  ]    ; ## FMC0_LA03_P         IO_L22P_T3U_N6_DBC_AD0P_66
set_property  -quiet -dict {PACKAGE_PIN N11   IOSTANDARD LVDS                                         } [get_ports fpga_syncout_0_n ]    ; ## FMC0_LA01_CC_N      IO_L16N_T2U_N7_QBC_AD3N_66
set_property  -quiet -dict {PACKAGE_PIN P11   IOSTANDARD LVDS                                         } [get_ports fpga_syncout_0_p ]    ; ## FMC0_LA01_CC_P      IO_L16P_T2U_N6_QBC_AD3P_66
set_property  -quiet -dict {PACKAGE_PIN L11   IOSTANDARD LVCMOS18                                     } [get_ports fpga_syncout_1_n ]    ; ## FMC0_LA06_N         IO_L19N_T3L_N1_DBC_AD9N_66
set_property  -quiet -dict {PACKAGE_PIN M11   IOSTANDARD LVCMOS18                                     } [get_ports fpga_syncout_1_p ]    ; ## FMC0_LA06_P         IO_L19P_T3L_N0_DBC_AD9P_66
set_property         -dict {PACKAGE_PIN V12   IOSTANDARD LVCMOS18                                     } [get_ports gpio[0]          ]    ; ## FMC0_LA15_P         IO_L6P_T0U_N10_AD6P_66
set_property         -dict {PACKAGE_PIN V11    IOSTANDARD LVCMOS18                                     } [get_ports gpio[1]          ]    ; ## FMC0_LA15_N         IO_L6N_T0U_N11_AD6N_66
set_property         -dict {PACKAGE_PIN AA2   IOSTANDARD LVCMOS18                                     } [get_ports gpio[2]          ]    ; ## FMC0_LA19_P         IO_L23P_T3U_N8_67
set_property         -dict {PACKAGE_PIN AA1   IOSTANDARD LVCMOS18                                     } [get_ports gpio[3]          ]    ; ## FMC0_LA19_N         IO_L23N_T3U_N9_67
set_property         -dict {PACKAGE_PIN L16   IOSTANDARD LVCMOS18                                     } [get_ports gpio[4]          ]    ; ## FMC0_LA13_P         IO_L8P_T1L_N2_AD5P_66
set_property         -dict {PACKAGE_PIN K16   IOSTANDARD LVCMOS18                                     } [get_ports gpio[5]          ]    ; ## FMC0_LA13_N         IO_L8N_T1L_N3_AD5N_66
set_property         -dict {PACKAGE_PIN P12   IOSTANDARD LVCMOS18                                     } [get_ports gpio[6]          ]    ; ## FMC0_LA14_P         IO_L7P_T1L_N0_QBC_AD13P_66
set_property         -dict {PACKAGE_PIN N12   IOSTANDARD LVCMOS18                                     } [get_ports gpio[7]          ]    ; ## FMC0_LA14_N         IO_L7N_T1L_N1_QBC_AD13N_66
set_property         -dict {PACKAGE_PIN N9   IOSTANDARD LVCMOS18                                     } [get_ports gpio[8]          ]    ; ## FMC0_LA16_P         IO_L5P_T0U_N8_AD14P_66
set_property         -dict {PACKAGE_PIN N8  IOSTANDARD LVCMOS18                                     } [get_ports gpio[9]          ]    ; ## FMC0_LA16_N         IO_L5N_T0U_N9_AD14N_66
set_property         -dict {PACKAGE_PIN W6   IOSTANDARD LVCMOS18                                     } [get_ports gpio[10]         ]    ; ## FMC0_LA22_N         IO_L20N_T3L_N3_AD1N_67
set_property         -dict {PACKAGE_PIN U8   IOSTANDARD LVCMOS18                                     } [get_ports hmc_gpio1        ]    ; ## FMC0_LA11_N         IO_L10N_T1U_N7_QBC_AD4N_66
set_property         -dict {PACKAGE_PIN U6    IOSTANDARD LVCMOS18                                     } [get_ports hmc_sync         ]    ; ## FMC0_LA07_N         IO_L18N_T2U_N11_AD2N_66
set_property         -dict {PACKAGE_PIN M15    IOSTANDARD LVCMOS18                                     } [get_ports irqb[0]          ]    ; ## FMC0_LA08_P         IO_L17P_T2U_N8_AD10P_66
set_property         -dict {PACKAGE_PIN M14    IOSTANDARD LVCMOS18                                     } [get_ports irqb[1]          ]    ; ## FMC0_LA08_N         IO_L17N_T2U_N9_AD10N_66
set_property         -dict {PACKAGE_PIN V6    IOSTANDARD LVCMOS18                                     } [get_ports rstb             ]    ; ## FMC0_LA07_P         IO_L18P_T2U_N10_AD2P_66
set_property         -dict {PACKAGE_PIN T12    IOSTANDARD LVCMOS18                                     } [get_ports rxen[0]          ]    ; ## FMC0_LA10_P         IO_L15P_T2L_N4_AD11P_66
set_property         -dict {PACKAGE_PIN R12    IOSTANDARD LVCMOS18                                     } [get_ports rxen[1]          ]    ; ## FMC0_LA10_N         IO_L15N_T2L_N5_AD11N_66
set_property         -dict {PACKAGE_PIN N13   IOSTANDARD LVCMOS18                                     } [get_ports spi0_csb         ]    ; ## FMC0_LA05_P         IO_L20P_T3L_N2_AD1P_66
set_property         -dict {PACKAGE_PIN M13   IOSTANDARD LVCMOS18                                     } [get_ports spi0_miso        ]    ; ## FMC0_LA05_N         IO_L20N_T3L_N3_AD1N_66
set_property         -dict {PACKAGE_PIN L13   IOSTANDARD LVCMOS18                                     } [get_ports spi0_mosi        ]    ; ## FMC0_LA04_P         IO_L21P_T3L_N4_AD8P_66
set_property         -dict {PACKAGE_PIN K13   IOSTANDARD LVCMOS18                                     } [get_ports spi0_sclk        ]    ; ## FMC0_LA04_N         IO_L21N_T3L_N5_AD8N_66
set_property         -dict {PACKAGE_PIN L15    IOSTANDARD LVCMOS18                                     } [get_ports spi1_csb         ]    ; ## FMC0_LA12_P         IO_L9P_T1L_N4_AD12P_66
set_property         -dict {PACKAGE_PIN U9   IOSTANDARD LVCMOS18                                     } [get_ports spi1_sclk        ]    ; ## FMC0_LA11_P         IO_L10P_T1U_N6_QBC_AD4P_66
set_property         -dict {PACKAGE_PIN K15    IOSTANDARD LVCMOS18                                     } [get_ports spi1_sdio        ]    ; ## FMC0_LA12_N         IO_L9N_T1L_N5_AD12N_66
set_property         -dict {PACKAGE_PIN P9   IOSTANDARD LVDS     DIFF_TERM_ADV TERM_100 DQS_BIAS TRUE} [get_ports sysref2_n        ]    ; ## FMC0_CLK0_M2C_N     IO_L12N_T1U_N11_GC_66
set_property         -dict {PACKAGE_PIN P10   IOSTANDARD LVDS     DIFF_TERM_ADV TERM_100 DQS_BIAS TRUE} [get_ports sysref2_p        ]    ; ## FMC0_CLK0_M2C_P     IO_L12P_T1U_N10_GC_66
set_property         -dict {PACKAGE_PIN V8    IOSTANDARD LVCMOS18                                     } [get_ports txen[0]          ]    ; ## FMC0_LA09_P         IO_L24P_T3U_N10_66
set_property         -dict {PACKAGE_PIN V7    IOSTANDARD LVCMOS18                                     } [get_ports txen[1]          ]    ; ## FMC0_LA09_N         IO_L24N_T3U_N11_66
set_property         -dict {PACKAGE_PIN E10    IOSTANDARD LVCMOS18                                     } [get_ports fmc_en          ]    ; ## FMC0_LA09_N         IO_L24N_T3U_N11_66



update
[edited by: marktr at 4:19 PM (GMT -5) on 12 Jan 2023]

Top Replies

Parents Reply Children