Hi,
Do you have No-OS STM32F4X and ARDV9003 project sample?
Best Regards
ADRV9003
Production
The ADRV9003 is a highly integrated RF transceiver that has a single-channel transmitter, dual-channel receivers, integrated synthesizers, and digital...
Datasheet
ADRV9003 on Analog.com
Hi,
Do you have No-OS STM32F4X and ARDV9003 project sample?
Best Regards
Nope, you need programmable logic to process data to/from adrv9001 family chips. See the document provided by ConradCollins above.
Hi, When i try to build STM32 (NO-OS) (Ubuntu); I have "No rule to make target" error for xilinx_axi_io.c file in generic.mk:293: recipe for target 'all' failed.
So BilginV I don't get it, do you use STM32 or a pure FPGA hardware ?
Our device is pure FPGA not SoC
STM32
Is STM32 just for the proof of concept, whether you can change carrier frequency and AGC over SPI ?
So BilginV I don't get it, do you use STM32 or a pure FPGA hardware ?
Our device is pure FPGA not SoC
STM32
Is STM32 just for the proof of concept, whether you can change carrier frequency and AGC over SPI ?
Yes, STM32 is just PoC, we want to see STM32 can configure ADRV9003 or not, then we are going to implement same SPI stream via ROM(FPGA) .