My application have RS422 interface. Kindly suggest which microcontroller will suits and how to connect.
Hi SK_Labs ,
There are different design options for implementing such a system. You can take a look at the following device and its associated typical application use.
https://www.analog.com/en/products/max3140.html#product-overview
Regards,
George

In this case can you suggest which micro processor to be used ??
Hi SK_Labs ,
You can use any microcontroller that has a SPI peripheral.
For example, you can use https://www.analog.com/en/products/max32650.html#product-overview
Regards,
George

For example on which pin we can connect RO and DI of MAX3140
Hi SK_Labs ,
You can use SPI0 (pins from P1.23 to P1.29) for the SPI connection, and RO to P2.11 and DI to P2.12, respectively.
Regards,
George
Thanks for your reply.......Is there any less Package Microcontroller is available for this kind of application ?
Thanks for your reply.......Is there any less Package Microcontroller is available for this kind of application ?

On which pin we can connect RE and DE of MAX3140
If you'd like something with less IO pins, please have a look at the MAX32660 ( https://www.analog.com/en/products/max32660.html ).

Kindly check the pin connection and correct if i am connecting wrong
P0.11 to RO,
P0.10 to DI,
P0.12 to DE
P0.13 to RE
P0.4 to P0.7 is for SPI.
okay thanks for your support