Post Go back to editing

AD9528 write register invalid

Category: Hardware
Product Number: AD9528
Software Version: Qt 5.12.11

1、In my ad9258 chip, the 8th pin VCXO_VT pin is always low voltage. The second pin (rfa) and the third pin (rfa_n) have differential signal input.

2、No matter how the register value is modified, out13 always outputs the reference clock input by rfa, but if I write a reset command to 0x000, all registers return to their default values. In addition, how to modify other register values, it seems that the function has not changed. After several times of reading and writing the register, confirm that the register is readable and writable, and after writing the register, write the update command to the box 00f register.

Schematic:

Register Configuration Order:

  • Hi,

    in the future, please entry questions related to the AD9528 functionality in the Clock and Timing section of Engineer Zone.

    I introduced the register values you gave me into the AD9528 evaluation software. I saw the VCXO has 100MHz. This makes REFA to be 50MHz based on your settings:

    PLL2 is not set correctly, so PLL2 should not function. Then, you selected the PLL1 feedback clock to come from PLL2 feedback clock, which does not work. I recommend changing the PLL1 feedback clock to come from the VCXO, bit 2 in register 0x109 set to 1.

    This should help you get PLL1 locked and obtain a clock at OUT13. I attach the stp file I created based on the register configuration you gave. It reflects the change in register 0x109, bit 2.

    <header>
    product = AD9528
    softwareversion = 1.0.0.3
    </header>
    
    <detailed setup information>
    -- PLL1 --
     - Ref A -
        Input Freq: 50.0 MHz
        Ra: 1
        PFD Freq: 50.0 MHz
     - Ref B -
        Powered Down
     - Clk In -
        Osc Freq: 100.0 MHz
        N1: 2
        PFD Freq: 50.0 MHz
    ------------------
    -- PLL2 --
        Input Freq: 100.0 MHz
        R2: /1
        PFD Freq: 100.0 MHz
        N2: 21
        Dist Freq: 2.1 GHz
        M: 4
        VCO Freq: 8.4 GHz
    ----------------------
    -- SysRef --
        Source: Internal Generation
        Freq: 781.25 kHz
    ----------------------
    -- Distribution --
        Input Source: PLL2
        Input Freq: 2.1 GHz
     - Out 0 -
        Input Source: D0
        D0:5
        Output Freq: 420.0 MHz
     - Out 1 -
        Input Source: Sysref
        Output Freq: 781.25 kHz
     - Out 2 -
        Input Source: D2
        D2:5
        Output Freq: 420.0 MHz
     - Out 3 -
        Input Source: Sysref
        Output Freq: 781.25 kHz
     - Out 4 -
        Input Source: D4
        D4:5
        Output Freq: 420.0 MHz
     - Out 5 -
        Input Source: Sysref
        Output Freq: 781.25 kHz
     - Out 6 -
        Input Source: D6
        D6:5
        Output Freq: 420.0 MHz
     - Out 7 -
        Input Source: Sysref
        Output Freq: 781.25 kHz
     - Out 8 -
        Input Source: D8
        D8:5
        Output Freq: 420.0 MHz
     - Out 9 -
        Input Source: Sysref
        Output Freq: 781.25 kHz
     - Out 10 -
        Input Source: D10
        D10:5
        Output Freq: 420.0 MHz
     - Out 11 -
        Input Source: Sysref
        Output Freq: 781.25 kHz
     - Out 12 -
        Input Source: PLL1
        Output Freq: 100.0 MHz
     - Out 13 -
        Input Source: PLL1
        Output Freq: 100.0 MHz
    ----------------------
    </detailed setup information>
    
    <registers>
    Register (Hex),	Value (Hex),	Value (Dec)
    0x0,		0x00,		0
    0x1,		0x00,		0
    0x3,		0x05,		5
    0x4,		0xFF,		255
    0x5,		0x00,		0
    0x6,		0x03,		3
    0xa,		0x00,		0
    0xb,		0x00,		0
    0xc,		0x56,		86
    0xd,		0x04,		4
    0xf,		0x00,		0
    0x100,		0x01,		1
    0x101,		0x00,		0
    0x102,		0x00,		0
    0x103,		0x00,		0
    0x104,		0x02,		2
    0x105,		0x00,		0
    0x106,		0x0A,		10
    0x107,		0x03,		3
    0x108,		0x28,		40
    0x109,		0x04,		4
    0x10a,		0x02,		2
    0x10b,		0x00,		0
    0x200,		0xE6,		230
    0x201,		0x15,		21
    0x202,		0x03,		3
    0x203,		0x01,		1
    0x204,		0x04,		4
    0x205,		0x2A,		42
    0x206,		0x00,		0
    0x207,		0x02,		2
    0x208,		0x14,		20
    0x209,		0x00,		0
    0x300,		0x00,		0
    0x301,		0x00,		0
    0x302,		0x04,		4
    0x303,		0x40,		64
    0x304,		0x00,		0
    0x305,		0x00,		0
    0x306,		0x00,		0
    0x307,		0x00,		0
    0x308,		0x04,		4
    0x309,		0x40,		64
    0x30a,		0x00,		0
    0x30b,		0x00,		0
    0x30c,		0x00,		0
    0x30d,		0x00,		0
    0x30e,		0x04,		4
    0x30f,		0x40,		64
    0x310,		0x00,		0
    0x311,		0x00,		0
    0x312,		0x00,		0
    0x313,		0x00,		0
    0x314,		0x04,		4
    0x315,		0x40,		64
    0x316,		0x00,		0
    0x317,		0x00,		0
    0x318,		0x00,		0
    0x319,		0x00,		0
    0x31a,		0x04,		4
    0x31b,		0x40,		64
    0x31c,		0x00,		0
    0x31d,		0x00,		0
    0x31e,		0x00,		0
    0x31f,		0x00,		0
    0x320,		0x04,		4
    0x321,		0x40,		64
    0x322,		0x00,		0
    0x323,		0x00,		0
    0x324,		0x20,		32
    0x325,		0x00,		0
    0x326,		0x00,		0
    0x327,		0x20,		32
    0x328,		0x00,		0
    0x329,		0x00,		0
    0x32a,		0x00,		0
    0x32b,		0x00,		0
    0x32c,		0x00,		0
    0x32d,		0x00,		0
    0x32e,		0x00,		0
    0x400,		0x00,		0
    0x401,		0x00,		0
    0x402,		0x00,		0
    0x403,		0x00,		0
    0x404,		0x04,		4
    0x500,		0x10,		16
    0x501,		0x00,		0
    0x502,		0x00,		0
    0x503,		0xFF,		255
    0x504,		0xFF,		255
    0x505,		0x00,		0
    0x506,		0x00,		0
    0x507,		0x00,		0
    0x508,		0x00,		0
    0x509,		0x00,		0
    </registers>
    
    <frequencies>
    50000000;122880000;100000000;768000
    </frequencies>
    

    I looked over the schematic and the VCXO connection to the AD9528 reflects the single ended pin VCXO_INP setting in the configuration. 

    Read the registers 0x508 and 0x509 to get info about how the AD9528 sees REFA, VCXO and PLL1 lock/unlock status.

    If you need help setting the PLL2 and/or SYSREF generator, just tell me what outputs you need to obtain and I'll create a configuration for you

    Petre

  • Hi
    Thank you Mr Petre.
    I configured the register according to the way you gave, but still did not solve the problem. My register configuration order is from 0x000 to 0x509, and finally 0x0000f01. If the register configuration has nothing to do with the order, I have to consider whether there is a problem with the schematic design.Thanks again Petre for being able to answer my question.


    Shun
  • HI,

    I recommended in my previous post to check the status registers: Read the registers 0x508 and 0x509 to get info about how the AD9528 sees REFA, VCXO and PLL1 lock/unlock status.

    I do not see any report on this.

    Please check the differential voltage on REFA pins and verify it meets these conditions:

    Petre

  • Hi 

    Thank you Mr Petre.

    I followed your advice to read registers 508, 509. Now I can control the AD9528 due to a problem with my hardware circuit. I really appreciate you giving me this help. Best wishes to you.

    Shun

  • Hi,

    excellent. I'm very happy you made it work. Please feel free to ask me further questions if you need.

    Petre