Category: Software
Product Number: EVAL-AD7175-2
Hi,
I would like to clarify if I still need to define the other parameters for the initialization of AD717x driver. Based on this wiki AD717X No-OS Software Drivers [Analog Devices Wiki], it only calls the spi_init, regs, and num_regs but in the ad717x header file(attached code), I see several parameters. Do I still need to define them all?
typedef struct { /* SPI */ no_os_spi_init_param spi_init; /* Device Settings */ ad717x_st_reg *regs; uint8_t num_regs; /* Active Device */ enum ad717x_device_type active_device; /* Reference Enable */ bool ref_en; /* Number of Channels */ uint8_t num_channels; /* Number of Setups */ uint8_t num_setups; /* Channel Mapping */ struct ad717x_channel_map chan_map[AD717x_MAX_CHANNELS]; /* Setups */ struct ad717x_channel_setup setups[AD717x_MAX_SETUPS]; /* Gain */ uint32_t pga[AD717x_MAX_SETUPS]; /* Filter Configuration */ struct ad717x_filtcon filter_configuration[AD717x_MAX_SETUPS]; /* ADC Mode */ enum ad717x_mode mode; } ad717x_init_param;
Thanks,
Kim