Post Go back to editing

interfacing EVAL-AD7175-2 with MAX32666FTHR

Category: Software
Product Number: EVAL-AD7175-2, MAX32666FTHR
Software Version: Ecilpse MaximSDK

Hi.

I don't know if this is the correct forum to ask this question. Anyway, I want to interface the EVAL-AD7175-2 with a microcontroller particularly the MAX32666FTHR. It seems I was able to understand some of the content in this wiki AD717X No-OS Software Drivers [Analog Devices Wiki] and write some codes but encounter some problem. It would be better if someone could provide a code that could communicate the microcontroller with the AD7175-2 to read the data from the ADC. Thanks

Top Replies

    •  Analog Employees 
    May 31, 2022 in reply to kimedia +2 verified

    Hi ,

    At the moment, only the MAX32650, 655, 660 and 78000 are officially supported by no-OS. However, adding platform drivers for the MAX32666 is a work in progress (you can checkout this branch…

Parents Reply
  • Greetings  

    It looks like the link is valid, but there was a comma right after, which was interpreted as part of the link. Alternatively, you can checkout the staging/max32666 branch in the no-OS repository. Also, I've corrected one mistake in the code from my previous answer (id -> device_id), sorry about that.

    Regards,

    Ciprian

Children
No Data