Post Go back to editing

No-os IIO initialization

Hi,

I am trying to create No-OS IIO with Zedboard+fmcomms.

Vivado 19.1, hdl-19r2, noos-19r2. 

I am using the command make TINYIIOD=y run

After the project is built, the following messages appear in the console at a speed of 115 200:

it was interrupted. Next, there should be messages about starting the server IIOD, but there are no messages. I guess the server is not starting.

If I enter the make run command without TINYIIOD=y the initialization message is not interrupted:

Also I can't get it with an IIO-cope (i don't use parallel with terminal). Tell me what to do next.

thxMetal