Post Go back to editing

ADRV9009-ZU11EG+ADRV2CRR-FMC 10 MHz reference in "no-OS" mode

Hi,

So I got a ADRV9009-ZU11EG mounted on a ADRV2CRR-FMC carrier and  I need to use a 10 MHz from a GPSDO to synchronize it.

We're using completely custom gateware and software to control it so far, based off the Talise no-OS driver and the HMC7044 no-OS driver to configure clocking.

However there doesn't seem to be any such driver for the AD9545 that I need to use to generate a 122.88 MHz reference from the 10 MHz input.

Is there any tool to generate a register config or something to help me configure that chip properly ?

Best regards,

     Sylvain Munaut