Post Go back to editing

sine_lut_iq description with default settings

Hello,

I'm currently running with an fmcomms4-ebz with a zedboard (ad9364 + Xilinx Zync 7000) and I'm trying to setup some IQ Streaming. As a baseline I was hoping to use the included sine wave look up table but there's no description of what the data is/what I should expect. I took the sine_lut_iq values and read the data as 16 bit integers and plotted what should produce a tone 1mhz baseband (using the sampling frequency of 30720000hz pulled from runtime). Is this the expected functionality when cloning down from the repo and using the dam example by defining DAC_DMA_EXAMPLE?

In addition to the first question I noticed that in 2019_R2 the function axi_dac_set_sine_lut was used rather than axi_dac_load_custom_data which is used in the latest master branch to load into memory for the chip to pull from. Is there a suggested path here to get custom data into memory? When running either function using the data from sine_lut_iq I see a clear tone from the local oscillator but nothing else.

Other Configuration Items:

No-OS branch: 2019_R2

No-OS Project: ad9361

HDL Branch: 2019_rel

HDL Project - fmcomms2/zed

app_config.h Definitions:

#define AD9361_DEVICE            0 /* set it 1 if AD9361 device is used, 0 otherwise */
#define AD9364_DEVICE            1 /* set it 1 if AD9364 device is used, 0 otherwise */
#define AD9363A_DEVICE            0 /* set it 1 if AD9363A device is used, 0 otherwise */

#define DAC_DMA_EXAMPLE

IIO Support is disabled.

AD9361 Params:

AD9361_InitParam default_init_param = {
    /* Device selection */
    ID_AD9364,    // dev_sel
    /* Identification number */
    0,        //id_no
    /* Reference Clock */
    40000000UL,    //reference_clk_rate
    /* Base Configuration */
    1,        //two_rx_two_tx_mode_enable *** adi,2rx-2tx-mode-enable
    1,        //one_rx_one_tx_mode_use_rx_num *** adi,1rx-1tx-mode-use-rx-num
    1,        //one_rx_one_tx_mode_use_tx_num *** adi,1rx-1tx-mode-use-tx-num
    1,        //frequency_division_duplex_mode_enable *** adi,frequency-division-duplex-mode-enable
    0,        //frequency_division_duplex_independent_mode_enable *** adi,frequency-division-duplex-independent-mode-enable
    0,        //tdd_use_dual_synth_mode_enable *** adi,tdd-use-dual-synth-mode-enable
    0,        //tdd_skip_vco_cal_enable *** adi,tdd-skip-vco-cal-enable
    0,        //tx_fastlock_delay_ns *** adi,tx-fastlock-delay-ns
    0,        //rx_fastlock_delay_ns *** adi,rx-fastlock-delay-ns
    0,        //rx_fastlock_pincontrol_enable *** adi,rx-fastlock-pincontrol-enable
    0,        //tx_fastlock_pincontrol_enable *** adi,tx-fastlock-pincontrol-enable
    0,        //external_rx_lo_enable *** adi,external-rx-lo-enable
    0,        //external_tx_lo_enable *** adi,external-tx-lo-enable
    5,        //dc_offset_tracking_update_event_mask *** adi,dc-offset-tracking-update-event-mask
    6,        //dc_offset_attenuation_high_range *** adi,dc-offset-attenuation-high-range
    5,        //dc_offset_attenuation_low_range *** adi,dc-offset-attenuation-low-range
    0x28,    //dc_offset_count_high_range *** adi,dc-offset-count-high-range
    0x32,    //dc_offset_count_low_range *** adi,dc-offset-count-low-range
    0,        //split_gain_table_mode_enable *** adi,split-gain-table-mode-enable
    MAX_SYNTH_FREF,    //trx_synthesizer_target_fref_overwrite_hz *** adi,trx-synthesizer-target-fref-overwrite-hz
    0,        // qec_tracking_slow_mode_enable *** adi,qec-tracking-slow-mode-enable
    /* ENSM Control */
    0,        //ensm_enable_pin_pulse_mode_enable *** adi,ensm-enable-pin-pulse-mode-enable
    0,        //ensm_enable_txnrx_control_enable *** adi,ensm-enable-txnrx-control-enable
    /* LO Control */
    2400000000UL,    //rx_synthesizer_frequency_hz *** adi,rx-synthesizer-frequency-hz
    2200000000UL,    //tx_synthesizer_frequency_hz *** adi,tx-synthesizer-frequency-hz
    1,                //tx_lo_powerdown_managed_enable *** adi,tx-lo-powerdown-managed-enable
    /* Rate & BW Control */
    {983040000, 245760000, 122880000, 61440000, 30720000, 30720000},// rx_path_clock_frequencies[6] *** adi,rx-path-clock-frequencies
    {983040000, 122880000, 122880000, 61440000, 30720000, 30720000},// tx_path_clock_frequencies[6] *** adi,tx-path-clock-frequencies
    18000000,//rf_rx_bandwidth_hz *** adi,rf-rx-bandwidth-hz
    18000000,//rf_tx_bandwidth_hz *** adi,rf-tx-bandwidth-hz
    /* RF Port Control */
    0,        //rx_rf_port_input_select *** adi,rx-rf-port-input-select
    0,        //tx_rf_port_input_select *** adi,tx-rf-port-input-select
    /* TX Attenuation Control */
    10000,    //tx_attenuation_mdB *** adi,tx-attenuation-mdB
    0,        //update_tx_gain_in_alert_enable *** adi,update-tx-gain-in-alert-enable
    /* Reference Clock Control */
    0,        //xo_disable_use_ext_refclk_enable *** adi,xo-disable-use-ext-refclk-enable
    {8, 5920},    //dcxo_coarse_and_fine_tune[2] *** adi,dcxo-coarse-and-fine-tune
    CLKOUT_DISABLE,    //clk_output_mode_select *** adi,clk-output-mode-select
    /* Gain Control */
    2,        //gc_rx1_mode *** adi,gc-rx1-mode
    2,        //gc_rx2_mode *** adi,gc-rx2-mode
    58,        //gc_adc_large_overload_thresh *** adi,gc-adc-large-overload-thresh
    4,        //gc_adc_ovr_sample_size *** adi,gc-adc-ovr-sample-size
    47,        //gc_adc_small_overload_thresh *** adi,gc-adc-small-overload-thresh
    8192,    //gc_dec_pow_measurement_duration *** adi,gc-dec-pow-measurement-duration
    0,        //gc_dig_gain_enable *** adi,gc-dig-gain-enable
    800,    //gc_lmt_overload_high_thresh *** adi,gc-lmt-overload-high-thresh
    704,    //gc_lmt_overload_low_thresh *** adi,gc-lmt-overload-low-thresh
    24,        //gc_low_power_thresh *** adi,gc-low-power-thresh
    15,        //gc_max_dig_gain *** adi,gc-max-dig-gain
    0,        //gc_use_rx_fir_out_for_dec_pwr_meas_enable *** adi,gc-use-rx-fir-out-for-dec-pwr-meas-enable
    /* Gain MGC Control */
    2,        //mgc_dec_gain_step *** adi,mgc-dec-gain-step
    2,        //mgc_inc_gain_step *** adi,mgc-inc-gain-step
    0,        //mgc_rx1_ctrl_inp_enable *** adi,mgc-rx1-ctrl-inp-enable
    0,        //mgc_rx2_ctrl_inp_enable *** adi,mgc-rx2-ctrl-inp-enable
    0,        //mgc_split_table_ctrl_inp_gain_mode *** adi,mgc-split-table-ctrl-inp-gain-mode
    /* Gain AGC Control */
    10,        //agc_adc_large_overload_exceed_counter *** adi,agc-adc-large-overload-exceed-counter
    2,        //agc_adc_large_overload_inc_steps *** adi,agc-adc-large-overload-inc-steps
    0,        //agc_adc_lmt_small_overload_prevent_gain_inc_enable *** adi,agc-adc-lmt-small-overload-prevent-gain-inc-enable
    10,        //agc_adc_small_overload_exceed_counter *** adi,agc-adc-small-overload-exceed-counter
    4,        //agc_dig_gain_step_size *** adi,agc-dig-gain-step-size
    3,        //agc_dig_saturation_exceed_counter *** adi,agc-dig-saturation-exceed-counter
    1000,    // agc_gain_update_interval_us *** adi,agc-gain-update-interval-us
    0,        //agc_immed_gain_change_if_large_adc_overload_enable *** adi,agc-immed-gain-change-if-large-adc-overload-enable
    0,        //agc_immed_gain_change_if_large_lmt_overload_enable *** adi,agc-immed-gain-change-if-large-lmt-overload-enable
    10,        //agc_inner_thresh_high *** adi,agc-inner-thresh-high
    1,        //agc_inner_thresh_high_dec_steps *** adi,agc-inner-thresh-high-dec-steps
    12,        //agc_inner_thresh_low *** adi,agc-inner-thresh-low
    1,        //agc_inner_thresh_low_inc_steps *** adi,agc-inner-thresh-low-inc-steps
    10,        //agc_lmt_overload_large_exceed_counter *** adi,agc-lmt-overload-large-exceed-counter
    2,        //agc_lmt_overload_large_inc_steps *** adi,agc-lmt-overload-large-inc-steps
    10,        //agc_lmt_overload_small_exceed_counter *** adi,agc-lmt-overload-small-exceed-counter
    5,        //agc_outer_thresh_high *** adi,agc-outer-thresh-high
    2,        //agc_outer_thresh_high_dec_steps *** adi,agc-outer-thresh-high-dec-steps
    18,        //agc_outer_thresh_low *** adi,agc-outer-thresh-low
    2,        //agc_outer_thresh_low_inc_steps *** adi,agc-outer-thresh-low-inc-steps
    1,        //agc_attack_delay_extra_margin_us; *** adi,agc-attack-delay-extra-margin-us
    0,        //agc_sync_for_gain_counter_enable *** adi,agc-sync-for-gain-counter-enable
    /* Fast AGC */
    64,        //fagc_dec_pow_measuremnt_duration ***  adi,fagc-dec-pow-measurement-duration
    260,    //fagc_state_wait_time_ns ***  adi,fagc-state-wait-time-ns
    /* Fast AGC - Low Power */
    0,        //fagc_allow_agc_gain_increase ***  adi,fagc-allow-agc-gain-increase-enable
    5,        //fagc_lp_thresh_increment_time ***  adi,fagc-lp-thresh-increment-time
    1,        //fagc_lp_thresh_increment_steps ***  adi,fagc-lp-thresh-increment-steps
    /* Fast AGC - Lock Level (Lock Level is set via slow AGC inner high threshold) */
    1,        //fagc_lock_level_lmt_gain_increase_en ***  adi,fagc-lock-level-lmt-gain-increase-enable
    5,        //fagc_lock_level_gain_increase_upper_limit ***  adi,fagc-lock-level-gain-increase-upper-limit
    /* Fast AGC - Peak Detectors and Final Settling */
    1,        //fagc_lpf_final_settling_steps ***  adi,fagc-lpf-final-settling-steps
    1,        //fagc_lmt_final_settling_steps ***  adi,fagc-lmt-final-settling-steps
    3,        //fagc_final_overrange_count ***  adi,fagc-final-overrange-count
    /* Fast AGC - Final Power Test */
    0,        //fagc_gain_increase_after_gain_lock_en ***  adi,fagc-gain-increase-after-gain-lock-enable
    /* Fast AGC - Unlocking the Gain */
    0,        //fagc_gain_index_type_after_exit_rx_mode ***  adi,fagc-gain-index-type-after-exit-rx-mode
    1,        //fagc_use_last_lock_level_for_set_gain_en ***  adi,fagc-use-last-lock-level-for-set-gain-enable
    1,        //fagc_rst_gla_stronger_sig_thresh_exceeded_en ***  adi,fagc-rst-gla-stronger-sig-thresh-exceeded-enable
    5,        //fagc_optimized_gain_offset ***  adi,fagc-optimized-gain-offset
    10,        //fagc_rst_gla_stronger_sig_thresh_above_ll ***  adi,fagc-rst-gla-stronger-sig-thresh-above-ll
    1,        //fagc_rst_gla_engergy_lost_sig_thresh_exceeded_en ***  adi,fagc-rst-gla-engergy-lost-sig-thresh-exceeded-enable
    1,        //fagc_rst_gla_engergy_lost_goto_optim_gain_en ***  adi,fagc-rst-gla-engergy-lost-goto-optim-gain-enable
    10,        //fagc_rst_gla_engergy_lost_sig_thresh_below_ll ***  adi,fagc-rst-gla-engergy-lost-sig-thresh-below-ll
    8,        //fagc_energy_lost_stronger_sig_gain_lock_exit_cnt ***  adi,fagc-energy-lost-stronger-sig-gain-lock-exit-cnt
    1,        //fagc_rst_gla_large_adc_overload_en ***  adi,fagc-rst-gla-large-adc-overload-enable
    1,        //fagc_rst_gla_large_lmt_overload_en ***  adi,fagc-rst-gla-large-lmt-overload-enable
    0,        //fagc_rst_gla_en_agc_pulled_high_en ***  adi,fagc-rst-gla-en-agc-pulled-high-enable
    0,        //fagc_rst_gla_if_en_agc_pulled_high_mode ***  adi,fagc-rst-gla-if-en-agc-pulled-high-mode
    64,        //fagc_power_measurement_duration_in_state5 ***  adi,fagc-power-measurement-duration-in-state5
    2,        //fagc_large_overload_inc_steps *** adi,fagc-adc-large-overload-inc-steps
    /* RSSI Control */
    1,        //rssi_delay *** adi,rssi-delay
    1000,    //rssi_duration *** adi,rssi-duration
    3,        //rssi_restart_mode *** adi,rssi-restart-mode
    0,        //rssi_unit_is_rx_samples_enable *** adi,rssi-unit-is-rx-samples-enable
    1,        //rssi_wait *** adi,rssi-wait
    /* Aux ADC Control */
    256,    //aux_adc_decimation *** adi,aux-adc-decimation
    40000000UL,    //aux_adc_rate *** adi,aux-adc-rate
    /* AuxDAC Control */
    1,        //aux_dac_manual_mode_enable ***  adi,aux-dac-manual-mode-enable
    0,        //aux_dac1_default_value_mV ***  adi,aux-dac1-default-value-mV
    0,        //aux_dac1_active_in_rx_enable ***  adi,aux-dac1-active-in-rx-enable
    0,        //aux_dac1_active_in_tx_enable ***  adi,aux-dac1-active-in-tx-enable
    0,        //aux_dac1_active_in_alert_enable ***  adi,aux-dac1-active-in-alert-enable
    0,        //aux_dac1_rx_delay_us ***  adi,aux-dac1-rx-delay-us
    0,        //aux_dac1_tx_delay_us ***  adi,aux-dac1-tx-delay-us
    0,        //aux_dac2_default_value_mV ***  adi,aux-dac2-default-value-mV
    0,        //aux_dac2_active_in_rx_enable ***  adi,aux-dac2-active-in-rx-enable
    0,        //aux_dac2_active_in_tx_enable ***  adi,aux-dac2-active-in-tx-enable
    0,        //aux_dac2_active_in_alert_enable ***  adi,aux-dac2-active-in-alert-enable
    0,        //aux_dac2_rx_delay_us ***  adi,aux-dac2-rx-delay-us
    0,        //aux_dac2_tx_delay_us ***  adi,aux-dac2-tx-delay-us
    /* Temperature Sensor Control */
    256,    //temp_sense_decimation *** adi,temp-sense-decimation
    1000,    //temp_sense_measurement_interval_ms *** adi,temp-sense-measurement-interval-ms
    0xCE,    //temp_sense_offset_signed *** adi,temp-sense-offset-signed
    1,        //temp_sense_periodic_measurement_enable *** adi,temp-sense-periodic-measurement-enable
    /* Control Out Setup */
    0xFF,    //ctrl_outs_enable_mask *** adi,ctrl-outs-enable-mask
    0,        //ctrl_outs_index *** adi,ctrl-outs-index
    /* External LNA Control */
    0,        //elna_settling_delay_ns *** adi,elna-settling-delay-ns
    0,        //elna_gain_mdB *** adi,elna-gain-mdB
    0,        //elna_bypass_loss_mdB *** adi,elna-bypass-loss-mdB
    0,        //elna_rx1_gpo0_control_enable *** adi,elna-rx1-gpo0-control-enable
    0,        //elna_rx2_gpo1_control_enable *** adi,elna-rx2-gpo1-control-enable
    0,        //elna_gaintable_all_index_enable *** adi,elna-gaintable-all-index-enable
    /* Digital Interface Control */
    0,        //digital_interface_tune_skip_mode *** adi,digital-interface-tune-skip-mode
    0,        //digital_interface_tune_fir_disable *** adi,digital-interface-tune-fir-disable
    1,        //pp_tx_swap_enable *** adi,pp-tx-swap-enable
    1,        //pp_rx_swap_enable *** adi,pp-rx-swap-enable
    0,        //tx_channel_swap_enable *** adi,tx-channel-swap-enable
    0,        //rx_channel_swap_enable *** adi,rx-channel-swap-enable
    1,        //rx_frame_pulse_mode_enable *** adi,rx-frame-pulse-mode-enable
    0,        //two_t_two_r_timing_enable *** adi,2t2r-timing-enable
    0,        //invert_data_bus_enable *** adi,invert-data-bus-enable
    0,        //invert_data_clk_enable *** adi,invert-data-clk-enable
    0,        //fdd_alt_word_order_enable *** adi,fdd-alt-word-order-enable
    0,        //invert_rx_frame_enable *** adi,invert-rx-frame-enable
    0,        //fdd_rx_rate_2tx_enable *** adi,fdd-rx-rate-2tx-enable
    0,        //swap_ports_enable *** adi,swap-ports-enable
    0,        //single_data_rate_enable *** adi,single-data-rate-enable
    1,        //lvds_mode_enable *** adi,lvds-mode-enable
    0,        //half_duplex_mode_enable *** adi,half-duplex-mode-enable
    0,        //single_port_mode_enable *** adi,single-port-mode-enable
    0,        //full_port_enable *** adi,full-port-enable
    0,        //full_duplex_swap_bits_enable *** adi,full-duplex-swap-bits-enable
    0,        //delay_rx_data *** adi,delay-rx-data
    0,        //rx_data_clock_delay *** adi,rx-data-clock-delay
    4,        //rx_data_delay *** adi,rx-data-delay
    7,        //tx_fb_clock_delay *** adi,tx-fb-clock-delay
    0,        //tx_data_delay *** adi,tx-data-delay
#ifdef ALTERA_PLATFORM
    300,    //lvds_bias_mV *** adi,lvds-bias-mV
#else
    150,    //lvds_bias_mV *** adi,lvds-bias-mV
#endif
    1,        //lvds_rx_onchip_termination_enable *** adi,lvds-rx-onchip-termination-enable
    0,        //rx1rx2_phase_inversion_en *** adi,rx1-rx2-phase-inversion-enable
    0xFF,    //lvds_invert1_control *** adi,lvds-invert1-control
    0x0F,    //lvds_invert2_control *** adi,lvds-invert2-control
    /* GPO Control */
    0,        //gpo_manual_mode_enable *** adi,gpo-manual-mode-enable
    0,        //gpo_manual_mode_enable_mask *** adi,gpo-manual-mode-enable-mask
    0,        //gpo0_inactive_state_high_enable *** adi,gpo0-inactive-state-high-enable
    0,        //gpo1_inactive_state_high_enable *** adi,gpo1-inactive-state-high-enable
    0,        //gpo2_inactive_state_high_enable *** adi,gpo2-inactive-state-high-enable
    0,        //gpo3_inactive_state_high_enable *** adi,gpo3-inactive-state-high-enable
    0,        //gpo0_slave_rx_enable *** adi,gpo0-slave-rx-enable
    0,        //gpo0_slave_tx_enable *** adi,gpo0-slave-tx-enable
    0,        //gpo1_slave_rx_enable *** adi,gpo1-slave-rx-enable
    0,        //gpo1_slave_tx_enable *** adi,gpo1-slave-tx-enable
    0,        //gpo2_slave_rx_enable *** adi,gpo2-slave-rx-enable
    0,        //gpo2_slave_tx_enable *** adi,gpo2-slave-tx-enable
    0,        //gpo3_slave_rx_enable *** adi,gpo3-slave-rx-enable
    0,        //gpo3_slave_tx_enable *** adi,gpo3-slave-tx-enable
    0,        //gpo0_rx_delay_us *** adi,gpo0-rx-delay-us
    0,        //gpo0_tx_delay_us *** adi,gpo0-tx-delay-us
    0,        //gpo1_rx_delay_us *** adi,gpo1-rx-delay-us
    0,        //gpo1_tx_delay_us *** adi,gpo1-tx-delay-us
    0,        //gpo2_rx_delay_us *** adi,gpo2-rx-delay-us
    0,        //gpo2_tx_delay_us *** adi,gpo2-tx-delay-us
    0,        //gpo3_rx_delay_us *** adi,gpo3-rx-delay-us
    0,        //gpo3_tx_delay_us *** adi,gpo3-tx-delay-us
    /* Tx Monitor Control */
    37000,    //low_high_gain_threshold_mdB *** adi,txmon-low-high-thresh
    0,        //low_gain_dB *** adi,txmon-low-gain
    24,        //high_gain_dB *** adi,txmon-high-gain
    0,        //tx_mon_track_en *** adi,txmon-dc-tracking-enable
    0,        //one_shot_mode_en *** adi,txmon-one-shot-mode-enable
    511,    //tx_mon_delay *** adi,txmon-delay
    8192,    //tx_mon_duration *** adi,txmon-duration
    2,        //tx1_mon_front_end_gain *** adi,txmon-1-front-end-gain
    2,        //tx2_mon_front_end_gain *** adi,txmon-2-front-end-gain
    48,        //tx1_mon_lo_cm *** adi,txmon-1-lo-cm
    48,        //tx2_mon_lo_cm *** adi,txmon-2-lo-cm
    /* GPIO definitions */
    {
        .number = -1,
#ifdef XILINX_PLATFORM
        .platform_ops = &xil_gpio_platform_ops,
        .extra = &xil_gpio_param
#endif
#ifdef LINUX_PLATFORM
        .platform_ops = &linux_gpio_platform_ops
#endif
#ifdef GENERIC_PLATFORM
        .platform_ops = &generic_gpio_platform_ops
#endif
    },        //gpio_resetb *** reset-gpios
    /* MCS Sync */
    {
        .number = -1,
#ifdef XILINX_PLATFORM
        .platform_ops = &xil_gpio_platform_ops,
        .extra = &xil_gpio_param
#endif
#ifdef LINUX_PLATFORM
        .platform_ops = &linux_gpio_platform_ops
#endif
#ifdef GENERIC_PLATFORM
        .platform_ops = &generic_gpio_platform_ops
#endif
    },        //gpio_sync *** sync-gpios

    {
        .number = -1,
#ifdef XILINX_PLATFORM
        .platform_ops = &xil_gpio_platform_ops,
        .extra = &xil_gpio_param
#endif
#ifdef LINUX_PLATFORM
        .platform_ops = &linux_gpio_platform_ops
#endif
#ifdef GENERIC_PLATFORM
        .platform_ops = &generic_gpio_platform_ops
#endif
    },        //gpio_cal_sw1 *** cal-sw1-gpios

    {
        .number = -1,
#ifdef XILINX_PLATFORM
        .platform_ops = &xil_gpio_platform_ops,
        .extra = &xil_gpio_param
#endif
#ifdef LINUX_PLATFORM
        .platform_ops = &linux_gpio_platform_ops
#endif
#ifdef GENERIC_PLATFORM
        .platform_ops = &generic_gpio_platform_ops
#endif
    },        //gpio_cal_sw2 *** cal-sw2-gpios

    {
        .device_id = SPI_DEVICE_ID,
        .mode = SPI_MODE_1,
        .chip_select = SPI_CS,
#ifdef XILINX_PLATFORM
        .extra = &xil_spi_param,
        .platform_ops = &xil_platform_ops
#endif
#ifdef LINUX_PLATFORM
        .platform_ops = &linux_spi_platform_ops
#endif
#ifdef GENERIC_PLATFORM
        .platform_ops = &generic_spi_platform_ops
#endif
    },

    /* External LO clocks */
    NULL,    //(*ad9361_rfpll_ext_recalc_rate)()
    NULL,    //(*ad9361_rfpll_ext_round_rate)()
    NULL,    //(*ad9361_rfpll_ext_set_rate)()
#ifndef AXI_ADC_NOT_PRESENT
    &rx_adc_init,    // *rx_adc_init
    &tx_dac_init,   // *tx_dac_init
#endif
};

FIR configuration is the same as the tip of 2019_R2 branch.

Thanks,

Will

Top Replies

    •  Analog Employees 
    Jul 21, 2022 in reply to wfkolb +1 suggested
    looking at the axi_dac_load_custom_data function vs axi_dac_set_sine_lut, I'm seeing different axi bus calls in both functions. Is there a break down of calls I should make? I couldn't find…
Parents
  • Hello,

    Apologies for the late response.

    While not an expert on the matter, I believe you are correct. The default functionality is seeing a sine wave at 1MHz by choosing DAC_DMA_EXAMPLE. The axi_dac_load_custom_data function loads the sine_lut_iq table in the DAC DMA buffer dac_buffer.

    To use axi_dac_load_custom_data function you would just need to compile your own wave table and give it to the function in place of the sine_lut_iq table. To use axi_dac_set_sine_lut, I think you would have to change data in this table and possibly adjust the size constraints in the function or meet the existing ones. As such, I would use axi_dac_load_custom_data.

    Regards,
    Andrei

  • Thanks for getting back to me Andrei!

    Okay, at least the 1mhz matches up with what I'm assuming should happen. However, two follow up questions

    1. looking at the axi_dac_load_custom_data function vs axi_dac_set_sine_lut, I'm seeing different axi bus calls in both functions. Is there a break down of calls I should make? I couldn't find it in the reference manual for ad9364. Primary difference is in axi_dac_set_sine_lut i'm seeing only calls to axi_io_write for the data while axi_dac_load_custom_data has calls to axi_dac_write which are not present in the other data.
    2. The FIR filter by default is set to 3/20*fs to 1/4*fs, 1mhz is 1/30*fs (roughly) , upon disabling the fir filter using axi_dac_load_custom_data with the custom sine data I still don't see any tone at 1mhz. Any chance there's another set of test data for the DMA example that I could attempt to use? I have octave so a .mat file would work here.
    3. Is this an issue with the branch I'm on? Is there a combination of hdl repo, vivado + vitis, and no-os that is known good for the zedboard/Fmcomms4-ebz project?

    The only other thing to note is that if I run the included sd card for the fmcomms4-ebz which has linux and iio oscilloscope compiled using 2016_R1 everything functions as expected when sending data through the iio oscilloscope application. Therefore I think my hardware is functioning, I think it's just my usage of the no-os drivers.

    Thanks,

    Will

Reply
  • Thanks for getting back to me Andrei!

    Okay, at least the 1mhz matches up with what I'm assuming should happen. However, two follow up questions

    1. looking at the axi_dac_load_custom_data function vs axi_dac_set_sine_lut, I'm seeing different axi bus calls in both functions. Is there a break down of calls I should make? I couldn't find it in the reference manual for ad9364. Primary difference is in axi_dac_set_sine_lut i'm seeing only calls to axi_io_write for the data while axi_dac_load_custom_data has calls to axi_dac_write which are not present in the other data.
    2. The FIR filter by default is set to 3/20*fs to 1/4*fs, 1mhz is 1/30*fs (roughly) , upon disabling the fir filter using axi_dac_load_custom_data with the custom sine data I still don't see any tone at 1mhz. Any chance there's another set of test data for the DMA example that I could attempt to use? I have octave so a .mat file would work here.
    3. Is this an issue with the branch I'm on? Is there a combination of hdl repo, vivado + vitis, and no-os that is known good for the zedboard/Fmcomms4-ebz project?

    The only other thing to note is that if I run the included sd card for the fmcomms4-ebz which has linux and iio oscilloscope compiled using 2016_R1 everything functions as expected when sending data through the iio oscilloscope application. Therefore I think my hardware is functioning, I think it's just my usage of the no-os drivers.

    Thanks,

    Will

Children
  • looking at the axi_dac_load_custom_data function vs axi_dac_set_sine_lut, I'm seeing different axi bus calls in both functions. Is there a break down of calls I should make? I couldn't find it in the reference manual for ad9364. Primary difference is in axi_dac_set_sine_lut i'm seeing only calls to axi_io_write for the data while axi_dac_load_custom_data has calls to axi_dac_write which are not present in the other data.

    1. Ok this is a late answer but I hope it clears up some things. If you read through this document https://wiki.analog.com/resources/fpga/docs/axi_dac_ip you'll notice the DAC Register area (click to expand). You may see there that the 0x418 register which is additionally written by axi_dac_load_custom_data() function is the data source selector register which is set to the value of 2, meaning DMA. Also, the AXI_DAC_SYNC bit of AXI_DAC_REG_SYNC_CONTROL register is additionally accessed.

    So axi_dac_load_custom_data() is hardcoded to configure the AXI_DAC source as DMA and populate the data buffer with given values.

    The FIR filter by default is set to 3/20*fs to 1/4*fs, 1mhz is 1/30*fs (roughly) , upon disabling the fir filter using axi_dac_load_custom_data with the custom sine data I still don't see any tone at 1mhz. Any chance there's another set of test data for the DMA example that I could attempt to use? I have octave so a .mat file would work here.

    2. Sine lut needs to be in IQ format. This would be a good thread:  https://ez.analog.com/microcontroller-no-os-drivers/f/q-a/85900/ad9361-dac-explanation

    Is this an issue with the branch I'm on? Is there a combination of hdl repo, vivado + vitis, and no-os that is known good for the zedboard/Fmcomms4-ebz project?

    3. There were quite a few changes to the DAC_DMA_EXAMPLE recently, I'm pretty confident master branch of HDL+ no-OS works (even though I didn't run a test on hardware before writing this statement). I still think it'd be worth for you to try code from master.