Where is the log file that function talWriteToLog write into ?

Hi,I am using the hdl 'master' branch . And i am using no-os master branch. And I am using the project design for  zc706 and EVAL-ADRV9008/9.

I am migrating the reference design to a custom design board . While I am debug the no-os program ,the console shows a error message : ""TALISE_verifySpiReadWrite(): Cannot read from a low SPI address".

I search the TALISE_verifySpiReadWrite() and seems there is a function "talWriteToLog " write the error information into  a log file.

1.Where can i find the log file?

2. What is the function of "TALISE_verifySpiReadWrite()" ?

Thanks.

uint32_t TALISE_verifySpiReadWrite (taliseDevice_t *device)
{
	talRecoveryActions_t retVal = TALACT_NO_ACTION;
	adiHalErr_t halError = ADIHAL_OK;
	uint8_t spiReg = 0;

#if TALISE_VERBOSE
	halError = talWriteToLog(device->devHalInfo, ADIHAL_LOG_MSG, TAL_ERR_OK,
				 "TALISE_verifySpiReadWrite()\n");
	retVal = talApiErrHandler(device, TAL_ERRHDL_HAL_LOG, halError, retVal,
				  TALACT_WARN_RESET_LOG);
#endif