Post Go back to editing
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

serial connection with iio oscilloscope

Hello,

I have a problem connecting my project with the iio oscilloscope.

I followed the link to build the sample project.


https://wiki.analog.com/resources/tools-software/no-os-software/iio

Then I open the iio oscilloscope and it doesn't have the serial context option.



What is the problem with this?

Thank you,
Nicole.

Edit Notes


[locked by: buha at 7:04 AM (GMT -5) on 25 Nov 2021]
Parents
  • Hello,

    I see you are using a virtual machine to try to connect with the board. I am thinking that that may interfere if the machine is not set correctly, for example it doesn't have the serial drivers, or serial devices are not correctly piped through to it. Could you make sure a serial connection is possible? Maybe use a putty or similar program to send "PRINT" to the board and see if there is any output.

    Alternatively you can install IIO osc on the host machine and it might work smoother.

    Regards,
    Andrei

  • Thanks for the reply,
    
    by means of putty and serial connection I can see the output of DAC_DMA_EXAMPLE.

     I don't know if there might be an installation error in iio oscilloscope.
  • ,

    You need to build the project with TINYIIOD=y flag.

    So go ahead to your project directory and

    make clean_all
    make TINYIIOD=y

    After this, you will see a different message at the serial console and iio-oscilloscope will be able to see the iio device.

Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.