AD7134
Not Recommended for New Designs
The AD7134 is a quad channel, low noise, simultaneous sampling, precision analog-to-digital converter (ADC) that delivers on functionality, performance...
Datasheet
AD7134 on Analog.com
Hi,
I'm working with the AD7134 trying to get the Zedboard example working.
I've tried uploading to the board from CMD and Vivado - both successfully upload, but have this same issue.
I'm trying to use the spi.c commands to read out info to verify functionality:

You can see that it accepts spi_init and write_and_read as valid commands and not xil_spi_init or jibberish.
I'm just not getting anything back - so I can't even tell if this is a hw connection issue, I'm using the commands incorrectly, or if something didn't build correctly. I do get the below two error and warning which may be causing the issue. I'm just not sure how to resolve them.


Thank you for any assistance.
Hi,
Your board seems to run u-boot or Linux instead of the no-OS project.
What HDL/no-OS branch did you use? Did you follow these instructions: https://wiki.analog.com/resources/no-os/build for building the project?
Thanks,
Dragos
Hi Dragos,
I'm using the master branch and have Vivado 2020.1.
The reference you linked is the one I'm looking at. Below is a copy of my CMD commands and outputs.
After your U-boot comment I tried swapping the headers for JTAG programming on the Zedboard, but that resulted in nothing coming out of TeraTerm once programming was finished and the blue LED came on.
I also found the link below which makes no reference to changing the headers so I don't believe changing them is necessary.
Thanks.
https://wiki.analog.com/resources/fpga/xilinx/pmod/ad7476a
C:\tmp\adi\no-OS\projects\ad713x_fmcz>C:\Xilinx\vitis\2020.1\settings64.bat
C:\tmp\adi\no-OS\projects\ad713x_fmcz>make
[00:00:00] Building for xilinx
[00:00:00] Evaluating hardware: system_top.xsa
[00:00:00] Creating and configuring the IDE project
arm-none-eabi-ar: creating ../../../lib/libxil.a
In file included from usleep.c:34:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from xil_sleeptimer.c:32:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from xtime_l.c:27:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from sleep.c:31:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from main.c:115:
zynq_fsbl_bsp/ps7_cortexa9_0/include/xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from pcap.c:78:
zynq_fsbl_bsp/ps7_cortexa9_0/include/xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
arm-none-eabi-ar: creating ../../../lib/libxil.a
In file included from usleep.c:34:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from xil_sleeptimer.c:32:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from xtime_l.c:27:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from sleep.c:31:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
[00:00:00] Linking srcs to created project
The system cannot find the file specified.
The system cannot find the file specified.
The system cannot find the file specified.
make[1]: [../../tools/scripts/generic.mk:339: update_srcs] Error 2 (ignored)
[00:00:00] [CC] ad713x.c
[00:00:00] [CC] iio_ad713x.c
[00:00:00] [CC] iio_dual_ad713x.c
[00:00:00] [CC] axi_dmac.c
[00:00:00] [CC] spi_engine.c
[00:00:00] [CC] gpio.c
[00:00:00] [CC] axi_io.c
[00:00:00] [CC] delay.c
[00:00:00] [CC] xilinx_gpio.c
[00:00:00] [CC] xilinx_spi.c
[00:00:00] [CC] spi.c
C:/tmp/adi/no-OS/projects/ad713x_fmcz/build/app/noos/drivers/spi/spi.c: In function 'spi_transfer':
C:/tmp/adi/no-OS/projects/ad713x_fmcz/build/app/noos/drivers/spi/spi.c:98:11: warning: 'ret' may be used uninitialized in this function [-Wmaybe-uninitialized]
98 | int32_t ret;
| ^~~
[00:00:00] [CC] ad713x_fmc.c
[00:00:00] [CC] util.c
[00:00:00] [LD] ad713x.o iio_ad713x.o iio_dual_ad713x.o axi_dmac.o spi_engine.o gpio.o axi_io.o delay.o xilinx_gpio.o xilinx_spi.o spi.o ad713x_fmc.o util.o
make[2]: Nothing to be done for 'post_build'.
[00:00:00] Done (build/ad713x_fmcz.elf)
C:\tmp\adi\no-OS\projects\ad713x_fmcz>make run
[00:00:00] Building for xilinx
[00:00:00] Creating and configuring the IDE project
A project with given name already exists in the workspace. Please choose a differenet name.
while executing
"error [dict get $msg err]"
(procedure "xsdk_eval" line 15)
invoked from within
"xsdk_eval $chan "XSDx" createAppFromDsa "o{$fmt}" e [list $data]"
(procedure "app" line 330)
invoked from within
"app create -name app -hw $::hw -proc $cpu -os standalone -template {Empty Application}"
(procedure "_vitis_project" line 9)
invoked from within
"_vitis_project"
(procedure "create_project" line 6)
invoked from within
"$function"
(file "C:/tmp/adi/no-OS/tools/scripts/platform/xilinx/util.tcl" line 251)
[00:00:00] Linking srcs to created project
The system cannot find the file specified.
make[1]: [../../tools/scripts/generic.mk:339: update_srcs] Error 2 (ignored)
[00:00:00] [CC] axi_dmac.c
[00:00:00] [CC] spi_engine.c
[00:00:00] [CC] gpio.c
[00:00:00] [CC] axi_io.c
[00:00:00] [CC] delay.c
[00:00:00] [CC] xilinx_gpio.c
[00:00:00] [CC] xilinx_spi.c
[00:00:00] [CC] spi.c
C:/tmp/adi/no-OS/projects/ad713x_fmcz/build/app/noos/drivers/spi/spi.c: In function 'spi_transfer':
C:/tmp/adi/no-OS/projects/ad713x_fmcz/build/app/noos/drivers/spi/spi.c:98:11: warning: 'ret' may be used uninitialized in this function [-Wmaybe-uninitialized]
98 | int32_t ret;
| ^~~
[00:00:00] [CC] util.c
[00:00:00] [LD] ad713x.o iio_ad713x.o iio_dual_ad713x.o axi_dmac.o spi_engine.o gpio.o axi_io.o delay.o xilinx_gpio.o xilinx_spi.o spi.o ad713x_fmc.o util.o
make[2]: Nothing to be done for 'post_build'.
[00:00:00] Done (build/ad713x_fmcz.elf)
[00:00:00] ad713x_fmcz.elf uploaded to board
Antoniu,
I'm having the same problem. After I execute the "make run" I get the following on my UART port then it no longer responds to any input.
[1B][0;31mzynq>[1B][m
U-Boot 2011.03-dirty (Jul 11 2012 - 16:07:00)
DRAM: 512 MiB
MMC: SDHCI: 0
Using default environment
In: serial
Out: serial
Err: serial
Net: zynq_gem
Hit any key to stop autoboot: 3
Your board is booting u-boot instead of the no-OS project - if inserted, try to remove the SD card.
Thanks,
Dragos
Here's what I tried:
1) power down
2) remove SD Card
3) power up
4) rerun "make run"; the elf file uploaded to board as before
5) same problem; no response at all on the UART port
Can you put the board into JTAG boot mode and try again? I believe all the jumpers need to be in GND position.
-Travis
OK. Tried that as well.
1) power down
2) Change jumpers to JTAG boot mode (all in GND position)
3) power up
4) make run; [00:00:00] ad738x_fmcz.elf uploaded to board
5) same problem
Sorry, this is the actual response:
I would still like an explanation for the following during the make:
[00:00:00] Linking srcs to created project
The system cannot find the file specified.
make[1]: [../../tools/scripts/generic.mk:339: update_srcs] Error 2 (ignored)
Hi,
Please make sure your no-Os repository is up to date. It looks like the run command is building the project instead of uploading the elf file.
Sergiu
Thanks. My repository is up to date since I just started over from scratch.
Please answer these questions.
1) Do you have these boards (AD7134 and zedboard) to try this code?
2) Can you confirm that my make output is as expected, including missing files and errors? (see below)
C:\cygwin64\home\Steve\adi4\no-OS\projects\ad713x_fmcz>make clean
[00:00:00] [Delete] ad713x.o iio_ad713x.o iio_dual_ad713x.o axi_dmac.o spi_engine.o gpio.o axi_io.o delay.o xilinx_gpio.o xilinx_spi.o spi.o ad713x_fmc.o util.o ad713x_fmcz.elf
The system cannot find the file specified.
make: [../../tools/scripts/generic.mk:358: clean] Error 1 (ignored)
C:\cygwin64\home\Steve\adi4\no-OS\projects\ad713x_fmcz>make
[00:00:00] Building for xilinx
[00:00:00] Evaluating hardware: system_top.xsa
[00:00:00] Creating and configuring the IDE project
arm-none-eabi-ar: creating ../../../lib/libxil.a
In file included from usleep.c:34:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from xil_sleeptimer.c:32:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from xtime_l.c:27:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from sleep.c:31:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from main.c:115:
zynq_fsbl_bsp/ps7_cortexa9_0/include/xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from pcap.c:78:
zynq_fsbl_bsp/ps7_cortexa9_0/include/xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
arm-none-eabi-ar: creating ../../../lib/libxil.a
In file included from usleep.c:34:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from xil_sleeptimer.c:32:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from xtime_l.c:27:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from sleep.c:31:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
[00:00:00] Linking srcs to created project
The system cannot find the file specified.
The system cannot find the file specified.
The system cannot find the file specified.
make[1]: [../../tools/scripts/generic.mk:339: update_srcs] Error 2 (ignored)
[00:00:00] [CC] ad713x.c
[00:00:00] [CC] iio_ad713x.c
[00:00:00] [CC] iio_dual_ad713x.c
[00:00:00] [CC] axi_dmac.c
[00:00:00] [CC] spi_engine.c
[00:00:00] [CC] gpio.c
[00:00:00] [CC] axi_io.c
[00:00:00] [CC] delay.c
[00:00:00] [CC] xilinx_gpio.c
[00:00:00] [CC] xilinx_spi.c
[00:00:00] [CC] spi.c
[00:00:00] [CC] ad713x_fmc.c
[00:00:00] [CC] util.c
[00:00:00] [LD] ad713x.o iio_ad713x.o iio_dual_ad713x.o axi_dmac.o spi_engine.o gpio.o axi_io.o delay.o xilinx_gpio.o xilinx_spi.o spi.o ad713x_fmc.o util.o
make[2]: Nothing to be done for 'post_build'.
[00:00:00] Done (build/ad713x_fmcz.elf)
Hi Steve,
As I see in the code in the master version of the project (https://github.com/analogdevicesinc/no-OS/blob/master/projects/ad713x_fmcz/src/ad713x_fmc.c) you don't need to interact with the code it will just print data, or if you enable TINYIIOD (how to enable tinyiiod) you can connect using IIO Osciloscope.
My recommendation are:
Open a windows cmd with administrator privileges in the project folder.
Run a `make clean_all` in order to start from a clean workspace.
Then run `make update_srcs` this will just create an sdk project you can edit.
Run `make develop` : will open xsdk with the created projects.
Program the fpga from the sdk.
Set a breakpoint at main and then debug.
Are you able to see data from the first printf?
Regards,
Mihail
Hi Steve,
As I see in the code in the master version of the project (https://github.com/analogdevicesinc/no-OS/blob/master/projects/ad713x_fmcz/src/ad713x_fmc.c) you don't need to interact with the code it will just print data, or if you enable TINYIIOD (how to enable tinyiiod) you can connect using IIO Osciloscope.
My recommendation are:
Open a windows cmd with administrator privileges in the project folder.
Run a `make clean_all` in order to start from a clean workspace.
Then run `make update_srcs` this will just create an sdk project you can edit.
Run `make develop` : will open xsdk with the created projects.
Program the fpga from the sdk.
Set a breakpoint at main and then debug.
Are you able to see data from the first printf?
Regards,
Mihail
Mihail,
I did as you suggested. The result is the same. I get as far as this instruction on line 209 in ad713x_fmc.c, which fails every time.
ret = ad713x_init(&ad713x_dev_1, &ad713x_init_param_1);
Here is the output from CMD:
NOTE that I'm still getting errors during the final link process. I've asked several times if these errors are expected, but no one has answered this question.
C:\cygwin64\home\Steve\adi4\no-OS\projects\ad713x_fmcz>make clean_all
[00:00:00] [Delete] C:/cygwin64/home/Steve/adi4/no-OS/projects/ad713x_fmcz/build
C:\cygwin64\home\Steve\adi4\no-OS\projects\ad713x_fmcz>make update_srcs
[00:00:00] Evaluating hardware: system_top.xsa
[00:00:00] Creating and configuring the IDE project
arm-none-eabi-ar: creating ../../../lib/libxil.a
In file included from usleep.c:34:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from xil_sleeptimer.c:32:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from xtime_l.c:27:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from sleep.c:31:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from main.c:115:
zynq_fsbl_bsp/ps7_cortexa9_0/include/xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from pcap.c:78:
zynq_fsbl_bsp/ps7_cortexa9_0/include/xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
arm-none-eabi-ar: creating ../../../lib/libxil.a
In file included from usleep.c:34:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from xil_sleeptimer.c:32:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from xtime_l.c:27:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
In file included from sleep.c:31:
xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
65 | #pragma message ("For the sleep routines, Global timer is being used")
| ^~~~~~~
[00:00:00] Linking srcs to created project
The system cannot find the file specified.
The system cannot find the file specified.
The system cannot find the file specified.
make: [../../tools/scripts/generic.mk:339: update_srcs] Error 2 (ignored)
C:\cygwin64\home\Steve\adi4\no-OS\projects\ad713x_fmcz>make develop
vitis -workspace=C:/cygwin64/home/Steve/adi4/no-OS/projects/ad713x_fmcz/build
****** Xilinx Vitis Development Environment
Vitis v2020.1 (64-bit)
****** SW Build 2902540 on Wed May 27 19:55:32 MDT 2020
** Copyright 1986-2020 Xilinx, Inc. All Rights Reserved.
C:\cygwin64\home\Steve\adi4\no-OS\projects\ad713x_fmcz>
Yes, the output of the terminal is normal. They are xilinx bsp related warnings.
Can you step inside the ad713x_init function and see which function fails, there seems to be many thinks that can fail.
Yes, it's failing in spi.c on line 57 and returning FAILURE
int32_t spi_init(struct spi_desc **desc,
const struct spi_init_param *param)
{
if (!param)
return FAILURE;
if ((param->platform_ops->init(desc, param)))
return FAILURE;
(*desc)->platform_ops = param->platform_ops;
return SUCCESS;
}
Do you have the same hardware to try this on (AD7134_EVAL and zedboard)?
Some of these parameters look suspect. Can you confirm they are correct?

Hi Steve,
For this platform, the device id and bit order parameters are irrelevant.
Also 0x989680 in hex is the same as 10 000 000 in decimal which represents the 10mhz sclk speed.
You could try debugging a bit deeper and go inside the param->platform_ops->init(desc, param) function (that should go to https://github.com/analogdevicesinc/no-OS/blob/master/drivers/axi_core/spi_engine/spi_engine.c#L623 ) and see exactly where the code is failing.
Sergiu
The device_id was causing the failure for both of these commands. I changed them both to a value of 01 and the init function no longer fails.
ret = ad713x_init(&ad713x_dev_1, &ad713x_init_param_1);
ret = ad713x_init(&ad713x_dev_2, &ad713x_init_param_2);
However, I believe this causes later issues since the first read from spi returns 0x0. What is the correct device_id to use ?
Now that I'm past that error, here's the next issue...failing ad713x_spi_reg_read...line 106 of ad713x.c..

Hello Vick,
Let's continue our discussion here: ez.analog.com/.../spi_init-error-using-ad7134_eval-board-with-zedboard-running-no-os
Regards,
Antoniu