Post Go back to editing

spi_init error using AD7134_EVAL board with zedboard running no-os

I am getting an error when the spi_init routine is run.  This routine returns FAILURE.

    ret = ad713x_init(&ad713x_dev_1, &ad713x_init_param_1);
    if (ret != SUCCESS)
        return FAILURE;

I'm using this version of no-os...https://wiki.analog.com/resources/tools-software/uc-drivers/ad713x?s%5b%5d=ad7134

How can I resolve this issue?

  • Hello Vick,

    Can you please specify the hdl branch and the no-OS branch that you used to build your application?

    Can you try to use our build guide for generating your project: https://wiki.analog.com/resources/no-os/build

    Regards,

    Antoniu

  • hdl master and I used the guide you specify for no-os.

    I found out yesterday there is a design issue with the AD7134_EVAL board.  The FMC connectors don't mate fully with the zedboard because the VGA connector on the zedboard is too tall.  How are you guys dealing with this issue?  I suspect this is why my spi is failing.

  • Why is there no warning on the product page? 

    Are you planning to fix this this problem? If so, when will it be released?

  • https://ez.analog.com/data_converters/precision_adcs/ can provide more details about the EVAL-AD7134FMCZ hardware.

    Thanks,
    Dragos

  • OK, I now have the adapter cable to go between the AD7134 and zedboard.  However, I'm still getting the same error upon initialization of the spi interface.

    On this command in ad713x.c

        if (!init_param->spi_common_dev) {
            ret = spi_init(&dev->spi_desc, &init_param->spi_init_prm);
            if (IS_ERR_VALUE(ret))
                goto error_dev;

    What might be the problem with this code?

  • I started over and cloned the most recent no-os software from ad713x_fmcz and ran the make again.  My output is shown below.  Please let me know if this is what you would expect.

    Please note the following lines during linking:

    (1)     The system cannot find the file specified

    (2)      make[1]: [../../tools/scripts/generic.mk:339: update_srcs] Error 2 (ignored)

    C:\cygwin64\home\Steve\adi4\no-OS\projects\ad713x_fmcz>make
    [00:00:00] Building for xilinx
    [00:00:00] Evaluating hardware: system_top.xsa
    [00:00:00] Creating and configuring the IDE project
    arm-none-eabi-ar: creating ../../../lib/libxil.a
    In file included from usleep.c:34:
    xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
       65 | #pragma message ("For the sleep routines, Global timer is being used")
          |         ^~~~~~~
    In file included from xil_sleeptimer.c:32:
    xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
       65 | #pragma message ("For the sleep routines, Global timer is being used")
          |         ^~~~~~~
    In file included from xtime_l.c:27:
    xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
       65 | #pragma message ("For the sleep routines, Global timer is being used")
          |         ^~~~~~~
    In file included from sleep.c:31:
    xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
       65 | #pragma message ("For the sleep routines, Global timer is being used")
          |         ^~~~~~~
    In file included from main.c:115:
    zynq_fsbl_bsp/ps7_cortexa9_0/include/xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
       65 | #pragma message ("For the sleep routines, Global timer is being used")
          |         ^~~~~~~
    In file included from pcap.c:78:
    zynq_fsbl_bsp/ps7_cortexa9_0/include/xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
       65 | #pragma message ("For the sleep routines, Global timer is being used")
          |         ^~~~~~~
    arm-none-eabi-ar: creating ../../../lib/libxil.a
    In file included from usleep.c:34:
    xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
       65 | #pragma message ("For the sleep routines, Global timer is being used")
          |         ^~~~~~~
    In file included from xil_sleeptimer.c:32:
    xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
       65 | #pragma message ("For the sleep routines, Global timer is being used")
          |         ^~~~~~~
    In file included from xtime_l.c:27:
    xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
       65 | #pragma message ("For the sleep routines, Global timer is being used")
          |         ^~~~~~~
    In file included from sleep.c:31:
    xtime_l.h:65:9: note: #pragma message: For the sleep routines, Global timer is being used
       65 | #pragma message ("For the sleep routines, Global timer is being used")
          |         ^~~~~~~
    [00:00:00]  Linking srcs to created project
    The system cannot find the file specified.
    The system cannot find the file specified.
    The system cannot find the file specified.
    make[1]: [../../tools/scripts/generic.mk:339: update_srcs] Error 2 (ignored)
    [00:00:00] [CC] ad713x.c
    [00:00:00] [CC] iio_ad713x.c
    [00:00:00] [CC] iio_dual_ad713x.c
    [00:00:00] [CC] axi_dmac.c
    [00:00:00] [CC] spi_engine.c
    [00:00:00] [CC] gpio.c
    [00:00:00] [CC] axi_io.c
    [00:00:00] [CC] delay.c
    [00:00:00] [CC] xilinx_gpio.c
    [00:00:00] [CC] xilinx_spi.c
    [00:00:00] [CC] spi.c
    [00:00:00] [CC] ad713x_fmc.c
    [00:00:00] [CC] util.c
    [00:00:00] [LD] ad713x.o iio_ad713x.o iio_dual_ad713x.o axi_dmac.o spi_engine.o gpio.o axi_io.o delay.o xilinx_gpio.o xilinx_spi.o spi.o ad713x_fmc.o util.o
    make[2]: Nothing to be done for 'post_build'.
    [00:00:00] Done (build/ad713x_fmcz.elf)

  • build/ad713x_fmcz.elf seems to have been generated. Try to run it.

    Thanks,
    Dragos

  • No response on the UART port when I do a "make run"

    I get the errors shown above when I try to debug in Vitis.  Either way the code does not seem to run.

  • Hello Vick,

    We managed to get the hardware up and running on our side. Indeed there is an issue on the spi side of the project.

    Can you try the following patch:
    https://github.com/analogdevicesinc/no-OS/commit/bb2bd9be4de0c002f2805cfe532ebcf6828a8bc2

    If everything is fine, we will merge the fix on the master branch.

    In my case, it solved the issue. Here is the serial output:

    Regards,

    Antoniu

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.