AD9371 no-OS IIO Oscilloscope Question

Hi, Antoniu

1、I fixed the bug and rebuild the no-OS master through the command 'make TINYIIO=y',then 'make run'

2、I opened the IIO Oscilloscope client () in Windows、set baud rate to 921600 and connected to the IIO device.

My quenstions:

1、The capture feature can receive data in Time Domain, but cannot receive data in Frquency Domain.

2、I setup IIO Oscilloscope () in Ubuntu, but there is no Serial Context in osc, so how can I find and connect to the IIO Device?

Thank you!

Top Replies