Connection problem with TINYIIO-OSCILLOSCOPE when Combination of ADRV9002 + ZCU102

I want to connect to TINYIIO-OSCILLOSCOPE with EVAL-ADRV9002 + ZCU102 and get to the screen below.

However, the screen does not have the following ADRV9002 tabs.

environment :

hdl : hdl_2019_r2

vivado 2019.1

    -> create system_top.hdf

no-os : master branch

reference :

ADRV9002 No-OS System Level Design Setup [Analog Devices Wiki]

How to build the NO-OS adrv9002 TINYIIOD application - Q&A - Microcontroller no-OS Drivers - EngineerZone (analog.com)

Post build steps · analogdevicesinc/no-OS Wiki · GitHub

no-OS IIO [Analog Devices Wiki]

How to build the NO-OS adrv9002 TINYIIOD application - Q&A - Microcontroller no-OS Drivers - EngineerZone (analog.com)

The procedure to connect is as follows.

>make clean_all

>make

>./zynqmp_ddr_patch.sh build/hw/psu_init.tcl

>make TINYIIO=y run

check the console output. (baud rate : 115200bps)

connect IIO-OSCILLOSCOPE. (baud rate : 921600bps)

The screen at runtime is shown below.