AD9364 CMOS mode interface

Hi,

I'm using AD9364 in custom board with FPGA with NO-OS driver in CMOS mode interface,

As per mentioned in the reference manual changes are done as below for CMOS half duplex, single port.

/* Digital Interface Control */

0, //swap_ports_enable *** adi,swap-ports-enable
1, //single_data_rate_enable *** adi,single-data-rate-enable
0, //cmos-mode-enable *** adi,cmos-mode-enable
1, //half_duplex_mode_enable *** adi,half-duplex-mode-enable
1, //single_port_mode_enable *** adi,single-port-mode-enable
0, //full_port_enable *** adi,full-port-enable
0, //full_duplex_swap_bits_enable *** adi,full-duplex-swap-bits-enable

0,    //lvds_rx_onchip_termination_enable *** adi,lvds-rx-onchip-termination-enable

we are testing the interface with BIST as per the "AD9361BISTFAQ.pdf" but  test is not working as intended.

ad9361_bist_tone(ad9361_phy, BIST_INJ_RX, 3, 0, 0)”. function used to validate the RX path.

ad9361_bist_loopback(ad9361_phy, 1); function used to test the loopback.

Both are not working, not able see the any output at FPGA.

Can anybody please give me complete information regarding CMOS mode changes. 

Thanks,

Parents Reply Children
No Data