I run no-os project on zc706+9009, why the jesd stay at CGS mode, it just been Data mode once in a while, may one time of 100 times try.
Even if it's recommended, the external reference clock is not mandatory for receiving/transmitting some data. That is the reference for the AD9528's PLL1. PLL1 provides reference input clock cleanup…
Hello,
What version of HDL / No-OS are you using ?
Regards,
Adrian
2019-r1,if I must provide a sysref clk to 9009 externally?
For the single evaluation board you don't need to provide sysref clk externally.
The issue that I see is that the Rx and ORx jesd204 links are overclocked as they should run at maximum 6.6Gbps on the ZC706
how to fix it?
You'll need to use the QPLL for both RX/TX/ORx. I don't think we currently support this.
Moving to No-OS for additional comments.
This profile should work on ZC706: https://github.com/analogdevicesinc/no-OS/tree/master/projects/adrv9009/profiles/tx_bw100_ir122p88_rx_bw100_or122p88_orx_bw100_or122p88_dc122p88
Dragos
Hello. I use the profile what you provide, and in following picture the left one is the result of nothing changes, and the right one is the result after
externalSysref = 0, /* 0=use internal SYSREF, 1= use external SYSREF */ change 1 to 0 for I did not provide external sysref to it
Does this refclk should be provided?
Just checked the no-OS master branch for adrv9009 with 2019-r1 hdl.
ZC706 carrier.
Profile used is the one provided by DragosB above.
Please find the output below:
Antoniu
As you may notice, the JESD link status is DATA. I checked the status several times and it remains the same.
Well, Does the no-os_2019r1 is not the same as no-OS master branch?
I do what you say but the tx_jesd state is stiil stay in CGS
Are you using this version of the project? github.com/.../adrv9009
How did you build your project? Did you use these guides?https://github.com/analogdevicesinc/no-OS/wiki/Building-no-OS-on-Linuxhttps://github.com/analogdevicesinc/no-OS/wiki/Building-no-OS-on-Windows
Yes I do follow these
Do you notice that the log warning of talise enable multichipsync failed
and tal_frame/deframe status
there are did not occur on your screen shot? why that happened?
Best wishes!
It get error when make the no-os-master, does no-os-2019_r1 make the tx_jesd link failed which stay in CGS