Post Go back to editing

AD9467 KC705 Reference design

Thread Summary

The user is troubleshooting the AD9467 FMC reference design on the KC705 FPGA board, experiencing inconsistent test results and incorrect waveforms when dumping data from DDR3. The final answer confirms the need for an external clock and suggests that the input is AC-coupled, not suitable for square waves. The user should connect a 10 MHz sine wave clock and consider modifying the analog input coupling to DC if necessary.
AI Generated Content

hi all,

I use the AD9467 default FMC reference design on KC705(https://wiki.analog.com/resources/fpga/xilinx/fmc/ad9467#more_information).
However I face many problems while executing ad9467_fmc_ebz.c:
1. I have no idea whether the software project build successfully.

   There is the project contents and build settings.
project contents 


2. Sometimes I get "Test passed", and sometimes I get ERRORs.


3. How can I read the data in ddr3?
I have tried to dump file by Xilinx>Dump/Restor Data File and setting Start Address = 0, Size = 8192,
The data I dumped isn't correct (The input signal is 1 Vpp , 1.2Vdc ,1MHz sine wave)

Could any body give me some advices.
Thanks,
Wei-Chieh

Parents
  • Hello,

    I've checked the latest version of the project from the master branch:
    https://github.com/analogdevicesinc/no-OS/tree/master/ad9467-fmc-ebz

    With the 2019_R1 HDL release for this project.

    Using the common_drivers https://github.com/analogdevicesinc/no-OS/tree/master/common_drivers

    (you will have to change the "#include "spi.h"" with "#include "platform_drivers.h"" in the ad9467.h and ad9517.h files, since the drivers are using a newer version of communication drivers)

    I've checked multiple times the output and I did not get different results (as you mentioned in your case).

    The output is always this one:

    *****************************************************
      ADI AD9467-FMC-EBZ Reference Design
      AD9467 CHIP ID: 0x50
      AD9467 CHIP GRADE: 0x20
      AD9517 CHIP ID: 0xd3d3
    *****************************************************
    adc_setup adc core initialized (186 MHz).
                                             AD9467[0x016]: 00
    adc_delay: setting zero error delay (28)
    ADC Test: mode - MIDSCALE
              format - OFFSET BINARY
            Test passed
    ADC Test: mode - MIDSCALE
              format - TWOS_COMPLEMENT
            Test passed
    ADC Test: mode - POS_FULLSCALE
              format - OFFSET BINARY
            Test passed
    ADC Test: mode - POS_FULLSCALE
              format - TWOS_COMPLEMENT
            Test passed
    ADC Test: mode - NEG_FULLSCALE BINARY
              format - OFFSET BINARY
            Test passed
    ADC Test: mode - NEG_FULLSCALE BINARY
              format - TWOS_COMPLEMENT
            Test passed
    ADC Test: mode - CHECKERBOARD
              format - OFFSET BINARY
            Test passed
    ADC Test: mode - CHECKERBOARD
              format - TWOS_COMPLEMENT
            Test passed
    ADC Test: mode - PN_23_SEQUENCE
              format - OFFSET BINARY
              Test passed
    ADC Test: mode - PN_23_SEQUENCE
              format - TWOS_COMPLEMENT
              Test skipped
    ADC Test: mode - PN_9_SEQUENCE
              format - OFFSET BINARY
      ERROR: PN status(0002).
    ADC Test: mode - PN_9_SEQUENCE
              format - TWOS_COMPLEMENT
              Test skipped
    ADC Test: mode - ONE_ZERO_TOGGLE
              format - OFFSET BINARY
            Test passed
    ADC Test: mode - ONE_ZERO_TOGGLE
              format - TWOS_COMPLEMENT
            Test passed
    Testing done.
    Start capturing data...

    Done.

    Also, the data in the memory (0x80800000) looks fine for the test modes (+ Full-scale, - Full-scale, Checkerboard).

    Regards,

    Antoniu

  • Hi Antoniu,

    Thank you for the reply.
    I tried to print the data as the following structure:

    Addr |                        0x80800000                    |                         0x80800000 + 1                         | 
    Data | D[7] D[6] D[5] D[4] D[3] D[2] D[1] D[0]   |   D[15] D[14] D[13] D[12] D[11] D[10] D[9] D[8] |

    <sine>                                                                                              <square>

          

    The waveform is more clean than before, but the waveform is still far from the ideal one

    Could you give some advice?

    Thanks

    Wei-Chieh

  • Hi Andrei,

    No, I only connect AIN.
    Does the default setting of the no-os project and the default RTL should connect the externel clock?

    Thanks
    Wei-Chieh

  • Hi Wei-Chieh,

    Does the default setting of the no-os project and the default RTL should connect the externel clock?

    Yes, as stated in the link I posted above.

    Andrei

  • Hi Andrei,

    I connect the 10MHz Sine Wave with 2.2Vpp 1.9Vdc as clock signal to sample the 100kHz 2.2Vpp 1.9Vdc analog source.
    And I get the following waveform:
    <sine 100kHz 2.2Vpp 1.9Vdc>                                                <square 100kHz 2.2Vpp 1.9Vdc>

          

    The sine wave is great, but the square wave fail.

    Thanks

    Wei-Chieh

  • Hi Wei-Chieh,

    As I said in the beginning of the thread, the input of the evaluation board is AC coupled not DC. This means it was not design to capture square waves(DC components).

    Andrei

  • Hi Andrei,

    Because I have only one function generator now, I want to sample data by AD9517.

    And I have the following 2 questions:
    1. Can I just short P200 and ON as the follwing picture to enable the clock input?

        Or I should weld some 0.1uF capacitors (C304, C305, C306, C307) and remove C209 and C210?

    2. Can I switch to DC-coupling by adding 

         ad9467_analog_input_coupling(ad9467_device, 1, &status);
         ad9467_transfer(ad9467_device);

         in no-OS project?

    Thanks,

    Wei-Chieh

Reply
  • Hi Andrei,

    Because I have only one function generator now, I want to sample data by AD9517.

    And I have the following 2 questions:
    1. Can I just short P200 and ON as the follwing picture to enable the clock input?

        Or I should weld some 0.1uF capacitors (C304, C305, C306, C307) and remove C209 and C210?

    2. Can I switch to DC-coupling by adding 

         ad9467_analog_input_coupling(ad9467_device, 1, &status);
         ad9467_transfer(ad9467_device);

         in no-OS project?

    Thanks,

    Wei-Chieh

Children
  • Hello,

    P200 is used to disable the clock. If it's open, the clock is running (https://eu.mouser.com/datasheet/2/268/VCC6-1539124.pdf).

    In the documentation pointed above: "The evaluation board can be set up to be clocked from the crystal oscillator, Y200. This oscillator is a low phase noise oscillator from Vectron (VCC6-QCD-250M000). If this clock source is desired, install C205 and C206 and remove C202. Jumper P200 is used to disable the oscillator from running."

    If you want to use the AD9517 you could also do, on top of the above: "A differential LVPECL or LVDS clock driver can also be used to clock the ADC input using the AD9517. Populate C304, C305, C306, and C307 with 0.1 µF capacitors for one drive option or the other and remove C209 and C210 to disconnect the default clock path inputs. The AD9517 has many SPI-selectable options that are set to a default mode of operation. Consult the AD9517 data sheet for more information about these and other options."

    Regarding the Analog Input, you can check the schematic page 1 for the analog input circuitry https://wiki.analog.com/_media/resources/fpga/xilinx/fmc/9467fmc01c_sch.pdf 

    Regards,

    Adrian