Post Go back to editing

AD9467 KC705 Reference design

Thread Summary

The user is troubleshooting the AD9467 FMC reference design on the KC705 FPGA board, experiencing inconsistent test results and incorrect waveforms when dumping data from DDR3. The final answer confirms the need for an external clock and suggests that the input is AC-coupled, not suitable for square waves. The user should connect a 10 MHz sine wave clock and consider modifying the analog input coupling to DC if necessary.
AI Generated Content

hi all,

I use the AD9467 default FMC reference design on KC705(https://wiki.analog.com/resources/fpga/xilinx/fmc/ad9467#more_information).
However I face many problems while executing ad9467_fmc_ebz.c:
1. I have no idea whether the software project build successfully.

   There is the project contents and build settings.
project contents 


2. Sometimes I get "Test passed", and sometimes I get ERRORs.


3. How can I read the data in ddr3?
I have tried to dump file by Xilinx>Dump/Restor Data File and setting Start Address = 0, Size = 8192,
The data I dumped isn't correct (The input signal is 1 Vpp , 1.2Vdc ,1MHz sine wave)

Could any body give me some advices.
Thanks,
Wei-Chieh

Parents
  • Hello,

    I've checked the latest version of the project from the master branch:
    https://github.com/analogdevicesinc/no-OS/tree/master/ad9467-fmc-ebz

    With the 2019_R1 HDL release for this project.

    Using the common_drivers https://github.com/analogdevicesinc/no-OS/tree/master/common_drivers

    (you will have to change the "#include "spi.h"" with "#include "platform_drivers.h"" in the ad9467.h and ad9517.h files, since the drivers are using a newer version of communication drivers)

    I've checked multiple times the output and I did not get different results (as you mentioned in your case).

    The output is always this one:

    *****************************************************
      ADI AD9467-FMC-EBZ Reference Design
      AD9467 CHIP ID: 0x50
      AD9467 CHIP GRADE: 0x20
      AD9517 CHIP ID: 0xd3d3
    *****************************************************
    adc_setup adc core initialized (186 MHz).
                                             AD9467[0x016]: 00
    adc_delay: setting zero error delay (28)
    ADC Test: mode - MIDSCALE
              format - OFFSET BINARY
            Test passed
    ADC Test: mode - MIDSCALE
              format - TWOS_COMPLEMENT
            Test passed
    ADC Test: mode - POS_FULLSCALE
              format - OFFSET BINARY
            Test passed
    ADC Test: mode - POS_FULLSCALE
              format - TWOS_COMPLEMENT
            Test passed
    ADC Test: mode - NEG_FULLSCALE BINARY
              format - OFFSET BINARY
            Test passed
    ADC Test: mode - NEG_FULLSCALE BINARY
              format - TWOS_COMPLEMENT
            Test passed
    ADC Test: mode - CHECKERBOARD
              format - OFFSET BINARY
            Test passed
    ADC Test: mode - CHECKERBOARD
              format - TWOS_COMPLEMENT
            Test passed
    ADC Test: mode - PN_23_SEQUENCE
              format - OFFSET BINARY
              Test passed
    ADC Test: mode - PN_23_SEQUENCE
              format - TWOS_COMPLEMENT
              Test skipped
    ADC Test: mode - PN_9_SEQUENCE
              format - OFFSET BINARY
      ERROR: PN status(0002).
    ADC Test: mode - PN_9_SEQUENCE
              format - TWOS_COMPLEMENT
              Test skipped
    ADC Test: mode - ONE_ZERO_TOGGLE
              format - OFFSET BINARY
            Test passed
    ADC Test: mode - ONE_ZERO_TOGGLE
              format - TWOS_COMPLEMENT
            Test passed
    Testing done.
    Start capturing data...

    Done.

    Also, the data in the memory (0x80800000) looks fine for the test modes (+ Full-scale, - Full-scale, Checkerboard).

    Regards,

    Antoniu

Reply
  • Hello,

    I've checked the latest version of the project from the master branch:
    https://github.com/analogdevicesinc/no-OS/tree/master/ad9467-fmc-ebz

    With the 2019_R1 HDL release for this project.

    Using the common_drivers https://github.com/analogdevicesinc/no-OS/tree/master/common_drivers

    (you will have to change the "#include "spi.h"" with "#include "platform_drivers.h"" in the ad9467.h and ad9517.h files, since the drivers are using a newer version of communication drivers)

    I've checked multiple times the output and I did not get different results (as you mentioned in your case).

    The output is always this one:

    *****************************************************
      ADI AD9467-FMC-EBZ Reference Design
      AD9467 CHIP ID: 0x50
      AD9467 CHIP GRADE: 0x20
      AD9517 CHIP ID: 0xd3d3
    *****************************************************
    adc_setup adc core initialized (186 MHz).
                                             AD9467[0x016]: 00
    adc_delay: setting zero error delay (28)
    ADC Test: mode - MIDSCALE
              format - OFFSET BINARY
            Test passed
    ADC Test: mode - MIDSCALE
              format - TWOS_COMPLEMENT
            Test passed
    ADC Test: mode - POS_FULLSCALE
              format - OFFSET BINARY
            Test passed
    ADC Test: mode - POS_FULLSCALE
              format - TWOS_COMPLEMENT
            Test passed
    ADC Test: mode - NEG_FULLSCALE BINARY
              format - OFFSET BINARY
            Test passed
    ADC Test: mode - NEG_FULLSCALE BINARY
              format - TWOS_COMPLEMENT
            Test passed
    ADC Test: mode - CHECKERBOARD
              format - OFFSET BINARY
            Test passed
    ADC Test: mode - CHECKERBOARD
              format - TWOS_COMPLEMENT
            Test passed
    ADC Test: mode - PN_23_SEQUENCE
              format - OFFSET BINARY
              Test passed
    ADC Test: mode - PN_23_SEQUENCE
              format - TWOS_COMPLEMENT
              Test skipped
    ADC Test: mode - PN_9_SEQUENCE
              format - OFFSET BINARY
      ERROR: PN status(0002).
    ADC Test: mode - PN_9_SEQUENCE
              format - TWOS_COMPLEMENT
              Test skipped
    ADC Test: mode - ONE_ZERO_TOGGLE
              format - OFFSET BINARY
            Test passed
    ADC Test: mode - ONE_ZERO_TOGGLE
              format - TWOS_COMPLEMENT
            Test passed
    Testing done.
    Start capturing data...

    Done.

    Also, the data in the memory (0x80800000) looks fine for the test modes (+ Full-scale, - Full-scale, Checkerboard).

    Regards,

    Antoniu

Children