Post Go back to editing

AD9467 KC705 Reference design

Thread Summary

The user is troubleshooting the AD9467 FMC reference design on the KC705 FPGA board, experiencing inconsistent test results and incorrect waveforms when dumping data from DDR3. The final answer confirms the need for an external clock and suggests that the input is AC-coupled, not suitable for square waves. The user should connect a 10 MHz sine wave clock and consider modifying the analog input coupling to DC if necessary.
AI Generated Content

hi all,

I use the AD9467 default FMC reference design on KC705(https://wiki.analog.com/resources/fpga/xilinx/fmc/ad9467#more_information).
However I face many problems while executing ad9467_fmc_ebz.c:
1. I have no idea whether the software project build successfully.

   There is the project contents and build settings.
project contents 


2. Sometimes I get "Test passed", and sometimes I get ERRORs.


3. How can I read the data in ddr3?
I have tried to dump file by Xilinx>Dump/Restor Data File and setting Start Address = 0, Size = 8192,
The data I dumped isn't correct (The input signal is 1 Vpp , 1.2Vdc ,1MHz sine wave)

Could any body give me some advices.
Thanks,
Wei-Chieh

Parents
  • Today, I tried dump file by Xilinx>Dump/Restor Data File and setting Start Address = 0x80800000, Size = 16384,
    And the dump data is processed by data = data(1:2:end) + data(2:2:end) * 256;
    Then I get the following,

    <1MHz Sine, 2-Vpp>                                                                                  <1MHz Square, 2-Vpp>   

                         

    However, the wave form is weird.

Reply
  • Today, I tried dump file by Xilinx>Dump/Restor Data File and setting Start Address = 0x80800000, Size = 16384,
    And the dump data is processed by data = data(1:2:end) + data(2:2:end) * 256;
    Then I get the following,

    <1MHz Sine, 2-Vpp>                                                                                  <1MHz Square, 2-Vpp>   

                         

    However, the wave form is weird.

Children
  • Question moved to Microcontroller no-OS Drivers forum.
    Someone here can help you out with the capture scrips(moving data from DDR to computer).

  • Regarding the captured wave forms. In the above images you posted, In the left one your format is wrong, Try printing the data in two's complement not binary offset.
    Regarding the right image, there should be some filters on the evaluation board before the AD9467. As I can see in your captured waveform the input is AC coupled not DC, meaning your signal will look more like waveform on charging/discharging capacitor. Are you using the AIN input on the evaluation board?

    Andrei

  • Hi Andrei,

    I use AIN input on evaluation.

    I am not sure how the data store in DDR3. I suggest the 16-bit datas are stored as the following structure:

    Addr |               dma.transfer->start_address            |          dma.transfer->start_address + 1             |
    Data |    D[15] D[13] D[11] D[9] D[7] D[5] D[3] D[1]   |    D[14] D[12] D[10] D[8] D[6] D[4] D[2] D[0]    | 

    I tried to print data in two's complement and finally I get the following wave form:

    <1MHz Sine, 2-Vpp>                                                                          

       

    <1MHz Square, 2-Vpp>

    Both the waveform looks weird,

    Thanks

    Wei-Chieh

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.