AD9361 Filter Wizard - Input Parameters

Hi,

We are using the MATLAB GUI Filter tool to generate FIR filter parameters for AD9364. The wiki description mentions the Rdata variable which is the sample rate, is this the same as the 'Data' input field in the GUI? Is the unit for that in MSPS? If that is the case, when I set the sample rate to 61.44 (MSPS presumably), Fpass is 20.48 MHz, meaning bandwidth should be 40.96 MHz which is less than the 'Data' rate. How is this possible?

If this field does not contain the sample rate, but instead is the raw data rate, how is this related to sample rate and what modulation is being used?

Regards,

Sanjeev