Hello,
I am using the ADRV9009+ZCU102 and am trying to run headless.c.
I have taken the following steps:
1. Obtained the Linux image here: https://wiki.analog.com/resources/tools-software/linux-software/zynq_images I am using the system.dtb and BOOT.bin provided for the ZCU102 + ADRV9009 and the Linux image from zynqmp-common.
2. Built the FPGA project from here: https://github.com/analogdevicesinc/hdl
3. Obtained no-OS source code: github.com/.../no-OS
4. In the Xilinx SDK, I followed these steps: https://wiki.analog.com/resources/eval/user-guides/adrv9009/no-os-setup
I am able to build the project successfully, but I get a segmentation fault when I try to run the resulting .elf. I found that the program is failing at the function AD9528_initDeviceDataStruct() in headless.c. This eventually calls function XGpioPs_WriteReg in xgpiops.c:
Additionally, I notice the following compiler warnings when building the program:
To build the project without error, I had to change the compiler in the SDK from arm-none-eabi-gcc to arm-linux-gnueabihf-gcc. Are the above warnings due to that? It seems that the BSP code is still being built with arm-none-eabi-gcc. What is the best way to change the compiler in the BSP project? Could this be the reason I'm running into a seg fault, or is there something else that I am missing?
I appreciate the help.