i'm having an calibration timeout error of (0x244, 0x80) with AD9361.
i'm using the Tiva TM4CNCPDT1294 controller to generate the communication with the AD9361.
the configuration file that is being used is for 947.5 MHz.
Please Help.
AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiverâ„¢ designed for use in 3G and
4G base station applications....
Datasheet
AD9361 on Analog.com
i'm having an calibration timeout error of (0x244, 0x80) with AD9361.
i'm using the Tiva TM4CNCPDT1294 controller to generate the communication with the AD9361.
the configuration file that is being used is for 947.5 MHz.
Please Help.
Hey,
Has this been resolved ?
Thanks
Alex
Hi, I am getting same error while running No-OS on pluto sdr!!!
Hi, I am getting same error while running No-OS on pluto sdr!!!
Waleed Please create a separate thread for your question. Answered thread are ignored by staff.
-Travis