AnsweredAssumed Answered


Question asked by on Mar 8, 2012
Latest reply on Mar 9, 2012 by

I have interest in use Adum3472 to isolate two micro controlers and DSS and VGA.

The problem is: in side A I have a Li-On cell (3V to 4.2V) and in side B I need +5V and -5V and based in DataSheet Adum34x function only in range of 3 to 3.6V or 4 to 5V. I need input range of 3 to 4.2V.

Is posible?

If obtain only +5 in the output is't OK.


Thank you in advance.


Aldo Ferszt

General Manager