AnsweredAssumed Answered

AD9522-4: how to obtain an 800MHz single-ended output

Question asked by luca.banchi on Jun 1, 2016
Latest reply on Jun 1, 2016 by pkern

Dear support,


in my design an AD9522-4 is involved in order to generate all the clocks required in the system from a 100MHz reference.

The on-chip VCO is tuned to 1600MHz in order to generate all the frequencies I require. Among them, an 800MHz single-ended sinewave is required. Since the AD9522 LVDS output can work up to 800MHz, I would ask if there is an effective way to convert the LVDS output in a single-ended 50Ohm signal, then the filter to select the 800MHz fundamental frequency will be my own job.


Do you have a reference design to obtain this signal conversion?


Thank you for your response