AnsweredAssumed Answered

ADXL321 replacement

Question asked by Roman_ on Dec 9, 2015
Latest reply on Sep 27, 2016 by FRCmentor

On the "Not Recommended for New Designs" ADXL321 page ADXL326 is indicated as a replacement part. But for the ADXL326 supply voltage range is 1.8 to 3.6V while for the ADXL321 supply voltage range is 2.4 V to 6V. So  ADXL326 is not a suitable replacement for the ADXL321 for the 5V supplied systems.

Does the 5V supplied pin-to-pin compatable replacement for the ADXL321 exist and what is the possible production period for this part?


Also I have noticed the ADXL203 is not recommended for new designs too.

Is it applied for all versions (ADXL203, AD22037 and AD22293) or only for 1.7g version?

What is a replacement for the AD22037 and AD22293?