AnsweredAssumed Answered

Encode problems in ADV202

Question asked by taku on Apr 5, 2011
Latest reply on Apr 11, 2011 by DaveD

I am tring to encode mono-chrome image (640x480 pixels) when input is RAW mode and output is single transfer DREQ/ACK DMA mode in ADV202.
I have 2 problems.

1. VRDY becomes '0' at 305718bytes when i input pixel until 640x480=307200bytes
   Is the remaind byte (307200-305718=1382bytes) lost, or not.
   What is set, if i want to input correctly pxiel size ?

2. I could encode the first image (305718bytes). But i can not encode next image.
   Is the register setting needed before input next image ?
   What shall i do, if need ?

 

Please give me a advise.
--
Kubo

Outcomes