Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
MEMS Inertial Sensors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
MEMS Inertial Sensors
MEMS Inertial Sensors
Documents ADXL362 + Arduino: Using Interrupts to Implement Motion-Activated Sleep
  • Q&A
  • Files
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +3-D Model/STEP: FAQ
  • +AD22282-A-R2: FAQ
  • +ADIS16000: FAQ
  • +ADIS16003 MTBF: FAQ
  • +ADIS16006: FAQ
  • +ADIS16201: FAQ
  • +ADIS16203: FAQ
  • +ADIS16204: FAQ
  • +ADIS16209: FAQ
  • +ADIS16210: FAQ
  • +ADIS16223: FAQ
  • +ADIS16227: FAQ
  • +ADIS16228: FAQ
  • +ADIS16229: FAQ
  • +ADIS16240: FAQ
  • +ADIS16255: FAQ
  • +ADIS16355: FAQ
  • +ADIS16364: FAQ
  • +ADIS16365: FAQ
  • +ADIS16375: FAQ
  • +ADIS16385: FAQ
  • +ADIS16400: FAQ
  • +ADIS16405: FAQ
  • +ADIS16407: FAQ
  • +ADIS16445: FAQ
  • +ADIS16448: FAQ
  • +ADIS16460: FAQ
  • +ADIS16475: FAQ
  • +ADIS16477: FAQ
  • +ADIS1647x: FAQ
  • +ADIS16480: FAQ
  • +ADISUSB: FAQ
  • +ADXL001: FAQ
  • +ADXL203: FAQ
  • +ADIS16300: FAQ
  • +ADIS16485: FAQ
  • +ADIS16488: FAQ
  • +ADIS16488A: FAQ
  • +ADIS16490: FAQ
  • +ADIS16495: FAQ
  • +ADIS16497: FAQ
  • +ADXL103: FAQ
  • +ADXL150: FAQ
  • +ADxL193: FAQ
  • +ADXL202: FAQ
  • +ADXL206: FAQ
  • +ADXL210: FAQ
  • +ADXL210E: FAQ
  • +ADXL213: FAQ
  • +ADxL230: FAQ
  • +ADXL278: FAQ
  • +ADXL312: FAQ
  • +ADXL313: FAQ
  • +ADXL320: FAQ
  • +ADXL321: FAQ
  • +ADXL322: FAQ
  • +ADXL327: FAQ
  • +ADXL335: FAQ
  • +ADXL337: FAQ
  • +ADXL345: FAQ
  • +AD22290: FAQ
  • +ADIS16003: FAQ
  • +ADIS16133: FAQ
  • +ADIS16135: FAQ
  • +ADIS16265: FAQ
  • +ADIS16305: FAQ
  • +ADXL326: FAQ
  • +ADXL350: FAQ
  • -ADXL362: FAQ
    • ADXL362 + Arduino: Using Interrupts to Implement Motion-Activated Sleep
    • ADXL362 200Hz Bandwidth
    • ADXL362 Arduino How-To
    • ADXL362 as a Motion Switch
    • ADXL362 Clock Accuracy
    • ADXL362 Current Usage versus Competitors
    • ADXL362 Evaluation Boards
    • ADXL362 External Sync Pin
    • ADXL362 FIFO
    • ADXL362 FIFO Advantages
    • ADXL362 footprint error in datasheet (Rev C)
    • ADXL362 Motion Status Indicator Pin
    • ADXL362 register configuration
    • ADXL362 Self Test Procedure
    • ADXL362 Target Applications
    • ADXL362 Wakeup Mode vs. Full Power Mode
    • ADXL362  advantages as a motion switch
    • ADXL362: Acceleration beyond measurement range
    • ADXL362: Accessing real-time data in Wakeup Mode
    • ADXL362: autosleep mode
    • ADXL362: Bare minimum to acquire data
    • ADXL362: Output Data Rates (ODR)
    • ADXL362: Wakeup Mode and Autosleep
    • ADXL362: Wider bandwitdh than 200Hz
    • Are customers parts close to the ADXL362
    • EVAL-ADXL362Z-MLP threshold setting
    • Evaluating the ADXL362
    • Is ADXL362 data AC coupled?
    • Is ultrasonic welding a suitable assembly process for ADXL362 ?
    • Logging Data Prior to an Event
    • ADXL362 Blinky Demo
    • How to use the ADXL362 to eliminate a power switch and control system power
  • +ADXL375: FAQ
  • +ADXL377: FAQ
  • +ADXL78: FAQ
  • +ADXRS150: FAQ
  • +ADXRS290: FAQ
  • +ADXRS300: FAQ
  • +ADXRS401: FAQ
  • +ADXRS453: FAQ
  • +ADXRS610: FAQ
  • +ADxRS614: FAQ
  • +ADXRS623: FAQ
  • +ADXRS646: FAQ
  • +ADXRS652: FAQ
  • +ADXRS800: FAQ
  • +ADIS16136: FAQ
  • +ADIS16137: FAQ
  • +ADIS16266: FAQ
  • +ADIS16334: FAQ
  • +ADIS16362 Evaluation Tool: FAQ
  • +ADIS16364 Evaluation Tool: FAQ
  • +ADIS16367: FAQ
  • +ADIS163xx: FAQ
  • +ADIS16489: FAQ
  • +ADIS1648x: FAQ
  • +ADXL346: FAQ
  • +ADXL363: FAQ
  • +EVAL-ADIS: FAQ
  • +EVAL-ADIS2: FAQ
  • +Filtering Functions: FAQ
  • +General: FAQ
  • +Gyroscope: FAQ
  • +Hard & Soft Iron Correction: FAQ
  • +ISEB USB: FAQ
  • +IMU: FAQ
  • +MEMS: FAQ
  • +Slip Ring Interface: FAQ
  • +SPI Troubleshooting: FAQ
  • +TEMP_OUT Variation: FAQ
  • +Test Procedures: FAQ
  • +AD590: FAQ
  • +AD5940: FAQ
  • +AD5941: FAQ
  • +AD595: FAQ
  • +AD8495: FAQ
  • +AD8497: FAQ
  • +ADIS16IMU2 FAQ:
  • +ADUCM355: FAQ
  • +ADXL343: FAQ
  • +ADXL357: FAQ
  • +ADXL367: FAQ
  • +Breakout Board FAQ:
  • +CN0429: FAQ
  • DS1922E: FAQ
  • +DS1922L: FAQ
  • +DS1922T: FAQ
  • +DS1923: FAQ
  • +EVAL-ADXL312-SDP: FAQ
  • +IMU/Gryoscope Alignment FAQ:
  • +iSensor FAQ:
  • +MAX30001: FAQ
  • +MAX30003: FAQ
  • +MAX30003CTI+: FAQ
  • +MAX30003WING: FAQ
  • +MAX30009EVKIT: FAQ
  • +MAX30134EVSYS: FAQ
  • +MAX9621: FAQ
  • +TMP01: FAQ
  • +Wireless Vibration Sensors FAQ:

ADXL362 + Arduino: Using Interrupts to Implement Motion-Activated Sleep

This tutorial details, step-by-step, how to use an ADXL362 to put an Arduino in a low-power state when the circuit is not moving, and then power it back up when motion is detected.

Before you get started:

If you haven't already, make sure you are able to successfully complete the ADXL362 Arduino How-To tutorial, which will guide you through hookup, ADXL362 Arduino library installation, and uploading/executing the "ADXL362_SimpleRead" example.  Any unresolved issues you have while working through the first tutorial will cause you trouble in this one.

Download the Rocket Scream Low Power Arduino Library:

I'm sure there are many good examples/libraries for putting your Arduino to sleep, but I have had good luck with Rocket Scream's Low Power Arduino library - download zip file here.

In my examples, I renamed the "Low-Power" top level library directory to "LowPower".  (My environment doesn't like the hyphen... I'm not sure if it's an OS issue, or perhaps the hyphen worked fine on an older version of the Arduino software?  Either way... please remove the hyphen to make the library work with my example code.)

Remember lessons learned while installing the ADXL362 Arduino library in previous tutorial.  "LowPower" library folder should be placed in your <sketchbook>/libraries folder.

You libraries directory structure should look like the picture below.  Go to ADXL362 Arduino How-To for a more detailed description of how to install Arduino libraries.

If you have it installed successfully, The Rocket Scream LowPower library will show up under Sketch -> Import Library -> LowPower (See image below):

Add interrupt connection between ADXL362 and Arduino:

This sleep example utilizes the INT1 pin of the ADXL362, and the Interrupt 0 (digital pin 2) on the Arduino.  So, adding to the connections that were made on the previous tutorial, add a wire to connect INT1 pin on the ADXL362 to DP2 pin on the Arduino.  See image below for an illustration of required connections:

More information about Arduino interrupts can be found at https://arduino.cc/en/Reference/AttachInterrupt

Upload ADXL362_MotionActivatedSleep sketch to Arduino:

Once you have completed steps above, uploading the ADXL362_MotionActivatedSleep example to your Arduino should be simple and straightforward.  The Motion activated sleep example requires the LowPower library to be properly installed.

Open the example by clicking File -> Examples -> ADXL362 -> ADXL362_MotionActivatedSleep, as shown in image below:

Make sure you have the correct board and serial port selected (see previous tutorial) and click the Upload button, as illustrated below:

Observe awake/asleep activity on Serial Monitor:

Open the serial monitor,  and watch as your circuit goes to sleep and wakes up, depending on if it's being shaken or moved.

In the example code, the circuit stays "on" for two seconds after it's been motionless, then shuts off.  The on/off timing, as well as the motion threshold, can be changed by tweaking the activity/inactivity interrupt settings, which I've set with the setupDCActivityInterrupt and setupDCInactivityInterrupt functions.

Or, Observe awake/Asleep activity with a multimeter:

To measure overall current, I disconnected the Pro Mini Arduino from my PC and FTDI Basic, and connected a multimeter in series with a 4.5V battery supply - I connected the battery supply to the RAW pin of my Pro Mini Arduino.  My quick observation was that the overall circuit consumes a little over 4mA while awake, and roughly 270uA while asleep.

  This tutorial does not include a thorough investigation of what portions of the circuit are consuming what portion of the overall power dissipation.  But in this example, the ADXL362 consumes less than 3uA while on, and 300nA while the circuit is "sleeping." (The ADXL362 current consumption varies slightly with output data rate, input voltage, and mode)  Therefore, most of the overall current, awake or asleep, is being consumed by the Pro Mini Arduino.  I'll leave it to the reader to conduct their own experiments regarding power consumption.

Images below - Current consumption while Pro Mini Arduino + ADXL362 circuit is "awake," and "asleep."

And, for even lower sleep power, use a Rocket Scream Ultra Mini Arduino-compatible

So, as much as I love, love, love the Pro Mini, I wasn't completely satisfied with the sleep current of my overall circuit.  And, I probably could have hacked my Pro Mini to make a few improvements (removing the 10K resistor across VCC comes to mind), I instead decided to purchase a Rocket Scream Mini Ultra Arduino-compatible board, especially since I'm using their handy Arduino library for sleep modes.

https://www.rocketscream.com/blog/wp-content/uploads/2011/07/miniUltra8Mhz.jpg

   Using the Mini Ultra, I was able to get my sleep current down to roughly 2uA! That's more like it!

Image below - Current consumption while Mini Ultra + ADXL362 circuit is  "asleep."

What am I going to do with my motion-activated Arduino?

I have a few ideas... stay tuned!

 

Tags: lowest_power sensors accelerometers motion arduino ADXl362 motion_detection low_power lowpower Show More
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • ADXL362 Arduino How-To
    GenevaC
    What you'll need: A 3.3V Arduino, such as: Arduino Pro Mini (3.3V version) - requires FTDI Breakout (3.3V version) Or, Arduino Pro (3.3V version) - requires FTDI Breakout (3.3V version) ...
  • Comment on ADXL362 + Arduino: Using Interrupts to Implement Motion-Activated Sleep
    stefanoc
    Hi, thanks for your tutorial and for your library. I've a problem. I installed your Arduino ADXL362 library; everything works fine and the demo "ADXL362_SimpleRead" has no problem. Instead, loading the...
  • Comment on ADXL362 + Arduino: Using Interrupts to Implement Motion-Activated Sleep
    AnneM
    Stefano, Oh no! So sorry for the trouble... I can verify I'm having the same issue. A month or so ago, I merged in a bunch of pull requests, many of which were excellent improvements. It looks like...
 
Related Content
  • ADXL362 Arduino How-To
    GenevaC
    What you'll need: A 3.3V Arduino, such as: Arduino Pro Mini (3.3V version) - requires FTDI Breakout (3.3V version) Or, Arduino Pro (3.3V version) - requires FTDI Breakout (3.3V version) ...
  • Comment on ADXL362 + Arduino: Using Interrupts to Implement Motion-Activated Sleep
    stefanoc
    Hi, thanks for your tutorial and for your library. I've a problem. I installed your Arduino ADXL362 library; everything works fine and the demo "ADXL362_SimpleRead" has no problem. Instead, loading the...
  • Comment on ADXL362 + Arduino: Using Interrupts to Implement Motion-Activated Sleep
    AnneM
    Stefano, Oh no! So sorry for the trouble... I can verify I'm having the same issue. A month or so ago, I merged in a bunch of pull requests, many of which were excellent improvements. It looks like...