Q:
Do you have a VB.NET software development kit (SDK) for the EVAL-ADIS?
A:
--------------------------------------------------------------------------------------------------------------
The EVAL-ADIS provides a basic communication conduit between Windows-PCs and many of the iSensor products (ADIS16xxx). It provides functional evaluation support to those who were also developing a direct interface between an ADIS16xxx product and their preferred SPI-compatible processor. Custom software development is not listed as a "feature" or "promised function" in any of the EVAL-ADIS documentation, but the attached file provides a potential starting point for prototype data collection. Download this file to access the VB.NET DLL file, along with an example VB.NET project. The project file provides examples for reading registers, writing to registers and a streaming data acquisition function.
Hello Everyone!
We just posted a 64-bit version of this DLL at https://ez.analog.com/docs/DOC-17643
Take care!
Is there any examples or settings up an "event" based register read instead of the polling queue version? Is this possible with the DLL?
Thank you for your question. What type of event are you hoping to use, in order to trigger the register access?
I was hoping that there would be some event that I could trigger on when new data was available instead of polling a queue to see if it is full or empty. Is this possible with the DLL?
I am not a software developer, but I was under the impression that the data reads in this SPI were triggered by the data-ready signal pulsing, which the IMUs provide for this exact purpose. Let me ask one of our developers if they can comment on this and get back to you.
Let me give you some brief details of what we'd like to do. We want to be able to put a high precision time-stamp on motion data for a platform. It needs to be as accurate as possible. So, we need to be able to capture the time when the measurement is generated. If it is put into a queue without a timestamp, then we have no way of knowing when that sample was created. We realize that this is a non-realtime, development system. But, we are in the evaluation (R&D) stage and just need the ability to capture accurate, time-stamped motion data.
I appreciate that, but we probably can't accept "as accurate as possible" as our objective. I can imagine a number of limitations to this, some of which could be very expensive for us to address on this platform. Let me give this a little more thought, but it might help to know which IMU you are evaluating with the EVAL-ADISx platform to evaluate. Can you share that?