Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    View All Webinars
  • Community Hub

    Challenge Yourself!

      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
MEMS Inertial Sensors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
MEMS Inertial Sensors
MEMS Inertial Sensors
Documents ADIS16209/ADIS16265 Lead Integrity
  • Q&A
  • Files
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +3-D Model/STEP: FAQ
  • +AD22282-A-R2: FAQ
  • +ADIS16000: FAQ
  • +ADIS16003 MTBF: FAQ
  • +ADIS16006: FAQ
  • +ADIS16201: FAQ
  • +ADIS16203: FAQ
  • +ADIS16204: FAQ
  • -ADIS16209: FAQ
    • ADIS162xx LGA Assembly Guidelines
    • ADIS16209 Evaluation Tool Overview
    • ADIS16209 Self-Test Management
    • ADIS16209/ADIS16265 Lead Integrity
    • ADIS16209/ADIS16265 Pb-free Assembly Tips
    • ADIS1620x/21x/22x Power Regulator Suggestion
    • ADIS1620x/21x/22x Power Supply Considersations
    • Tilt Angle Window Detector
    • Tilt Angle Window Detector with Evaluation Tools
    • Bias Stability over 1 Year
    • IMU Evaluation Software Bug: ADIS16209 Data Capture
    • The direction of axis X and axis Y
    • ADIS16201 and ADIS16209 Pins 8 and 10 Grounded - Performance Issues
    • ADIS16209 Datasheet Error: Address code length
    • ADIS16209 Datasheet Error; SPI Address Code Missing MSB
    • ADIS16209 Datecode Revision Change
    • ADIS16209 self-test
    • ADIS16209: How do I connect pins 7,8,10,11? There are contradictions in datasheet.
    • ADIS16209: Stability and sensitivity
    • ADIS1620x Evaluation Board dimensions
  • +ADIS16210: FAQ
  • +ADIS16223: FAQ
  • +ADIS16227: FAQ
  • +ADIS16228: FAQ
  • +ADIS16229: FAQ
  • +ADIS16240: FAQ
  • +ADIS16255: FAQ
  • +ADIS16355: FAQ
  • +ADIS16364: FAQ
  • +ADIS16365: FAQ
  • +ADIS16375: FAQ
  • +ADIS16385: FAQ
  • +ADIS16400: FAQ
  • +ADIS16405: FAQ
  • +ADIS16407: FAQ
  • +ADIS16445: FAQ
  • +ADIS16448: FAQ
  • +ADIS16460: FAQ
  • +ADIS16475: FAQ
  • +ADIS16477: FAQ
  • +ADIS1647x: FAQ
  • +ADIS16480: FAQ
  • +ADISUSB: FAQ
  • +ADXL001: FAQ
  • +ADXL203: FAQ
  • +ADIS16300: FAQ
  • +ADIS16485: FAQ
  • +ADIS16488: FAQ
  • +ADIS16488A: FAQ
  • +ADIS16490: FAQ
  • +ADIS16495: FAQ
  • +ADIS16497: FAQ
  • +ADXL103: FAQ
  • +ADXL150: FAQ
  • +ADxL193: FAQ
  • +ADXL202: FAQ
  • +ADXL206: FAQ
  • +ADXL210: FAQ
  • +ADXL210E: FAQ
  • +ADXL213: FAQ
  • +ADxL230: FAQ
  • +ADXL278: FAQ
  • +ADXL312: FAQ
  • +ADXL313: FAQ
  • +ADXL320: FAQ
  • +ADXL321: FAQ
  • +ADXL322: FAQ
  • +ADXL327: FAQ
  • +ADXL335: FAQ
  • +ADXL337: FAQ
  • +ADXL345: FAQ
  • +AD22290: FAQ
  • +ADIS16003: FAQ
  • +ADIS16133: FAQ
  • +ADIS16135: FAQ
  • +ADIS16265: FAQ
  • +ADIS16305: FAQ
  • +ADXL326: FAQ
  • +ADXL350: FAQ
  • +ADXL362: FAQ
  • +ADXL375: FAQ
  • +ADXL377: FAQ
  • +ADXL78: FAQ
  • +ADXRS150: FAQ
  • +ADXRS290: FAQ
  • +ADXRS300: FAQ
  • +ADXRS401: FAQ
  • +ADXRS453: FAQ
  • +ADXRS610: FAQ
  • +ADxRS614: FAQ
  • +ADXRS623: FAQ
  • +ADXRS646: FAQ
  • +ADXRS652: FAQ
  • +ADXRS800: FAQ
  • +ADIS16136: FAQ
  • +ADIS16137: FAQ
  • +ADIS16266: FAQ
  • +ADIS16334: FAQ
  • +ADIS16362 Evaluation Tool: FAQ
  • +ADIS16364 Evaluation Tool: FAQ
  • +ADIS16367: FAQ
  • +ADIS163xx: FAQ
  • +ADIS16489: FAQ
  • +ADIS1648x: FAQ
  • +ADXL346: FAQ
  • +ADXL363: FAQ
  • +EVAL-ADIS: FAQ
  • +EVAL-ADIS2: FAQ
  • +Filtering Functions: FAQ
  • +General: FAQ
  • +Gyroscope: FAQ
  • +Hard & Soft Iron Correction: FAQ
  • +ISEB USB: FAQ
  • +IMU: FAQ
  • +MEMS: FAQ
  • +Slip Ring Interface: FAQ
  • +SPI Troubleshooting: FAQ
  • +TEMP_OUT Variation: FAQ
  • +Test Procedures: FAQ
  • +AD590: FAQ
  • +AD5940: FAQ
  • +AD5941: FAQ
  • +AD595: FAQ
  • +AD8495: FAQ
  • +AD8497: FAQ
  • +ADIS16IMU2 FAQ:
  • +ADUCM355: FAQ
  • +ADXL343: FAQ
  • +ADXL357: FAQ
  • +ADXL367: FAQ
  • +Breakout Board FAQ:
  • +CN0429: FAQ
  • DS1922E: FAQ
  • +DS1922L: FAQ
  • +DS1922T: FAQ
  • +DS1923: FAQ
  • +EVAL-ADXL312-SDP: FAQ
  • +IMU/Gryoscope Alignment FAQ:
  • +iSensor FAQ:
  • +MAX30001: FAQ
  • +MAX30003: FAQ
  • +MAX30003CTI+: FAQ
  • +MAX30003WING: FAQ
  • +MAX30009EVKIT: FAQ
  • +MAX30134EVSYS: FAQ
  • +MAX9621: FAQ
  • +TMP01: FAQ
  • +Wireless Vibration Sensors FAQ:

ADIS16209/ADIS16265 Lead Integrity

UPDATE ALERT!

Please visit the following link for an updated set of assembly instructions:

FAQ: ADIS162xx LGA Assembly Guidelines

 

Start of older assembly instructions, for historical reference but not for present use>>

Q:

What is causing my ADIS16209 leads to fracture or crack on my PCB?

A:

--------------------------------------------------------------------------------------------------------

Without knowing specific details of any particular case, we can offer that this is most often caused by PCB bending, which places peeling stress on one or more of the leads. From our experience, the two most common causes of PCB bending are in the array separation process (after array-level processing is complete) and in drop testing (in-system).  While the bending stress associated with score and snap operations may seem to be very small, the ADIS16209's rigid structure (for best physical stability while in normal operation) and small leads do not provide a large amount of adhesion strength either.  Keep in mind, this is not a matter of device quality, but a matter of physics.

Fortunately, there are two things that can be done to help address this sensitivity.

  1. Employ a low-stress array separation technique.  For example, we use a router bit to cut finished PCB out of their arrays for our evaluation boards, such as the ADIS16209/PCBZ. This process has helped produce over 3000 boards with very high yields.
  2. Use an under-fill material to spread peeling stress across the entire ADIS16209 package bottom.

SUGGESTIONS FOR ADDITIONAL READING:

Use of under-fill materials, for the purpose of strengthening BGA and LGA interfaces:

http://www.embedded.com/design/system-integration/4235387/Underfill-revisited--How-a-decades-old-technique-enables-smaller--more-durable-PCBs

The impact array separation techniques have on ceramic capacitors:

http://www.smtinline.com/html-en/cap-failure.html

For more detailed information on ADIS16xxx LGA assembly, check out the following post:

https://ez.analog.com/docs/DOC-2962

Hope that helps everyone!

Best,

NevadaMark

Tags: adis16220 adis16209 adis16265 pcb_separation adis16204 adis16266 adis16006 sensors lead_broken adis16060 adis16003 adis16203 lead_crack Accelerometers - Special Purpose adis16260 lead_fracture lead_break adis16201 productpage adis16240 Show More