Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    Upcoming Learning & Events

    • Fast-Track Certification: Leveraging IC Safety App Notes for Functional Safety Designs
    View All Webinars
  • Community Hub

    Challenge Yourself!

      World Engineering Day Quiz!

      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
MEMS Inertial Sensors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
MEMS Inertial Sensors
MEMS Inertial Sensors
Documents Tilt Angle Window Detector
  • Q&A
  • Files
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +3-D Model/STEP: FAQ
  • +AD22282-A-R2: FAQ
  • +ADIS16000: FAQ
  • +ADIS16003 MTBF: FAQ
  • +ADIS16006: FAQ
  • +ADIS16201: FAQ
  • +ADIS16203: FAQ
  • +ADIS16204: FAQ
  • -ADIS16209: FAQ
    • ADIS162xx LGA Assembly Guidelines
    • ADIS16209 Evaluation Tool Overview
    • ADIS16209 Self-Test Management
    • ADIS16209/ADIS16265 Lead Integrity
    • ADIS16209/ADIS16265 Pb-free Assembly Tips
    • ADIS1620x/21x/22x Power Regulator Suggestion
    • ADIS1620x/21x/22x Power Supply Considersations
    • Tilt Angle Window Detector
    • Tilt Angle Window Detector with Evaluation Tools
    • Bias Stability over 1 Year
    • IMU Evaluation Software Bug: ADIS16209 Data Capture
    • The direction of axis X and axis Y
    • ADIS16201 and ADIS16209 Pins 8 and 10 Grounded - Performance Issues
    • ADIS16209 Datasheet Error: Address code length
    • ADIS16209 Datasheet Error; SPI Address Code Missing MSB
    • ADIS16209 Datecode Revision Change
    • ADIS16209 self-test
    • ADIS16209: How do I connect pins 7,8,10,11? There are contradictions in datasheet.
    • ADIS16209: Stability and sensitivity
    • ADIS1620x Evaluation Board dimensions
  • +ADIS16210: FAQ
  • +ADIS16223: FAQ
  • +ADIS16227: FAQ
  • +ADIS16228: FAQ
  • +ADIS16229: FAQ
  • +ADIS16240: FAQ
  • +ADIS16255: FAQ
  • +ADIS16355: FAQ
  • +ADIS16364: FAQ
  • +ADIS16365: FAQ
  • +ADIS16375: FAQ
  • +ADIS16385: FAQ
  • +ADIS16400: FAQ
  • +ADIS16405: FAQ
  • +ADIS16407: FAQ
  • +ADIS16445: FAQ
  • +ADIS16448: FAQ
  • +ADIS16460: FAQ
  • +ADIS16475: FAQ
  • +ADIS16477: FAQ
  • +ADIS1647x: FAQ
  • +ADIS16480: FAQ
  • +ADISUSB: FAQ
  • +ADXL001: FAQ
  • +ADXL203: FAQ
  • +ADIS16300: FAQ
  • +ADIS16485: FAQ
  • +ADIS16488: FAQ
  • +ADIS16488A: FAQ
  • +ADIS16490: FAQ
  • +ADIS16495: FAQ
  • +ADIS16497: FAQ
  • +ADXL103: FAQ
  • +ADXL150: FAQ
  • +ADxL193: FAQ
  • +ADXL202: FAQ
  • +ADXL206: FAQ
  • +ADXL210: FAQ
  • +ADXL210E: FAQ
  • +ADXL213: FAQ
  • +ADxL230: FAQ
  • +ADXL278: FAQ
  • +ADXL312: FAQ
  • +ADXL313: FAQ
  • +ADXL320: FAQ
  • +ADXL321: FAQ
  • +ADXL322: FAQ
  • +ADXL327: FAQ
  • +ADXL335: FAQ
  • +ADXL337: FAQ
  • +ADXL345: FAQ
  • +AD22290: FAQ
  • +ADIS16003: FAQ
  • +ADIS16133: FAQ
  • +ADIS16135: FAQ
  • +ADIS16265: FAQ
  • +ADIS16305: FAQ
  • +ADXL326: FAQ
  • +ADXL350: FAQ
  • +ADXL362: FAQ
  • +ADXL375: FAQ
  • +ADXL377: FAQ
  • +ADXL78: FAQ
  • +ADXRS150: FAQ
  • +ADXRS290: FAQ
  • +ADXRS300: FAQ
  • +ADXRS401: FAQ
  • +ADXRS453: FAQ
  • +ADXRS610: FAQ
  • +ADxRS614: FAQ
  • +ADXRS623: FAQ
  • +ADXRS646: FAQ
  • +ADXRS652: FAQ
  • +ADXRS800: FAQ
  • +ADIS16136: FAQ
  • +ADIS16137: FAQ
  • +ADIS16266: FAQ
  • +ADIS16334: FAQ
  • +ADIS16362 Evaluation Tool: FAQ
  • +ADIS16364 Evaluation Tool: FAQ
  • +ADIS16367: FAQ
  • +ADIS163xx: FAQ
  • +ADIS16489: FAQ
  • +ADIS1648x: FAQ
  • +ADXL346: FAQ
  • +ADXL363: FAQ
  • +EVAL-ADIS: FAQ
  • +EVAL-ADIS2: FAQ
  • +Filtering Functions: FAQ
  • +General: FAQ
  • +Gyroscope: FAQ
  • +Hard & Soft Iron Correction: FAQ
  • +ISEB USB: FAQ
  • +IMU: FAQ
  • +MEMS: FAQ
  • +Slip Ring Interface: FAQ
  • +SPI Troubleshooting: FAQ
  • +TEMP_OUT Variation: FAQ
  • +Test Procedures: FAQ
  • +AD590: FAQ
  • +AD5940: FAQ
  • +AD5941: FAQ
  • +AD595: FAQ
  • +AD8495: FAQ
  • +AD8497: FAQ
  • +ADIS16IMU2 FAQ:
  • +ADUCM355: FAQ
  • +ADXL343: FAQ
  • +ADXL357: FAQ
  • +ADXL367: FAQ
  • +Breakout Board FAQ:
  • +CN0429: FAQ
  • DS1922E: FAQ
  • +DS1922L: FAQ
  • +DS1922T: FAQ
  • +DS1923: FAQ
  • +EVAL-ADXL312-SDP: FAQ
  • +IMU/Gryoscope Alignment FAQ:
  • +iSensor FAQ:
  • +MAX30001: FAQ
  • +MAX30003: FAQ
  • +MAX30003CTI+: FAQ
  • +MAX30003WING: FAQ
  • +MAX30009EVKIT: FAQ
  • +MAX30134EVSYS: FAQ
  • +MAX9621: FAQ
  • +TMP01: FAQ
  • +Wireless Vibration Sensors FAQ:

Tilt Angle Window Detector

Q:

How can I use a tilt sensor to determine if my instrument has move clockwise or counterclockwise?

-----------------------------------------------------------------------------------------------------------------------------------------------

A:

The ADIS16209 offers a an accurate tilt sensor function, along with two programmable alarms that will simplify this process.  The ADIS16209 offers both horizontal (XINCL_OUT, YINCL_OUT) and vertical (ROT_OUT) tilt angle measurements, using a fully-calibrated dual-axis accelerometer. If we assume that the axis of rotation is perpendicular to gravity and to one of the accelerometers, one might be able to accomplish this using one of the horizontal outputs and the two alarms.  For this discussion, let's assume that the reference position is when the x-axis is at 0 degrees, clockwise rotation produces a positive response and counterclockwise rotation produces a negative response.

ALM_CTRL = 0x661F

ALM_MAG1 = 0x8028

ALM_MAG2 =0x3FD8

The ALM_CTRL setting options are located on page 16 of the ADIS16209 (Rev C) datasheet.  Setting this to 0x661F establishes the following settings:

  • Set Alarm 1 and Alarm 2 to monitor XINCL_OUT
  • Use static level comparisons (not dynamic, "rate of change")
  • Use filtered data for both Alarm 1 and Alarm 2
  • Set DIO2 as a positive-polarity alarm indicator.

Setting ALM_MAG1 = 0x8028 establishes the Alarm 1 threshold at greater than 1 degree.

Setting ALM_MAG2 = 0x3FD8 establishes the Alarm 2 threshold at less than -1 degree.

So, DIO2 will go high when XINCL_OUT is greater than 1 degree or less than -1 degree.

In order to discriminate between Alarm 1 (clockwise) and Alarm 2 (counterclockwise), monitor STATUS[9:8], using the SPI port. For more information on the STATUS register, refer to page 18 in the ADIS16209 (Rev C) datasheet.

Note that this technique will also work when using the ADIS16201, ADIS16203 or ADIS16210.

For a step-by-step guide for testing this, using the ADIS16209/PCB and EVAL-ADIS, click on the following link:

https://ez.analog.com/docs/DOC-10180

I hope that helps!

Best,

NevadaMark

Tags: adis16209 sensors accelerometers adis16203 adis16210 Accelerometers - Special Purpose adis16201 productpage Show More
  • Share
  • History
  • More