Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
MEMS Inertial Sensors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
MEMS Inertial Sensors
MEMS Inertial Sensors
Documents What is the ADXL375?
  • Q&A
  • Files
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +3-D Model/STEP: FAQ
  • +AD22282-A-R2: FAQ
  • +ADIS16000: FAQ
  • +ADIS16003 MTBF: FAQ
  • +ADIS16006: FAQ
  • +ADIS16201: FAQ
  • +ADIS16203: FAQ
  • +ADIS16204: FAQ
  • +ADIS16209: FAQ
  • +ADIS16210: FAQ
  • +ADIS16223: FAQ
  • +ADIS16227: FAQ
  • +ADIS16228: FAQ
  • +ADIS16229: FAQ
  • +ADIS16240: FAQ
  • +ADIS16255: FAQ
  • +ADIS16355: FAQ
  • +ADIS16364: FAQ
  • +ADIS16365: FAQ
  • +ADIS16375: FAQ
  • +ADIS16385: FAQ
  • +ADIS16400: FAQ
  • +ADIS16405: FAQ
  • +ADIS16407: FAQ
  • +ADIS16445: FAQ
  • +ADIS16448: FAQ
  • +ADIS16460: FAQ
  • +ADIS16475: FAQ
  • +ADIS16477: FAQ
  • +ADIS1647x: FAQ
  • +ADIS16480: FAQ
  • +ADISUSB: FAQ
  • +ADXL001: FAQ
  • +ADXL203: FAQ
  • +ADIS16300: FAQ
  • +ADIS16485: FAQ
  • +ADIS16488: FAQ
  • +ADIS16488A: FAQ
  • +ADIS16490: FAQ
  • +ADIS16495: FAQ
  • +ADIS16497: FAQ
  • +ADXL103: FAQ
  • +ADXL150: FAQ
  • +ADxL193: FAQ
  • +ADXL202: FAQ
  • +ADXL206: FAQ
  • +ADXL210: FAQ
  • +ADXL210E: FAQ
  • +ADXL213: FAQ
  • +ADxL230: FAQ
  • +ADXL278: FAQ
  • +ADXL312: FAQ
  • +ADXL313: FAQ
  • +ADXL320: FAQ
  • +ADXL321: FAQ
  • +ADXL322: FAQ
  • +ADXL327: FAQ
  • +ADXL335: FAQ
  • +ADXL337: FAQ
  • +ADXL345: FAQ
  • +AD22290: FAQ
  • +ADIS16003: FAQ
  • +ADIS16133: FAQ
  • +ADIS16135: FAQ
  • +ADIS16265: FAQ
  • +ADIS16305: FAQ
  • +ADXL326: FAQ
  • +ADXL350: FAQ
  • +ADXL362: FAQ
  • -ADXL375: FAQ
    • How do we communicate with the ADXL375?
    • How does the shock detection feature of the ADXL375 work?
    • What is the ADXL375?
    • What is the influence of accelerometer bandwidth on the accuracy of shock measurements?
    • Where can I find schematics for EVAL-ADXL375Z-M and EVAL-ADXL375Z-S
    • ADXL375 Output Data Rate vs. Current Consumption
    • What is the DC response for the ADXL372 and ADXL375 accelerometers?
  • +ADXL377: FAQ
  • +ADXL78: FAQ
  • +ADXRS150: FAQ
  • +ADXRS290: FAQ
  • +ADXRS300: FAQ
  • +ADXRS401: FAQ
  • +ADXRS453: FAQ
  • +ADXRS610: FAQ
  • +ADxRS614: FAQ
  • +ADXRS623: FAQ
  • +ADXRS646: FAQ
  • +ADXRS652: FAQ
  • +ADXRS800: FAQ
  • +ADIS16136: FAQ
  • +ADIS16137: FAQ
  • +ADIS16266: FAQ
  • +ADIS16334: FAQ
  • +ADIS16362 Evaluation Tool: FAQ
  • +ADIS16364 Evaluation Tool: FAQ
  • +ADIS16367: FAQ
  • +ADIS163xx: FAQ
  • +ADIS16489: FAQ
  • +ADIS1648x: FAQ
  • +ADXL346: FAQ
  • +ADXL363: FAQ
  • +EVAL-ADIS: FAQ
  • +EVAL-ADIS2: FAQ
  • +Filtering Functions: FAQ
  • +General: FAQ
  • +Gyroscope: FAQ
  • +Hard & Soft Iron Correction: FAQ
  • +ISEB USB: FAQ
  • +IMU: FAQ
  • +MEMS: FAQ
  • +Slip Ring Interface: FAQ
  • +SPI Troubleshooting: FAQ
  • +TEMP_OUT Variation: FAQ
  • +Test Procedures: FAQ
  • +AD590: FAQ
  • +AD5940: FAQ
  • +AD5941: FAQ
  • +AD595: FAQ
  • +AD8495: FAQ
  • +AD8497: FAQ
  • +ADAF1080-3EBZ, ADAF1080, ADAF1080: FAQ
  • +ADIS16IMU2 FAQ:
  • +ADMT4000: FAQ
  • +ADUCM355: FAQ
  • +ADXL343: FAQ
  • +ADXL357: FAQ
  • +ADXL367: FAQ
  • +ADXL372: FAQ
  • +ADXRS645 : FAQ
  • +Breakout Board FAQ:
  • +CN0429: FAQ
  • DS1922E: FAQ
  • +DS1922L: FAQ
  • +DS1922T: FAQ
  • +DS1923: FAQ
  • +EVAL-ADAF1080-3EBZ, ADAF1080: FAQ
  • +EVAL-ADXL312-SDP: FAQ
  • +IMU/Gryoscope Alignment FAQ:
  • +iSensor FAQ:
  • +MAX30001: FAQ
  • +MAX30003: FAQ
  • +MAX30003CTI+: FAQ
  • +MAX30003WING: FAQ
  • +MAX30009EVKIT: FAQ
  • +MAX30134EVSYS: FAQ
  • +MAX9621: FAQ
  • +TMP01: FAQ
  • +Wireless Vibration Sensors FAQ:

What is the ADXL375?

The ADXL375 is a low-power, 3-axis digital MEMS accelerometer that provides high resolution (98mg/LSB) measurement up to ±200g with a bandwidth of up to 1KHz. The ADXL375 is supplied in a 3mm × 5mm × 1mm, 14-lead LGA package.

What type of applications use the ADXL375?

The target application for ADXL375 is the measurement of shock and other high-g events.  Accurate shock information can be valuable in a wide range of applications, such as profiling the usage of leased assets or sensitive equipment, shipping data loggers, and accounting for motion artifacts. In contact sports, biking, or in the military, crash or impact metrics (such as magnitude, point of contact, and direction) can be used by doctors to better diagnose concussion or head trauma resulting from accidents.

What is special about the ADXL375?

The ADXL375 provides a compact, 3-axis and low power solution compatible with portable and battery powered applications but with sufficient dynamic range and bandwidth to accurately capture the shock events.  The current consumption at the maximum output data rate of 3200Hz is ~145µA and scales proportionally with data rate to as low as 35µA. The ADXL375 can be programmed to monitor single or double (primary and secondary) shocks along any combination of X, Y, and/or Z axes. In addition, the entire shock profile can be captured for further analysis using an integrated 32 sample memory.

How does the ADXL375 add value for the customer?

The ADXL375 provides a way of differentiating and recording shock events of interest based on both amplitude and pulse width. The shock detection function allows users to define a minimum threshold and time duration for the shock. This allows users to distinguish between two shock pulses where both pulses can exceed the minimum threshold setting, but differ in their sharpness.

In addition to the profile or time history, direction can also be an important parameter in determining the severity of a shock event. The ADXL375 allows monitoring of shock events in all 3-axes so that both the profile and direction can be accurately ascertained.

The ADXL375 also provides the option of capturing the entire shock profile for further analysis with no intervention from the host processor. This is achieved using the shock interrupt registers in combination with the accelerometer’s internal FIFO. Typically, in order to capture transient events the accelerometer needs to be continuously polled by the host processor at high data rates, significantly increasing the overall system power consumption.  The ADXL375 offers considerable power savings by letting the processor be in a low power state for the majority of the time especially in applications where shock events are rare and can occur over periods of months or years.

What are the critical performance parameters of the ADXL375?

  • Bandwidth up to 1KHz
  • Range = ±200g, tri-axis
  • Noise density = 5mg/√Hz
  • Current consumption = 35µA to 145µA
Tags: accelerometer adxl375 shock mems high-g
  • Share
  • History
  • More