Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

EngineerZone
EngineerZone
MEMS Inertial Sensors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
MEMS Inertial Sensors
MEMS Inertial Sensors
Documents ADxL230: X and Y axes matched, Calibration of zero point
  • Q&A
  • Files
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +3-D Model/STEP: FAQ
  • +AD22282-A-R2: FAQ
  • +ADIS16000: FAQ
  • +ADIS16003 MTBF: FAQ
  • +ADIS16006: FAQ
  • +ADIS16201: FAQ
  • +ADIS16203: FAQ
  • +ADIS16204: FAQ
  • +ADIS16209: FAQ
  • +ADIS16210: FAQ
  • +ADIS16223: FAQ
  • +ADIS16227: FAQ
  • +ADIS16228: FAQ
  • +ADIS16229: FAQ
  • +ADIS16240: FAQ
  • +ADIS16255: FAQ
  • +ADIS16355: FAQ
  • +ADIS16364: FAQ
  • +ADIS16365: FAQ
  • +ADIS16375: FAQ
  • +ADIS16385: FAQ
  • +ADIS16400: FAQ
  • +ADIS16405: FAQ
  • +ADIS16407: FAQ
  • +ADIS16445: FAQ
  • +ADIS16448: FAQ
  • +ADIS16460: FAQ
  • +ADIS16475: FAQ
  • +ADIS16477: FAQ
  • +ADIS1647x: FAQ
  • +ADIS16480: FAQ
  • +ADISUSB: FAQ
  • +ADXL001: FAQ
  • +ADXL203: FAQ
  • +ADIS16300: FAQ
  • +ADIS16485: FAQ
  • +ADIS16488: FAQ
  • +ADIS16488A: FAQ
  • +ADIS16490: FAQ
  • +ADIS16495: FAQ
  • +ADIS16497: FAQ
  • +ADXL103: FAQ
  • +ADXL150: FAQ
  • +ADxL193: FAQ
  • +ADXL202: FAQ
  • +ADXL206: FAQ
  • +ADXL210: FAQ
  • +ADXL210E: FAQ
  • +ADXL213: FAQ
  • -ADxL230: FAQ
    • ADxL230: X and Y axes matched, Calibration of zero point
  • +ADXL278: FAQ
  • +ADXL312: FAQ
  • +ADXL313: FAQ
  • +ADXL320: FAQ
  • +ADXL321: FAQ
  • +ADXL322: FAQ
  • +ADXL327: FAQ
  • +ADXL335: FAQ
  • +ADXL337: FAQ
  • +ADXL345: FAQ
  • +AD22290: FAQ
  • +ADIS16003: FAQ
  • +ADIS16133: FAQ
  • +ADIS16135: FAQ
  • +ADIS16265: FAQ
  • +ADIS16305: FAQ
  • +ADXL326: FAQ
  • +ADXL350: FAQ
  • +ADXL362: FAQ
  • +ADXL375: FAQ
  • +ADXL377: FAQ
  • +ADXL78: FAQ
  • +ADXRS150: FAQ
  • +ADXRS290: FAQ
  • +ADXRS300: FAQ
  • +ADXRS401: FAQ
  • +ADXRS453: FAQ
  • +ADXRS610: FAQ
  • +ADxRS614: FAQ
  • +ADXRS623: FAQ
  • +ADXRS646: FAQ
  • +ADXRS652: FAQ
  • +ADXRS800: FAQ
  • +ADIS16136: FAQ
  • +ADIS16137: FAQ
  • +ADIS16266: FAQ
  • +ADIS16334: FAQ
  • +ADIS16362 Evaluation Tool: FAQ
  • +ADIS16364 Evaluation Tool: FAQ
  • +ADIS16367: FAQ
  • +ADIS163xx: FAQ
  • +ADIS16489: FAQ
  • +ADIS1648x: FAQ
  • +ADXL346: FAQ
  • +ADXL363: FAQ
  • +EVAL-ADIS: FAQ
  • +EVAL-ADIS2: FAQ
  • +Filtering Functions: FAQ
  • +General: FAQ
  • +Gyroscope: FAQ
  • +Hard & Soft Iron Correction: FAQ
  • +ISEB USB: FAQ
  • +IMU: FAQ
  • +MEMS: FAQ
  • +Slip Ring Interface: FAQ
  • +SPI Troubleshooting: FAQ
  • +TEMP_OUT Variation: FAQ
  • +Test Procedures: FAQ
  • +AD590: FAQ
  • +AD5940: FAQ
  • +AD5941: FAQ
  • +AD595: FAQ
  • +AD8495: FAQ
  • +AD8497: FAQ
  • +ADIS16IMU2 FAQ:
  • +ADUCM355: FAQ
  • +ADXL343: FAQ
  • +ADXL357: FAQ
  • +ADXL367: FAQ
  • +Breakout Board FAQ:
  • +CN0429: FAQ
  • DS1922E: FAQ
  • +DS1922L: FAQ
  • +DS1922T: FAQ
  • +DS1923: FAQ
  • +EVAL-ADXL312-SDP: FAQ
  • +IMU/Gryoscope Alignment FAQ:
  • +iSensor FAQ:
  • +MAX30001: FAQ
  • +MAX30003: FAQ
  • +MAX30003CTI+: FAQ
  • +MAX30003WING: FAQ
  • +MAX30009EVKIT: FAQ
  • +MAX30134EVSYS: FAQ
  • +MAX9621: FAQ
  • +TMP01: FAQ
  • +Wireless Vibration Sensors FAQ:

ADxL230: X and Y axes matched, Calibration of zero point

Q 

1.
Is there any data available about the matching of sensitivity between the two
axis? It is necessary for me to be able to calibrate an instrument utilizing
this sensor. If the matching is negligible then I have to find only the 0g
points of the axes, but if it is not, then I also have to look for the +-1g
points. The reason, why only matching is important for me, is that I do
calculations with the quotient of the measured values.

2.
My other question relating calibration is the method for finding the accurate
zero of the sensor.
I have two ideas:
a. Find the +-1g points of that axis and do averaging b. Find the +-1g points
of the other axis and set that point to be the zero of the first axis Which
method is better? Are there any other methods better that theese?

3.
What is the minimum deviation when I apply logic "1" to the self test pin, that
shows  normal sensor functionality? It is necessary for me, because I have
problems with testing the sensor in the +1g position. Is it a reliable solution
to accept 150mg deviation when the sensor output reaches 1.2g?

 

A 

1. There is no specification for the matching of sensitivity of both axes. I
think it is safest therefore to assume that each axis can have sensitivity
variation of +/-60mV/g independent of the other axis. Even if we suppose that
the axes do tend to have similar sensitivity, this knowledge doesn't help much
if we don't know

2. Auto calibration is rather simple method, but a fixture is required. If the
PCB (with the accelerometer mounted on it) is mounted on a slowly rotating
fixture oriented such that the plane of the PCB is orthogonal to the surface of
the Earth the accelerometer will be exposed to ±1g in both axes as the PCB is
rotated 360°. The microcontroller should keep track of the minimum and maximum
output from both channels. Once this is known:

Zero g = (Minimum + Maximum) / 2
Sensitivity = (Maximum - Minimum) / 2

3. You should not rely on the ST pin to provide a precise aceleration stimulus.
It will give between 400mV and 1100mV of voltage change at 5V supply and this
number varies proportional to the cube of the supply voltage.

Tags: adxl230